Part Number: WL1835MOD
Tool/software: Linux
Hi
I am confusing with deception on 6622.swaa166.pdf
Section 5.3 Mesh+Station.
It said
Running mesh and station interfaces on the same device enables range extension of the AP and
offloading from the AP to the mesh network.
Which means if i connect AP which I want to extend the range. and run the mesh
It will extend my AP??
or
Am I have to make AP <->|STA+MESH|<->|MESH+AP|<-> User phone?
I made this connect it does not work
Is it because I did not configured routing table or iptables?
Is it because I have to make all in same network?
Basically I just want to extend AP using mesh
Could you give me some instruction or exmaple?
I tried 
and follow the multi role
It does not work for me
Thank you