This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TM4C1294NCPDT: TM4C1294 and Ti-RTOS and WiFi CC31xx/CC32xx, what he best solution?

Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: CC2640, CC3100

Tool/software: TI-RTOS

I wish to add WiFi solution that works between TM4C1294 and Ti-RTOS, what the best solution and is there example code I can use. So I far I cannot see demo project based on this devices

What suitable protocol to establish connection between laptop and device similar to the CDC protocol in USB (Serial links) for COM based data exchange or similar.

I'm familiar with Ethernet (15 year ago), BLE under CC2640 and USB (LPC1549, etc), this is first time I do WiFi.

R.