Other Parts Discussed in Thread: CC3220S, CC2650
Hi TI Team,
We have to send the Samples to RF lab for EMI/EMC testing so we have some query on below mentioned points . PLease help us to understand
>>1. What is the initialization state of radio firmware?
If we have flashed CC3220s with radio tool firmware and when we power on the board, will it transmit random packets or it will transmit only when by radio tool will be controlled?
>>2. What would be the state of all the GPIO when CC3220S has radio firmware and powered on?
>>3. What will happen on UART lines of CC3220S if it has radio firmware and powered ON?
We have connected CC3220S and CC2650 through UART lines. So i am asking for UART lines.
>>4. Does the CC2650 keep it's GPIOs connected to the WiFi UART in input/high-Z mode?
>>5. Is the WiFi UART RX line floating or does the CC3220 enable an internal pull-up?
Regards
Navendu