This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220: Consumption chart in LPDS: f(V_BAT)

Part Number: CC3220

Hello,

I'm not sure to write in the right channel,

anyway, i'm working on the CC3220SF with a supply voltage of 2.5V  (T° around 21°C) and I get 75uA of current draw in LPDS (MCU LPDS, NWP LPDS).

The datasheet says 135uA in those conditions with VBAT=3.6V and T=25°C.

I would like to know if you can provide me the following chart: current_drawn_in_LPDS = func(VBAT,T°) for me to see if there is any hardware problem with my schematics which will explain such a value.

Thank you very much for your time,

Jean BONO