Other Parts Discussed in Thread: DRA71XEVM, , DRA71, PMP, DRA718, DRA722, TPD12S015, TVP5158
Tool/software: Linux
Dear Sirs:
We are using a DRA71x EVM

And we have a module WL1835MODCOM8B EVM

The SDK we are using is ProcessorSDK Automotive 03.04.00.03

We bring it up by using SD card described in docs/the Processor_SDK_Linux_Automotive_Software_Developers_Guide.html
We try to run the Running basic Wifi tests section, but there is not wlan0 device.
Even if we insmod or modprobe and make sure the kernel module driver is loaded, the COM8B is still invisible in the console.
Please let us know what should we do, or what JUMP/SWITCH should be modified to run the test.
The below is our console log:
U-Boot SPL 2016.05-g333293e877 (Dec 28 2017 - 05:17:21)
DRA722-GP ES2.0
no pinctrl for hs200_1_8v
no pinctrl for ddr_1_8v
** First descriptor is NOT a primary desc on 1:1 **
*** Warning - bad CRC, using default environment
Trying to boot from MMC1
*** Warning - bad CRC, using default environment
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2016.05-g333293e877 (Dec 28 2017 - 05:17:21 +0530)
CPU : DRA722-GP ES2.0
Model: TI DRA71 EVM
Board: DRA71x EVM REV A.2
DRAM: 2 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
** First descriptor is NOT a primary desc on 1:1 **
*** Warning - bad CRC, using default environment
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid GPT ***
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid Backup GPT ***
ERROR: cannot find partition: 'userdata'
at arch/arm/cpu/armv7/omap-common/utils.c:199/mmc_get_part_size()
Warning: fastboot.userdata_size: unable to calc
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net:
Warning: ethernet@48484000 using MAC address from ROM
eth0: ethernet@48484000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
234 bytes read in 3 ms (76.2 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
3553072 bytes read in 197 ms (17.2 MiB/s)
103032 bytes read in 44 ms (2.2 MiB/s)
Booting from mmc0 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x363730 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe3000, end 8ffff277 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.84-g742f84423d (tiiappadmin@swubn03) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #1 SMP PREEMPT Thu Dec 28 05:05:59 IST 2017
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine model: TI DRA718 EVM
[ 0.000000] bootconsole [earlycon0] enabled
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
[ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
[ 0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009d000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 128 MiB at 0x00000000b0000000
[ 0.000000] Forcing write-allocate cache policy for SMP
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] OMAP4: Map 0x00000000fed00000 to fe600000 for dram barrier
[ 0.000000] DRA722 ES2.0
[ 0.000000] PERCPU: Embedded 11 pages/cpu @eed62000 s14912 r8192 d21952 u45056
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 516416
[ 0.000000] Kernel command line: console=ttyO0,115200n8 elevator=noop root=PARTUUID=e08b9073-02 rw rootwait earlyprintk fixrtc omapdrm.num_crtc=2 consoleblank=0 cma=128M@0xB0000000 rootfstype=ext4 snd.slots_reserved=1,1
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 1755896K/2072576K available (6615K kernel code, 319K rwdata, 2456K rodata, 340K init, 290K bss, 29960K reserved, 286720K cma-reserved, 1159168K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc08e402c (9073 kB)
[ 0.000000] .init : 0xc08e5000 - 0xc093a000 ( 340 kB)
[ 0.000000] .data : 0xc093a000 - 0xc0989ee0 ( 320 kB)
[ 0.000000] .bss : 0xc098b000 - 0xc09d3800 ( 290 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] RCU restricting CPUs from NR_CPUS=2 to nr_cpu_ids=1.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=1
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] Architected cp15 timer(s) running at 6.14MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.008317] Switching to timer-based delay loop, resolution 162ns
[ 0.014971] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.025239] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.030964] Console: colour dummy device 80x30
[ 0.035620] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.042414] This ensures that you still see kernel messages. Please
[ 0.048932] update your kernel commandline.
[ 0.053324] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.063967] pid_max: default: 32768 minimum: 301
[ 0.068884] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.075772] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.083629] Initializing cgroup subsys io
[ 0.087854] Initializing cgroup subsys memory
[ 0.092430] Initializing cgroup subsys devices
[ 0.097082] Initializing cgroup subsys freezer
[ 0.101737] Initializing cgroup subsys perf_event
[ 0.106657] Initializing cgroup subsys pids
[ 0.111060] CPU: Testing write buffer coherency: ok
[ 0.116358] /cpus/cpu@0 missing clock-frequency property
[ 0.121903] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.127844] Setting up static identity map for 0x80008380 - 0x800083e0
[ 0.178069] Brought up 1 CPUs
[ 0.181202] SMP: Total of 1 processors activated (12.29 BogoMIPS).
[ 0.187629] CPU: All CPU(s) started in HYP mode.
[ 0.192465] CPU: Virtualization extensions available.
[ 0.198047] devtmpfs: initialized
[ 0.232700] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.241633] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.430346] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.440552] futex hash table entries: 256 (order: 2, 16384 bytes)
[ 0.456233] pinctrl core: initialized pinctrl subsystem
[ 0.462672] NET: Registered protocol family 16
[ 0.468416] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.505639] cpuidle: using governor ladder
[ 0.535664] cpuidle: using governor menu
[ 0.548867] OMAP GPIO hardware version 0.1
[ 0.557266] GPIO line 161 (radio_rst) hogged as output/low
[ 0.565349] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
[ 0.598874] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.607207] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.613785] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.621482] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.629754] OMAP DMA hardware revision 0.0
[ 0.714763] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 0.725730] edma 43300000.edma: memcpy is disabled
[ 0.735502] edma 43300000.edma: TI EDMA DMA engine driver
[ 0.746028] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.752099] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.758177] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.764221] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.790636] pcf857x 0-0020: probed
[ 0.794824] pcf857x 0-0021: probed
[ 0.798772] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.805052] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[ 0.824699] pcf857x: probe of 3-0021 failed with error -121
[ 0.830539] omap_i2c 4807a000.i2c: bus 3 rev0.12 at 400 kHz
[ 0.856615] GPIO line 465 (vin6_sel_s0) hogged as output/low
[ 0.862632] GPIO line 464 (pm_oe_n) hogged as output/high
[ 0.868372] pcf857x 4-0026: probed
[ 0.872245] pca953x 4-0020: failed reading register
[ 0.877350] pca953x: probe of 4-0020 failed with error -121
[ 0.883772] omap_i2c 4807c000.i2c: bus 4 rev0.12 at 400 kHz
[ 0.889785] media: Linux media interface: v0.10
[ 0.894580] Linux video capture interface: v2.00
[ 0.899443] pps_core: LinuxPPS API ver. 1 registered
[ 0.904636] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.914115] PTP clock support registered
[ 0.918273] EDAC MC: Ver: 3.0.0
[ 0.928820] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.935351] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.942091] Advanced Linux Sound Architecture Driver Initialized.
[ 0.949313] clocksource: Switched to clocksource arch_sys_counter
[ 0.965685] NET: Registered protocol family 2
[ 0.970768] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.978150] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.984984] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.991652] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.997840] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 1.004669] NET: Registered protocol family 1
[ 1.019529] RPC: Registered named UNIX socket transport module.
[ 1.025695] RPC: Registered udp transport module.
[ 1.030646] RPC: Registered tcp transport module.
[ 1.035562] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.043360] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 1.071930] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 1.088682] NFS: Registering the id_resolver key type
[ 1.094015] Key type id_resolver registered
[ 1.098396] Key type id_legacy registered
[ 1.102678] ntfs: driver 2.1.32 [Flags: R/O].
[ 1.108772] bounce: pool size: 64 pages
[ 1.113018] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 1.120750] io scheduler noop registered (default)
[ 1.125758] io scheduler deadline registered
[ 1.130353] io scheduler cfq registered
[ 1.138463] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
[ 1.146061] pinctrl-single 4a002e8c.pinmux: 1 pins at pa fc002e8c size 4
[ 1.156301] PCI host bridge /ocp/axi@0/pcie_rc@51000000 ranges:
[ 1.162519] No bus range found for /ocp/axi@0/pcie_rc@51000000, using [bus 00-ff]
[ 1.170506] IO 0x20003000..0x20012fff -> 0x00000000
[ 1.175879] MEM 0x20013000..0x2fffffff -> 0x20013000
[ 1.213302] dra7-pcie 51000000.pcie_rc: link is not up
[ 1.218826] dra7-pcie 51000000.pcie_rc: PCI host bridge to bus 0000:00
[ 1.225639] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 1.231373] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 1.237805] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 1.245365] PCI: bus0: Fast back to back transfers disabled
[ 1.251299] PCI: bus1: Fast back to back transfers enabled
[ 1.257095] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 1.264179] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 1.271253] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 1.276659] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[ 1.340310] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 1.350352] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 301, base_baud = 3000000) is a 8250
[ 1.359590] console [ttyS0] enabled
[ 1.359590] console [ttyS0] enabled
[ 1.366753] bootconsole [earlycon0] disabled
[ 1.366753] bootconsole [earlycon0] disabled
[ 1.376440] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 302, base_baud = 3000000) is a 8250
[ 1.386520] [drm] Initialized drm 1.1.0 20060810
[ 1.392786] omapdss_dss 58000000.dss: master bind failed: -517
[ 1.399352] tpd12s015 encoder: failed to find video source
[ 1.405491] connector-hdmi connector: failed to find video source
[ 1.497997] loop: module loaded
[ 1.511284] m25p80 spi32766.0: s25fl256s1 (32768 Kbytes)
[ 1.516679] 7 ofpart partitions found on MTD device spi32766.0
[ 1.522576] Creating 7 MTD partitions on "spi32766.0":
[ 1.527738] 0x000000000000-0x000000040000 : "QSPI.SPL"
[ 1.543829] 0x000000040000-0x000000140000 : "QSPI.u-boot"
[ 1.560162] 0x000000140000-0x0000001c0000 : "QSPI.u-boot-spl-os"
[ 1.577055] 0x0000001c0000-0x0000001d0000 : "QSPI.u-boot-env"
[ 1.593714] 0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1"
[ 1.611040] 0x0000001e0000-0x0000009e0000 : "QSPI.kernel"
[ 1.627297] 0x0000009e0000-0x000002000000 : "QSPI.file-system"
[ 1.645079] libphy: Fixed MDIO Bus: probed
[ 1.699342] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[ 1.705467] libphy: 48485000.mdio: probed
[ 1.724039] davinci_mdio 48485000.mdio: phy[2]: device 48485000.mdio:02, driver TI DP83867
[ 1.732398] davinci_mdio 48485000.mdio: phy[3]: device 48485000.mdio:03, driver TI DP83867
[ 1.741431] cpsw 48484000.ethernet: Detected MACID = c8:fd:19:e0:59:78
[ 1.748079] cpsw 48484000.ethernet: cpts: overflow check period 800
[ 1.755161] cpsw 48484000.ethernet: cpsw: Detected MACID = c8:fd:19:e0:59:79
[ 1.763901] mousedev: PS/2 mouse device common for all mice
[ 1.780277] i2c /dev entries driver
[ 1.784487] tvp5158 4-0058: Unable to of_probe
[ 1.789452] ov1063x 4-0037: Failed writing register 0x0103!
[ 1.795060] ov1063x: probe of 4-0037 failed with error -121
[ 1.800841] ov490 4-0024: Failed reading register 0x300a!
[ 1.806270] ov490: probe of 4-0024 failed with error -121
[ 1.812422] vpe 489d0000.vpe: loading firmware vpdma-1b8.bin
[ 1.819487] vip 48970000.vip: loading firmware vpdma-1b8.bin
[ 1.829937] vpe 489d0000.vpe: Device registered as /dev/video0
[ 1.836531] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 1.842095] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 1.848480] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 1.854909] vip 48970000.vip: VPDMA firmware loaded
[ 1.860030] vsys_3v3: supplied by evm_12v0
[ 1.864187] evm_3v3: supplied by vsys_3v3
[ 1.899809] omap_hsmmc 480d1000.mmc: no pinctrl state for sdr25 mode
[ 1.907255] omap_hsmmc 480d1000.mmc: no pinctrl state for sdr12 mode
[ 1.915688] omap_hsmmc 480d1000.mmc: no pinctrl state for hs mode
[ 1.953327] mmc0: MAN_BKOPS_EN bit is not set
[ 1.960143] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.969079] mmc0: new HS200 MMC card at address 0001
[ 1.977941] hwspinlock_user gatemp: requested 20 hwspinlocks
[ 1.985306] aic_dvdd: supplied by evm_3v3
[ 1.991910] davinci-mcasp 48464000.mcasp: DAI is shared
[ 1.997719] mmcblk0: mmc0:0001 MMC08G 7.25 GiB
[ 2.002929] davinci-mcasp 48474000.mcasp: DAI is shared
[ 2.009560] NET: Registered protocol family 10
[ 2.019560] mmcblk0boot0: mmc0:0001 MMC08G partition 1 8.00 MiB
[ 2.025921] sit: IPv6 over IPv4 tunneling driver
[ 2.031189] NET: Registered protocol family 17
[ 2.035890] Key type dns_resolver registered
[ 2.040450] omap_voltage_late_init: Voltage driver support not added
[ 2.047401] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.053770] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.060070] mmcblk0boot1: mmc0:0001 MMC08G partition 2 8.00 MiB
[ 2.066500] cpu0 supply vdd not found, using dummy regulator
[ 2.073555] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.079867] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.087146] cpu0 supply vdd not found, using dummy regulator
[ 2.095879] Power Management for TI OMAP4+ devices.
[ 2.101143] Registering SWP/SWPB emulation handler
[ 2.107624] dmm 4e000000.dmm: workaround for errata i878 in use
[ 2.116338] dmm 4e000000.dmm: initialized all PAT entries
[ 2.133086] evm_5v0: supplied by evm_12v0
[ 2.137155] lp8733-ldo1: supplied by evm_5v0
[ 2.142955] lp8732-ldo0: supplied by vsys_3v3
[ 2.147883] OMAP DSS rev 6.1
[ 2.151712] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[ 2.160453] omap-hdmi-audio omap-hdmi-audio.4.auto: snd-soc-dummy-dai <-> 58040000.encoder mapping ok
[ 2.180681] omapdss_dss 58000000.dss: bound 58040000.encoder (ops hdmi5_component_ops)
[ 2.189991] tvp5158 4-0058: Unable to of_probe
[ 2.195034] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 2.200053] evm_3v3_sd: supplied by evm_3v3
[ 2.245245] asoc-simple-card sound@0: tlv320aic3x-hifi <-> 48468000.mcasp mapping ok
[ 2.269715] asoc-simple-card jamr3_sound: tlv320aic3x-hifi <-> 48474000.mcasp mapping ok
[ 2.279893] 58040000.encoder supply vdda not found, using dummy regulator
[ 2.290599] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.297244] [drm] No driver support for vblank timestamp query.
[ 2.303268] omapdrm omapdrm.0: No connectors reported connected with modes
[ 2.310241] [drm] Cannot find any crtc or sizes - going 1024x768
[ 2.321235] [drm] Enabling DMM ywrap scrolling
[ 2.332096] Console: switching to colour frame buffer device 128x48
[ 2.343884] omapdrm omapdrm.0: fb0: omapdrm frame buffer device
[ 2.380305] [drm] Initialized omapdrm 1.0.0 20110917 on minor 0
[ 2.386497] tvp5158 4-0058: Unable to of_probe
[ 2.391625] hctosys: unable to open rtc device (rtc0)
[ 2.408962] aic_dvdd: disabling
[ 2.412165] vmmcwl_fixed: disabling
[ 2.415852] lp8733-ldo0: disabling
[ 2.419827] ALSA device list:
[ 2.422835] #0: DRA7xx-EVM
[ 2.425755] #1: HDMI 58040000.encoder
[ 2.429647] #2: DRA7xx-JAMR3
[ 2.433768] Waiting for root device PARTUUID=e08b9073-02...
[ 2.445414] mmc2: host does not support reading read-only switch, assuming write-enable
[ 2.456539] mmc2: new high speed SDHC card at address aaaa
[ 2.472566] mmcblk1: mmc2:aaaa SU04G 3.69 GiB
[ 2.486609] mmcblk1: p1 p2
[ 2.490174] tvp5158 4-0058: Unable to of_probe
[ 3.049918] EXT4-fs (mmcblk1p2): recovery complete
[ 3.056209] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[ 3.064413] VFS: Mounted root (ext4 filesystem) on device 179:50.
[ 3.073388] devtmpfs: mounted
[ 3.076577] Freeing unused kernel memory: 340K
[ 3.081057] This architecture does not have kernel memory protection.
[ 3.271462] systemd[1]: System time before build time, advancing clock.
[ 3.312994] random: systemd: uninitialized urandom read (16 bytes read, 20 bits of entropy available)
[ 3.328408] random: systemd: uninitialized urandom read (16 bytes read, 20 bits of entropy available)
[ 3.340231] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT +GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[ 3.358783] systemd[1]: Detected architecture arm.
Welcome to Arago 2016.12!
[ 3.380500] systemd[1]: Set hostname to <dra7xx-evm>.
[ 3.415051] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 21 bits of entropy available)
[ 3.441005] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 21 bits of entropy available)
[ 3.460560] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 22 bits of entropy available)
[ 3.473984] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 22 bits of entropy available)
[ 3.491916] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 22 bits of entropy available)
[ 3.587150] random: systemd: uninitialized urandom read (16 bytes read, 25 bits of entropy available)
[ 3.597022] random: systemd: uninitialized urandom read (16 bytes read, 25 bits of entropy available)
[ 3.607175] random: systemd: uninitialized urandom read (16 bytes read, 25 bits of entropy available)
[ 3.963894] systemd[1]: sockets.target: Found ordering cycle on sockets.target/start
[ 3.971796] systemd[1]: sockets.target: Found dependency on rpcbind.socket/start
[ 3.979235] systemd[1]: sockets.target: Found dependency on sysinit.target/start
[ 3.986736] systemd[1]: sockets.target: Found dependency on alignment.service/start
[ 3.994450] systemd[1]: sockets.target: Found dependency on basic.target/start
[ 4.001724] systemd[1]: sockets.target: Found dependency on sockets.target/start
[ 4.009157] systemd[1]: sockets.target: Breaking ordering cycle by deleting job rpcbind.socket/start
[ 4.018354] systemd[1]: rpcbind.socket: Job rpcbind.socket/start deleted to break ordering cycle starting with sockets.target/start
[ SKIP ] Ordering cycle found, skipping RPCbind Server Activation Socket
[ 4.049781] systemd[1]: sockets.target: Found ordering cycle on sockets.target/start
[ 4.057568] systemd[1]: sockets.target: Found dependency on dbus.socket/start
[ 4.064796] systemd[1]: sockets.target: Found dependency on sysinit.target/start
[ 4.072272] systemd[1]: sockets.target: Found dependency on alignment.service/start
[ 4.080014] systemd[1]: sockets.target: Found dependency on basic.target/start
[ 4.087274] systemd[1]: sockets.target: Found dependency on sockets.target/start
[ 4.095003] systemd[1]: sockets.target: Breaking ordering cycle by deleting job dbus.socket/start
[ 4.103962] systemd[1]: dbus.socket: Job dbus.socket/start deleted to break ordering cycle starting with sockets.target/start
[ SKIP ] Ordering cycle found, skipping D-Bus System Message Bus Socket
[ 4.139703] systemd[1]: sockets.target: Found ordering cycle on sockets.target/start
[ 4.147488] systemd[1]: sockets.target: Found dependency on avahi-daemon.socket/start
[ 4.155463] systemd[1]: sockets.target: Found dependency on sysinit.target/start
[ 4.162966] systemd[1]: sockets.target: Found dependency on alignment.service/start
[ 4.170708] systemd[1]: sockets.target: Found dependency on basic.target/start
[ 4.177967] systemd[1]: sockets.target: Found dependency on sockets.target/start
[ 4.185440] systemd[1]: sockets.target: Breaking ordering cycle by deleting job avahi-daemon.socket/start
[ 4.195094] systemd[1]: avahi-daemon.socket: Job avahi-daemon.socket/start deleted to break ordering cycle starting with sockets.target/start
[ SKIP ] Ordering cycle found, skipping Avah...S/DNS-SD Stack Activation Socket
[ 4.229684] systemd[1]: sockets.target: Found ordering cycle on sockets.target/start
[ 4.237468] systemd[1]: sockets.target: Found dependency on dropbear.socket/stop
[ 4.244946] systemd[1]: sockets.target: Found dependency on sysinit.target/start
[ 4.252422] systemd[1]: sockets.target: Found dependency on alignment.service/start
[ 4.260179] systemd[1]: sockets.target: Found dependency on basic.target/start
[ 4.267438] systemd[1]: sockets.target: Found dependency on sockets.target/start
[ 4.274912] systemd[1]: sockets.target: Breaking ordering cycle by deleting job dropbear.socket/stop
[ 4.284130] systemd[1]: dropbear.socket: Job dropbear.socket/stop deleted to break ordering cycle starting with sockets.target/start
[ SKIP ] Ordering cycle found, skipping dropbear.socket
[ 4.320603] systemd[1]: basic.target: Found ordering cycle on basic.target/start
[ 4.328040] systemd[1]: basic.target: Found dependency on sysinit.target/start
[ 4.335351] systemd[1]: basic.target: Found dependency on alignment.service/start
[ 4.342915] systemd[1]: basic.target: Found dependency on basic.target/start
[ 4.350044] systemd[1]: basic.target: Breaking ordering cycle by deleting job alignment.service/start
[ 4.359350] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with basic.target/start
[ SKIP ] Ordering cycle found, skipping alignment.service
[ 4.402850] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 4.429603] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 4.459703] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 4.489617] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 4.509825] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 4.539708] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ 4.569546] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 4.589902] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ 4.619657] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 4.651040] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
[ 4.680344] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 4.710232] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 4.739576] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 4.759778] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 4.790274] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 4.820589] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 4.851894] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 4.872561] systemd[1]: Starting Setup Virtual Console...
Starting Setup Virtual Console...
[ 4.912140] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 4.951564] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 4.981534] systemd[1]: Mounting Debug File System...
[ 4.994795] CMEMK module: reference Linux version 4.4.84
Mounting Debug File System...
[ 5.017914] no physical memory specified
[ 5.030170] cmemk initialized
[ 5.035521] systemd[1]: Mounting Temporary Directory...
[ 5.059664] cryptodev: driver 1.8 loaded.
Mounting Temporary Directory...
[ 5.092583] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...[ 5.134457] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
[ 5.162430] systemd[1]: Starting Create list of required static device nodes for the current kernel...
Starting Create list of required st... nodes for the current kernel...
[ 5.199815] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 5.229595] systemd[1]: Reached target Sockets.
[ OK ] Reached target Sockets.
[ 5.256774] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 5.289785] systemd[1]: Mounted Debug File System.
[ OK ] Mounted Debug File System.
[ 5.320528] systemd[1]: Mounted Temporary Directory.
[ OK ] Mounted Temporary Directory.
[ 5.349874] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Started Setup Virtual Console.
[ OK ] Started Load Kernel Modules.
[ OK ] Started Remount Root and Kernel File Systems.
[ OK ] Started Create list of required sta...ce nodes for the current kernel.
Starting Create Static Device Nodes in /dev...
Starting udev Coldplug all Devices...
Starting Apply Kernel Variables...
Starting Flush Journal to Persistent Storage...
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Started Apply Kernel Variables.
[ 6.163486] systemd-journald[125]: Received request to flush runtime journal from PID 1
[ OK ] Started Flush Journal to Persistent Storage.
Starting udev Kernel Device Manager...
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
[ OK ] Mounted /var/volatile.
[ OK ] Mounted /media/ram.
[ OK ] Started udev Kernel Device Manager.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Load/Save Random Seed.
[ OK ] Started Create Volatile Files and Directories.
[ 7.266081] omap-rproc 58820000.ipu: assigned reserved memory node ipu1_cma@9d000000
[ 7.362823] remoteproc0: 58820000.ipu is available
[ 7.367731] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 7.489481] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 7.590097] tvp5158 4-0058: Unable to of_probe
[ 7.595616] omap-rproc 55020000.ipu: assigned reserved memory node ipu2_cma@95800000
[ 7.676276] remoteproc1: 55020000.ipu is available
[ OK ] Started udev Coldplug all Devices.[ 7.684062] remoteproc1: Note: remoteproc is still under development and considered experimental.
[ 7.842224] remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 7.870856] remoteproc0: registered virtio0 (type 7)
[ 7.975693] tvp5158 4-0058: Unable to of_probe
[ 7.980747] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
[ 8.010428] tvp5158 4-0058: Unable to of_probe
[ 8.015720] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[ OK ] Found device /dev/ttyS0.
[ 8.093663] tvp5158 4-0058: Unable to of_probe
[ 8.098398] omap-rproc 40800000.dsp: assigned reserved memory node dsp1_cma@99000000
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ 8.158867] remoteproc2: 40800000.dsp is available
[ 8.186315] remoteproc1: registered virtio1 (type 7)
[ 8.197207] remoteproc2: Note: remoteproc is still under development and considered experimental.
[ 8.281375] remoteproc2: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ OK ] Started Network Time Synchronization.
[ 8.425144] tvp5158 4-0058: Unable to of_probe
[ 8.754332] remoteproc2: registered virtio2 (type 7)
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Reached target System Time Synchronized.
Starting Synchronize System and HW clocks...
[FAILED] Failed to start Synchronize System and HW clocks.
See 'systemctl status sync-clocks.service' for details.
[ 9.355836] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 9.396127] CAN device driver interface
[ 9.462662] tvp5158 4-0058: Unable to of_probe
[ 9.468327] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
[ 9.576009] tvp5158 4-0058: Unable to of_probe
[ 9.580726] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
[ 9.646462] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
[ 9.652570] tvp5158 4-0058: Unable to of_probe
[ 9.673760] c_can_platform 4ae3c000.can: c_can_platform device registered (regs=fce3c000, irq=355)
[ 9.684995] tvp5158 4-0058: Unable to of_probe
[ OK ] Reached target System Initialization.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ 9.763443] tvp5158 4-0058: Unable to of_probe
[ OK ] Reached target Timers.
[ 9.793582] [drm] Initialized pvr 1.14.3699939 20110701 on minor 1
[ OK ] Reached target Basic System.
Starting TI MultiCore Tools Daemon...
[ 9.859685] tvp5158 4-0058: Unable to of_probe
[ OK ] Started Kernel Logging Service.
Starting Permit User Sessions...
Starting Network Service...
Starting Print notice about GPLv3 packages...
[ OK ] Started strongSwan IPsec IKEv1/IKEv2 daemon using ipsec.conf.
Starting Save/Restore Sound Card State...
Starting uim-sysfs.service...
[ OK ] Started System Logging Service.
[ 10.420287] net eth1: initializing cpsw version 1.15 (0)
[ 10.448604] tvp5158 4-0058: Unable to of_probe
[ OK ] Started Network Service.
[FAILED] Failed to start TI MultiCore Tools Daemon.
See 'systemctl status ti-mct-daemon.service' for details.
[ OK ] Started Permit User Sessions.
[ 10.555081] tvp5158 4-0058: Unable to of_probe
[ 10.574383] net eth0: initialized cpsw ale version 1.4
[ 10.669698] net eth0: ALE Table size 1024
[[032m OK ]Started Save/Restore Sound Card State.
[ 10.907857] NET: Registered protocol family 15
[ 11.195191] net eth1: phy found : id is : 0x2000a231
[ 11.432358] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[ 11.519412] net eth0: initializing cpsw version 1.15 (0)
[ 11.663640] Initializing XFRM netlink socket
[ 11.852679] net eth0: phy found : id is : 0x2000a231
[ 11.930719] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 12.331239] random: nonblocking pool is initialized
[ 13.598563] remoteproc0: powering up 58820000.ipu
[ 13.703353] remoteproc0: Booting fw image dra7-ipu1-fw.xem4, size 4794908
[ 13.806500] omap-iommu 58882000.mmu: 58882000.mmu: version 2.1
[ 13.885851] remoteproc0: remote processor 58820000.ipu is now up
[ 13.962321] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 13.967877] virtio_rpmsg_bus virtio0: creating channel rpmsg-client-sample addr 0x32
[ 13.998494] virtio_rpmsg_bus virtio0: creating channel rpmsg-client-sample addr 0x33
[ 14.009859] tvp5158 4-0058: Unable to of_probe
[ 14.055213] remoteproc1: powering up 55020000.ipu
[ 14.063019] virtio_rpmsg_bus virtio0: creating channel rpmsg-omx addr 0x3c
[ 14.105905] remoteproc1: Booting fw image dra7-ipu2-fw.xem4, size 3743112
[ 14.120862] virtio_rpmsg_bus virtio0: creating channel rpmsg-rpc addr 0x65
[ 14.171816] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
[ 14.608082] remoteproc1: remote processor 55020000.ipu is now up
[ 14.679732] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 14.685280] virtio_rpmsg_bus virtio1: creating channel rpmsg-rpc addr 0x65
[ 14.712443] virtio_rpmsg_bus virtio1: creating channel rpmsg-rpc addr 0x66
[ 14.732934] tvp5158 4-0058: Unable to of_probe
[ 14.760740] remoteproc2: powering up 40800000.dsp
[ 14.834595] remoteproc2: Booting fw image dra7-dsp1-fw.xe66, size 5635840
[ 14.886615] omap_hwmod: mmu0_dsp1: _wait_target_disable failed
[ 14.892523] omap-iommu 40d01000.mmu: 40d01000.mmu: version 3.0
[ 14.898478] omap-iommu 40d02000.mmu: 40d02000.mmu: version 3.0
[ 14.950480] tvp5158 4-0058: Unable to of_probe
[ 15.074222] remoteproc2: remote processor 40800000.dsp is now up
[ 15.127682] virtio_rpmsg_bus virtio2: rpmsg host is online
[ 15.133296] virtio_rpmsg_bus virtio2: creating channel rpmsg-client-sample addr 0x32
[ 15.169789] virtio_rpmsg_bus virtio2: creating channel rpmsg-client-sample addr 0x33
[ 15.182906] tvp5158 4-0058: Unable to of_probe
[ 15.232084] virtio_rpmsg_bus virtio2: creating channel rpmsg-omx addr 0x3c
[ 15.324949] rpmsg_rpc rpmsg3: probing service rpc_example_2 with src 1024 dst 101
[ 15.333627] virtio_rpmsg_bus virtio2: creating channel rpmsg-rpc addr 0x65
***************************************************************
**************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
binutils-dev
binutils
bison-dev
bison
cpp-symlinks
cpp
dosfstools
g++-symlinks
g++
gawk-dev
gawk
gcc-symlinks
gcc
gdb
gdbc6x
gdbserver
gstreamer1.0-libav
libcairo-perf-utils
libgmp10
libidn11
libmpc3
libmpfr4
m4-dev
m4
make
nettle
parted
swig-dev
swig
If you do not wish to distribute GPLv3 components please remove 15.370511] tvp5158 4-0058: Unable to of_probe
the above packages prior to distribution. This can be done usig
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
15.407963] rpmsg_rpc rpmsg4: probing service dce-callback with src 1024 dst 101
[ 15.472205] rpmsg_rpc rpmsg9: probing service rpc_example_4 with src 1024 dst 101
[ 15.523454] rpmsg_rpc rpmsg3: published functions = 8
[ 15.548227] rpmsg_rpc rpmsg9: published functions = 8
[[;32m OK ]Started Print notice about GPLv3 packages.
[ 15.595831] tvp5158 4-0058: Unable to of_probe
[ 15.670816] tvp5158 4-0058: Unable to of_probe
[ 15.675324] rpmsg_rpc rpmsg4: published functions = 4
[ 15.683346] rpmsg_rpc rpmsg5: probing service rpmsg-dce with src 1025 dst 102
[ 15.720251] tvp5158 4-0058: Unable to of_probe
[ 15.724753] rpmsg_rpc rpmsg5: published functions = 9
[ 15.964897] tvp5158 4-0058: Unable to of_probe
[ 16.040361] usbcore: registered new interface driver usbfs
[ 16.054610] usbcore: registered new interface driver hub
[ 16.076233] usbcore: registered new device driver usb
[ 16.105906] dwc3 48890000.usb: otg: primary host xhci-hcd.5.auto registered
[ 16.127709] dwc3 48890000.usb: otg: shared host xhci-hcd.5.auto registered
[ 16.151577] dwc3 48890000.usb: otg: can't start till gadget registers
[ 16.158357] tvp5158 4-0058: Unable to of_probe
[ 16.184529] xhci-hcd xhci-hcd.6.auto: xHCI Host Controller
[ 16.200941] xhci-hcd xhci-hcd.6.auto: new USB bus registered, assigned bus number 1
[ 16.226111] xhci-hcd xhci-hcd.6.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x00210010
[ 16.259804] xhci-hcd xhci-hcd.6.auto: irq 499, io mem 0x488d0000
[ 16.283458] hub 1-0:1.0: USB hub found
[ 16.294636] hub 1-0:1.0: 1 port detected
[ 16.313445] tvp5158 4-0058: Unable to of_probe
[ 16.318171] xhci-hcd xhci-hcd.6.auto: xHCI Host Controller
[ 16.328848] tvp5158 4-0058: Unable to of_probe
[ 16.341614] xhci-hcd xhci-hcd.6.auto: new USB bus registered, assigned bus number 2
[[;32m OK ]Listening on Load/Save RF Kill Switch Status dev/rfkill Watch.[ 16.358588] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ OK ] Reached target Sound Card.
[ 16.390733] hub 2-0:1.0: USB hub found
[ 16.398147] hub 2-0:1.0: 1 port detected
[ OK ] Started Getty on tty1.
[ 16.416113] tvp5158 4-0058: Unable to of_probe
[ 16.435387] tvp5158 4-0058: Unable to of_probe
[ OK ] Started Serial Getty on ttyS0.
[ OK ] Reached target Network.
Starting Lightning Fast Webserver With Light System Requirements...
Starting Network Name Resolution...
[ OK ] Started Lightning Fast Webserver With Light System Requirements.
[ OK ] Started Network Name Resolution.
[ OK ] Started uim-sysfs.service.
Starting rc.pvr.service...
[ 17.040221] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ]
[ OK ] Started rc.pvr.service.
Starting LSB: Dropbear Secure Shell server...
Starting weston.service...
[ OK ] Started weston.service.
Starting tiipclad-daemon.service...
Starting telnetd.service...
[ OK ] Started telnetd.service.
[ OK ] Started tiipclad-daemon.service.
[ OK ] Started LSB: Dropbear Secure Shell server.
Starting thttpd.service...
[ OK ] Started thttpd.service.
Starting rng-tools.service...
[ OK ] Started rng-tools.service.
Starting gdbserverproxy.service...
[ OK ] Started gdbserverproxy.service.
Starting matrix-gui-2.0.service...
[ OK ] Started matrix-gui-2.0.service.
Starting thermal-zone-init.service...
[ OK ] Started thermal-zone-init.service.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org dra7xx-evm ttyS0
Arago 2016.12 dra7xx-evm ttyS0
dra7xx-evm login: root
root@dra7xx-evm:~# [ 26.173501] omap_hwmod: mmu1_dsp1: _wait_target_disable failed
[ 26.187564] omap_hwmod: mmu0_dsp1: _wait_target_disable failed
ifconfig -a
can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:99
eth0 Link encap:Ethernet HWaddr C8:FD:19:E0:59:78
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:96
eth1 Link encap:Ethernet HWaddr C8:FD:19:E0:59:79
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1%132400/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:160 errors:0 dropped:0 overruns:0 frame:0
TX packets:160 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1
RX bytes:12160 (11.8 KiB) TX bytes:12160 (11.8 KiB)
sit0 Link encap:IPv6-in-IPv4
NOARP MTU:1480 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
root@dra7xx-evm:~#
root@dra7xx-evm:~#
root@dra7xx-evm:~#
root@dra7xx-evm:~#
root@dra7xx-evm:~# lsmod
Module Size Used by
bc_example 7186 0
xhci_plat_hcd 5311 0
xhci_hcd 109400 1 xhci_plat_hcd
usbcore 195602 2 xhci_plat_hcd,xhci_hcd
rpmsg_rpc 20010 0
dwc3 64707 0
udc_core 12063 1 dwc3
virtio_rpmsg_bus 13486 1 rpmsg_rpc
sha512_generic 9903 0
sha512_arm 12079 0
sha1_generic 2621 0
sha1_arm_neon 6261 0
sha1_arm 3862 1 sha1_arm_neon
md5 1897 0
cbc 2324 0
sha256_generic 9503 0
sha256_arm 12414 1
hmac 2735 1
drbg 13425 1
xfrm_user 23228 2
xfrm4_tunnel 2040 0
ipcomp 2473 0
xfrm_ipcomp 4695 1 ipcomp
esp4 6465 0
ah4 5665 0
af_key 27932 0
xfrm_algo 6970 5 ah4,esp4,af_key,xfrm_user,xfrm_ipcomp
extcon_usb_gpio 3756 0
pvrsrvkm 412372 1 bc_example
c_can_platform 6604 0
c_can 9718 1 c_can_platform
omap_aes_driver 19230 0
can_dev 13119 1 c_can
omap_sham 21089 0
omap_wdt 4570 0
dwc3_omap 5054 0
extcon 13943 3 dwc3,dwc3_omap,extcon_usb_gpio
omap_des 11446 0
omap_rng 4835 0
rng_core 7947 1 omap_rng
omap_remoteproc 13283 3
remoteproc 27313 3 omap_remoteproc,virtio_rpmsg_bus,rpmsg_rpc
virtio 7580 2 remoteproc,virtio_rpmsg_bus
virtio_ring 12291 2 remoteproc,virtio_rpmsg_bus
sch_fq_codel 8187 3
uio_module_drv 7353 0
gdbserverproxy 4671 0
cryptodev 37405 1
cmemk 35174 0
root@dra7xx-evm:~# insmod
root@dra7xx-evm:~# cd /lib/mod
-sh: cd: /lib/mod: No such file or directory
root@dra7xx-evm:~# cd /lib/mod
modprobe.d/ modules/
root@dra7xx-evm:~# cd /lib/modules/
root@dra7xx-evm:/lib/modules# ls
4.4.84-g742f84423d
root@dra7xx-evm:/lib/modules# cd 4.4.84-g742f84423d/
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d# ls
extra modules.builtin modules.devname modules.symbols.bin
kernel modules.builtin.bin modules.order
modules.alias modules.dep modules.softdep
modules.alias.bin modules.dep.bin modules.symbols
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d# cd kernel/
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel# ls
arch crypto drivers fs lib net sound
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel# cd drivers/
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers# ls
ata char gpio iio mfd power rtc virtio
bluetooth crypto hid input mtd remoteproc scsi w1
cdrom extcon hwmon media net rpmsg usb watchdog
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers# cd net/
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net# cd wireless/
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless# ls
brcm80211 iwlwifi mwifiex rt2x00 ti
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless# cd ti/
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti# ls
wl18xx wlcore
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti# cd wlcore/
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wlcore# ls
wlcore.ko wlcore_sdio.ko wlcore_spi.ko
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wlcore# insmod ./wlcore_sdio.ko
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wlcore# insmod ./wlcore.ko
[ 1046.925947] wlcore: Unknown symbol ieee80211_connection_loss (err 0)
[ 1046.932430] wlcore: Unknown symbol ieee80211_iterate_interfaces (err 0)
[ 1046.939088] wlcore: Unknown symbol ieee80211_sched_scan_stopped (err 0)
[ 1046.948600] wlcore: Unknown symbol ieee80211_chswitch_done (err 0)
[ 1046.956386] wlcore: Unknown symbol ieee80211_free_hw (err 0)
[ 1046.963021] wlcore: Unknown symbol ieee80211_probereq_get (err 0)
[ 1046.969176] wlcore: Unknown symbol ieee80211_ap_probereq_get (err 0)
[ 1046.977235] wlcore: Unknown symbol ieee80211_nullfunc_get (err 0)
[ 1046.984248] wlcore: Unknown symbol ieee80211_pspoll_get (err 0)
[ 1046.991134] wlcore: Unknown symbol ieee80211_register_hw (err 0)
[ 1046.997181] wlcore: Unknown symbol ieee80211_restart_hw (err 0)
[ 1047.004757] wlcore: Unknown symbol ieee80211_get_hdrlen_from_skb (err 0)
[ 1047.012391] wlcore: Unknown symbol ieee80211_stop_rx_ba_session (err 0)
[ 1047.019052] wlcore: Unknown symbol ieee80211_wake_queue (err 0)
[ 1047.026702] wlcore: Unknown symbol ieee80211_find_sta (err 0)
[ 1047.033423] wlcore: Unknown symbol wiphy_to_ieee80211_hw (err 0)
[ 1047.040370] wlcore: Unknown symbol ieee80211_queue_delayed_work (err 0)
[ 1047.047029] wlcore: Unknown symbol ieee80211_proberesp_get (err 0)
[ 1047.054938] wlcore: Unknown symbol ieee80211_remain_on_channel_expired (err 0)
[ 1047.063099] wlcore: Unknown symbol ieee80211_wake_queues (err 0)
[ 1047.069148] wlcore: Unknown symbol ieee80211_report_low_ack (err 0)
[ 1047.077089] wlcore: Unknown symbol ieee80211_free_txskb (err 0)
[ 1047.083934] wlcore: Unknown symbol ieee80211_alloc_hw_nm (err 0)
[ 1047.090897] wlcore: Unknown symbol rfc1042_header (err 0)
[ 1047.096350] wlcore: Unknown symbol ieee80211_tx_status (err 0)
[ 1047.103840] wlcore: Unknown symbol ieee80211_stop_queue (err 0)
[ 1047.110710] wlcore: Unknown symbol ieee80211_ready_on_channel (err 0)
[ 1047.117195] wlcore: Unknown symbol ieee80211_stop_queues (err 0)
[ 1047.124856] wlcore: Unknown symbol ieee80211_cqm_beacon_loss_notify (err 0)
[ 1047.132755] wlcore: Unknown symbol cfg80211_find_ie (err 0)
[ 1047.138379] wlcore: Unknown symbol ieee80211_sched_scan_results (err 0)
[ 1047.146652] wlcore: Unknown symbol ieee80211_scan_completed (err 0)
[ 1047.153830] wlcore: Unknown symbol ieee80211_iterate_active_interfaces_atomic (err 0)
[ 1047.162588] wlcore: Unknown symbol ieee80211_channel_to_frequency (err 0)
[ 1047.170281] wlcore: Unknown symbol ieee80211_unregister_hw (err 0)
[ 1047.176519] wlcore: Unknown symbol ieee80211_beacon_get_tim (err 0)
[ 1047.184441] wlcore: Unknown symbol ieee80211_hdrlen (err 0)
[ 1047.190940] wlcore: Unknown symbol ieee80211_cqm_rssi_notify (err 0)
[ 1047.197345] wlcore: Unknown symbol ieee80211_frequency_to_channel (err 0)
[ 1047.205854] wlcore: Unknown symbol ieee80211_queue_work (err 0)
[ 1047.212699] wlcore: Unknown symbol ieee80211_sta_ps_transition (err 0)
[ 1047.219288] wlcore: Unknown symbol cfg80211_find_vendor_ie (err 0)
[ 1047.227149] wlcore: Unknown symbol ieee80211_csa_finish (err 0)
[ 1047.233980] wlcore: Unknown symbol ieee80211_rx_napi (err 0)
insmod: ERROR: could not insert module ./wlcore.ko: Unknown symbol in module
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wlcore# ls
wlcore.ko wlcore_sdio.ko wlcore_spi.ko
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wlcore# modprobe wlcore
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wlcore# [ 1061.514496] cfg80211: World regulatory domain updated:
[ 1061.519727] cfg80211: DFS Master region: unset
[ 1061.524101] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp), (dfs_cac_time)
[ 1061.543046] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (N/A, 2000 mBm), (N/A)
[ 1061.551166] cfg80211: (2457000 KHz - 2482000 KHz @ 40000 KHz), (N/A, 2000 mBm), (N/A)
[ 1061.559205] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (N/A, 2000 mBm), (N/A)
[ 1061.569727] cfg80211: (5170000 KHz - 5250000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (N/A)
[ 1061.579254] cfg80211: (5250000 KHz - 5330000 KHz @ 80000 KHz, 160000 KHz AUTO), (N/A, 2000 mBm), (0 s)
[ 1061.590464] cfg80211: (5490000 KHz - 5730000 KHz @ 160000 KHz), (N/A, 2000 mBm), (0 s)
[ 1061.598593] cfg80211: (5735000 KHz - 5835000 KHz @ 80000 KHz), (N/A, 2000 mBm), (N/A)
[ 1061.608278] cfg80211: (57240000 KHz - 63720000 KHz @ 2160000 KHz), (N/A, 0 mBm), (N/A)
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wlcore#
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wlcore#
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wlcore# ls
wlcore.ko wlcore_sdio.ko wlcore_spi.ko
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wlcore# lsmod
Module Size Used by
wlcore 181887 0
mac80211 357826 1 wlcore
cfg80211 221800 2 mac80211,wlcore
wlcore_sdio 6911 0
bc_example 7186 0
xhci_plat_hcd 5311 0
xhci_hcd 109400 1 xhci_plat_hcd
usbcore 195602 2 xhci_plat_hcd,xhci_hcd
rpmsg_rpc 20010 0
dwc3 64707 0
udc_core 12063 1 dwc3
virtio_rpmsg_bus 13486 1 rpmsg_rpc
sha512_generic 9903 0
sha512_arm 12079 0
sha1_generic 2621 0
sha1_arm_neon 6261 0
sha1_arm 3862 1 sha1_arm_neon
md5 1897 0
cbc 2324 0
sha256_generic 9503 0
sha256_arm 12414 1
hmac 2735 1
drbg 13425 1
xfrm_user 23228 2
xfrm4_tunnel 2040 0
ipcomp 2473 0
xfrm_ipcomp 4695 1 ipcomp
esp4 6465 0
ah4 5665 0
af_key 27932 0
xfrm_algo 6970 5 ah4,esp4,af_key,xfrm_user,xfrm_ipcomp
extcon_usb_gpio 3756 0
pvrsrvkm 412372 1 bc_example
c_can_platform 6604 0
c_can 9718 1 c_can_platform
omap_aes_driver 19230 0
can_dev 13119 1 c_can
omap_sham 21089 0
omap_wdt 4570 0
dwc3_omap 5054 0
extcon 13943 3 dwc3,dwc3_omap,extcon_usb_gpio
omap_des 11446 0
omap_rng 4835 0
rng_core 7947 1 omap_rng
omap_remoteproc 13283 3
remoteproc 27313 3 omap_remoteproc,virtio_rpmsg_bus,rpmsg_rpc
virtio 7580 2 remoteproc,virtio_rpmsg_bus
virtio_ring 12291 2 remoteproc,virtio_rpmsg_bus
sch_fq_codel 8187 3
uio_module_drv 7353 0
gdbserverproxy 4671 0
cryptodev 37405 1
cmemk 35174 0
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wlcore# ls
wlcore.ko wlcore_sdio.ko wlcore_spi.ko
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wlcore# cd ..
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti# ls
wl18xx wlcore
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti# cd wl18xx/
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wl18xx# ls
wl18xx.ko
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wl18xx# insmod ./wl18xx.ko
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wl18xx# ls -al
drwxr-xr-x 2 root root 4096 Dec 27 2017 .
drwxr-xr-x 4 root root 4096 Dec 27 2017 ..
-rw-r--r-- 1 root root 115488 Dec 27 2017 wl18xx.ko
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wl18xx# ifconfig -a
can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:99
eth0 Link encap:Ethernet HWaddr C8:FD:19:E0:59:78
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:96
eth1 Link encap:Ethernet HWaddr C8:FD:19:E0:59:79
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1%132400/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:160 errors:0 dropped:0 overruns:0 frame:0
TX packets:160 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1
RX bytes:12160 (11.8 KiB) TX bytes:12160 (11.8 KiB)
sit0 Link encap:IPv6-in-IPv4
NOARP MTU:1480 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
root@dra7xx-evm:/lib/modules/4.4.84-g742f84423d/kernel/drivers/net/wireless/ti/wl18xx#