This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF-LAUNCHXL: Factory Default

Part Number: CC3220SF-LAUNCHXL
Other Parts Discussed in Thread: UNIFLASH, CC3200

I am trying to reset the LaunchXL to factory default. It is Rev A.

I am able to connect to it with UniFlash and have set it up as:
Image Mode: Development
Secured Device: False
Restore To Factory Image SOP: Enable
Restore To Factory Configuration: Defaults and Image

I use 'Program Image (Create & Program) which seems to execute.

I install SOP 0 & 1 and power up the board. I connect to the board using PuTTY via USB.

I don't ever see any communications. I remove all SOP jumpers. Same. Apparently I'm confused.