Part Number: WL1837MODCOM8I
Other Parts Discussed in Thread: WL1837
Tool/software: Linux
Hello,
I have been directed to this forum to inquire on the pin compatibility between WL1837 and WL1877Q. My original post discussed the compatibility between the TDA2EVM5777 Rev G and the WL1837 (WL1837COM8 evm) . In this previous forum post, I was directed to use the COM8Q board that is based on the WL1877Q. My questions are:
- Would I be able to develop software on the TDA2x for the WL1837 while using the COM8Q board connected to the TDA2EVM5777 Vayu EVM?
- Are the COM8Q board and the wl1837 pin compatible?
- Would the default Processor SDK Linux Automotive Kernel support the COM8Qboard or do I have to modify it?
- If I have to modify the kernel, what modifications do I have to make in order to get it to work?
Thank you,
-iFer