Other Parts Discussed in Thread: UNIFLASH, CC3200
HI,
I am trying to format cc3200 using UNIFLASH which is connected via USB but it is unable to connect and giving the error shown below:
[12:55:06] Begin Format operation.
[12:55:07] INFO: > Executing Operation: Connect
[12:55:09] INFO: setting break signal
[12:55:10] INFO: detecting FTDI for device reset
[12:55:25] ERROR: ---reading ACK signal failed---
[12:55:25] WARNING: ---seting break signal to false failed---
[12:55:27] INFO: setting break signal
[12:55:28] INFO: detecting FTDI for device reset
[12:55:44] ERROR: ---reading ACK signal failed---
[12:55:44] WARNING: ---seting break signal to false failed---
[12:55:46] INFO: setting break signal
[12:55:47] INFO: detecting FTDI for device reset
[12:56:02] ERROR: ---reading ACK signal failed---
[12:56:03] WARNING: ---seting break signal to false failed---
[12:56:05] INFO: setting break signal
[12:56:06] INFO: detecting FTDI for device reset
[12:56:21] ERROR: ---reading ACK signal failed---
[12:56:21] WARNING: ---seting break signal to false failed---
[12:56:21] FATAL: --- Can't connect to device !! ---
1. SOP2 jumper is not connected. Jumper is connected to VCC-P58
2. J6 and J7 are connected as Flash.