Other Parts Discussed in Thread: CC3220SF
Hi,
In the datasheet of the CC3220MOD module, there are two connections recommended for the reset pins-
1. "Connect nRESET to a switch, external controller, or host, only if nRESET will be in a defined state under all operating conditions. Leave VBAT_RESET unconnected to save power." -> Is it required to leave the VBAT_RESET input unconnected or it is fine to connect it to the 3.3V supply voltage? (as is done in the LAUNCH-CC3220MODSF development board)
2. "If nRESET cannot be in a defined state under all operating conditions, connect VBAT_RESET to the main module power supply (VBAT1 and VBAT2). Due to the internal pullup resistor a leakage current of 3.3 V / 100 kΩ is expected." -> Is it required to keep the nRESET pin open, or it can be driven from a reset switch?
Can you please show me an example of the schematic where the two options are shown? It will help with understanding clearly.
Regards,
Prachi