This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1837MOD: Disabling the 5G band in WL1837MOD

Part Number: WL1837MOD


Hi,

I want to know if I can disable the 5G band in the WL1837MOD completely to avoid regulation problem.

I need the 1837 for its temperature range but I don't need the 5G band.

Thanks

Noam

  • Hi,

    You should be able to disable 5GHz band by setting number of 5GHz antennas to 0 using wlconf.

    cd /usr/share/wlconf
    ./wlconf -i /lib/firmware/ti-connectivity/wl18xx-conf.bin -o /lib/firmware/ti-connectivity/wl18xx-conf.bin -s wl18xx.phy. number_of_assembled_ant5=0x0

    Then unload/load wilink driver modules.

    Best Regards,
    Eyal