I'm just starting a project that will consist of a number of CC3200-based sensors which send data back to a Windows PC using Wi-Fi. The PC will be running an app which reads and processes the data from these sensors utilizing the built-in Wi-Fi capabilities of the PC. Our client would also like to have access to the Internet over Wi-Fi on the PC at the same time. Is this possible? I'm assuming that I need to configure the sensors as Wi-Fi stations and the PC as a Wi-Fi AP to deal with collecting the sensor data. Is there a way to then use that same Wi-Fi card to access the Internet? Is there another way to configure everything to enable this functionality?
Thanks...
Brian