Hi,
Our customer used AM3517, Adeneo Wince BSP version:BSP_WINCE_ARM_A8-1.00.00.12.
They used AM3517EVM, SDIO WIFI type: Atheros AR6002 sd25 connection to EVM SD/MMC1 solt.
They have to build the WiFi driver into WinCE 6.0R2. When they insert the SDIO WiFi card,
below error message is appear repeatedly. The complete debug message see attached file.
BMI Read SOC Register: Exit (value: 1155)
BMI Read SOC Register: Enter (device: 0xC131EEC0, address:0x10004)
SDHCBusRequestHandler() - MMCHS_STAT_CTO
SDHCBusRequestHandler() - Timeout waiting for MMCHS_STAT_CC
SDSynchronousBusRequest_I: queue request failed(0xc0000014),TransferClass(0),
CommandCode(35),CommandArgument(1408a004)
SDSynchronousBusRequest__X: Failed status 0xC0000014
BMI Read SOC Register: Enter (device: 0xC131EEC0, address:0x10004)
Best Regards,
Shine