This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDC-WL1837MOD-AUDIO-MULTIROOM-CAPE: U105 CDCLVP1204

Part Number: TIDC-WL1837MOD-AUDIO-MULTIROOM-CAPE


I am working on an audio mesh using the TI WIlink 1837 on a beagle bone Black. My initial idea was to send audio A2DP via BT5 but it's not quite there. Using the TI audio mesh as a reference I am trying to find the replacement part for the U105 which I believe is part number is: CDCLVP1204. Two lines LVPECL Output, 2GHZ. Which alternate part would you recommend that best suited as an alternate part to the U105?  
Thanks

Darrin


Brand 1 - PERICOM/DIDES:

PI6C5922504 1:4 2.5GHz LVDS Clock/ Data Buffer 4Lines output, Frequency 2.5GHz, Higher than U105 specification
PI6C5913004-01 3GHz 1:4 LVPECL Fanout Buffer Buffer 4Lines output, Frequency 3 GHz, Higher than U105 specification
PI6C5916004 6GHz 1:4 LVPECL Fanout Buffer with Internal Termination Buffer 4Lines output, Frequency 6GHz, Higher than U105 specification
PI6C5946002 1:2 6GHz/ 12Gbps CML Clock/ Data Buffer 2lines output is the same as U105 output, but Frequency 6GHz, Higher than U105 specification

Brand 2-IDT:

8SLVS1118NLGI:2GHz 1:18 LVPECL 18lines output, It outputs more than U105 output, but frequency is same. All is 2G.
8SLVP1104I:2GHz 1:4 LVPECL 4Lines output, 2GHz with your sample specification is same, but PIN define has a little bit different
Sincerely
Darrin