This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220: Handling disconnect events when calling sl_Select() with an infinite timeout period in FreeRTOS

Part Number: CC3220


We're running our application under FreeRTOS on a CC3220SF.   Because we can't use trigger mode in FreeRTOS, and because we need to minimize the idle current, we're using an infinite timeout period when calling sl_Select(). That is, we set the timeout parameter to NULL.

However, I discovered that if the WiFi network is disconnected (that is, if a disconnect event occurs), sl_Select() remains blocked instead of returning.  What would be the best way to handle such situations?  Is there some way we can make sl_Select() return when a disconnect occurs?

  • Hi Velasco,

    Is it possible to structure your application as is done in the thread linked below? This would require creating a finite timeout for sl_select, which is called in a loop and exiting based on the return value.

    e2e.ti.com/.../373703
  • Only as an absolute last resort. We want to minimize the power consumption by sleeping for as long as possible.  Having to repeatedly poll sl_Select()'s return value would naturally defeat this approach.

  • Just following up on this. As I said, using a finite timeout would be an absolute last resort, since we do want to minimize the power consumption.

    Would calling sl_Stop() and then sl_Start() upon detecting a disconnect event be a reasonable approach, for example? Any other methods?
  • Hi Velasco,

    It would not be good practice to call sl_stop and sl_start. This is because the SL host driver uses objects to synchronize certain events via pending and posting a semaphore. Calling sl_stop and sl_start will not reset the state of these objects--which can cause problems when the host starts to communicate with the NWP again.

    So, the safest course of action would be to assign a finite timeout when calling sl_select--long enough to take advantage of power savings, but short enough to recover if a disconnect event occurs.