This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC3200MOD: CC3200MOD

Part Number: CC3200MOD
Other Parts Discussed in Thread: CC3200, UNIFLASH

Tool/software: Code Composer Studio

Hi,

I am using cc3200mod with my custom board and debugging it with the help of CC3200 LaunchpadXL. I amusing CCS 6 version with SDK1.3.0. I have modified HTTP client demo project and flashed .bin file to the c3200mod. After flash I have removed SOP2 jumper and reset the board but the device didn't start as expected. It is fine when I am debugging it but not working with Flash. I have also tried flashing .hex file  to the CC3200MOD but result is same as before. 

I have formatted the flash with 1MB option and programmed with latest service pack and after that flashed the .bin and .hex file with Uniflash. I didn't get any error while flashing with Uniflash.

Can anyone please tell me what I am missing or what should I do to make it work with Flash? 

Thanks and regards,

Nikhil