Hi,
I was working through the demo SSL application provided with the CC3200 SDK_1.3.0. I have the wifi setup and downloaded the .der certificate along with the .bin application program. But its not working. This is what i'm getting on the serial terminal:
...............
Connection established w/ AP and IP is aquired
Device couldn't connect to Google server
Error [-370] at line [876] in function [main]
I was following the PDF document relating to the SSL demo. The document says to download the Equifax CA. I exported it to a folder and when opened it says "This certificate has been revoked by its certification authority". is this a problem?
I also tried GeoTrust Global CA too. it didn't work either. what am I doing wrong?
CC3200 can connect to the internet and also the time is set correctly
these are the setup:
#define APPLICATION_NAME "SSL" #define APPLICATION_VERSION "1.1.1" #define SERVER_NAME "www.google.com" #define GOOGLE_DST_PORT 443 #define SL_SSL_CA_CERT_FILE_NAME "/cert/129.der" #define DATE 14 /* Current Date */ #define MONTH 6 /* Month 1-12 */ #define YEAR 2018 /* Current year */ #define HOUR 17 /* Time - hours */ #define MINUTE 23 /* Time - minutes */ #define SECOND 0 /* Time - seconds */
here's the main() funtion:
void main()
{
long lRetVal = -1;
//
// Initialize board configuration
//
BoardInit();
PinMuxConfig();
//#ifndef NOTERM
InitTerm();
//#endif
lRetVal = ssl();
if(lRetVal < 0)
{
ERR_PRINT(lRetVal);
}
//
// power off network processor
//
sl_Stop(SL_STOP_TIMEOUT);
LOOP_FOREVER();
}
//*****************************************************************************
//
// Close the Doxygen group.
//! @}
//
//*****************************************************************************