This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DRA745: WL1837MOD: hciattach Initialization timed out.

Part Number: DRA745
Other Parts Discussed in Thread: WL1837

Tool/software: Linux

Bring up bluetooth (wl1837 : NF3107) on dra74x
-------------------------------------------------------------------

We are able to bring up WLAN and facing problem with bluetooth bring up.

We have our custom board (J6) which is connected to MAX14830ETM+ using SPI interface and
the BT module is connected with MAX chip UART port 1 (ttyMAX1) as follows,

          SPI                                          ttyMAX1
J6 -----------  MAX14830ETM+  ------------------- NF31087

We have manually made the BT_EN pin high always (from u-boot).

When we are trying to attach the BT module (hciattach /dev/ttyMAX1 texas 115200 noflow),
getting the "Initialization timed out." error. When We probe it (from MAX chip),
RTS :   Toggling
              High   : when we do the hciattach
              LOW  : After getting "Initialization timed out" error.
CTS :     LOW always (no response).

The results are attached here (bt_log.txt).

We have also followed the following link and tried with changing the latest TIInit_11.8.32.bts file but does not help.
e2e.ti.com/.../683824

We stuck here and please help us to go forward.

Thanks,
LAL


======================================================================================
root@dra7xx-evm:~# hciattach /dev/ttyMAX1 texas 115200 flow
	Initialization timed out.

======================================================================================
root@dra7xx-evm:~# hciattach /dev/ttyMAX1 texas 115200 noflow                                                                                  
	Found a Texas Instruments' chip!
	Firmware file : /lib/firmware/TIInit_11.8.32.bts
	Loaded BTS script version 1
	texas: changing baud rate to 3000000, flow control to 1
	Initialization timed out.
=======================================================================================
root@dra7xx-evm:~# hciattach /dev/ttyMAX1 any 115200 noflow                                                                                    
	[   49.932218] Bluetooth: HCI UART driver ver 2.3
	[   49.936717] Bluetooth: HCI UART protocol H4 registered
	[   49.942333] Bluetooth: HCI UART protocol LL registered
	[   49.950065] Bluetooth: HCI UART protocol Three-wire (H5) registered
	Device setup complete
	[   50.092684] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
	[   50.098107] Bluetooth: BNEP filters: protocol multicast
	[   50.103367] Bluetooth: BNEP socket layer initialized

root@dra7xx-evm:~# hciconfig -a
	hci0:   Type: BR/EDR  Bus: UART
		BD Address: 50:8C:B1:50:60:C5  ACL MTU: 1021:6  SCO MTU: 180:4
		UP RUNNING PSCAN 
		RX bytes:668 acl:0 sco:0 events:38 errors:0
		TX bytes:990 acl:0 sco:0 commands:38 errors:0
		Features: 0xff 0xfe 0x2d 0xfe 0xdb 0xff 0x7b 0x87
		Packet type: DM1 DM3 DM5 DH1 DH3 DH5 HV1 HV2 HV3 
		Link policy: RSWITCH HOLD SNIFF 
		Link mode: SLAVE ACCEPT 
		Name: 'dra7xx-evm-0'
		Class: 0x000100
		Service Classes: Unspecified
		Device Class: Computer, Uncategorized
		HCI Version: 4.0 (0x6)  Revision: 0x0
		LMP Version: 4.0 (0x6)  Subversion: 0xac20
		Manufacturer: Texas Instruments Inc. (13)
==========================================================================================





  • Hi,
    Can you change baud rate to 3000000 and re-test ?

    Thanks
    Saurabh
  • Hi Saurabh,

    We have tried the same, but same result.

    root@dra7xx-evm:~# hciattach /dev/ttyMAX1 texas 3000000 flow
    Initialization timed out.

    Thanks,
    LAL
  • Hi LAL,

    I suggest you also probe the TX and RX lines on the UART.
    In addition, it would be very useful to take BT FW logs (www.ti.com/.../swau058d.pdf). The FW logs woul show, if the BT controller has detected a UART connection and if there is any traffic..

    Since, you are using a SPI-UART translator and the Bluez driver assumes a UART (virtual in your case) interface, please make sure the SPI-UART driver and the configuration on the host are working correctly..

    Thanks
  • Hi,

    I have pulled out the MAX chip port 0 pins (Tx, Rx, RTS and CTS ) and connects with PC using USB to TTL driver (YP-05).
    The connection as follows,

    MAX_Tx   -----> USB_TTL_Rx
    MAX_Rx   -----> USB_TTL_Tx
    MAX_RTS  -----> USB_TTL_CTS
    MAX_CTS  -----> USB_TTL_RTS

    I am able transfer the data between maxchip and PC without flow control.

    With flow control (Tested with minicom) :
        Able to transfer the data from PC to MAX Chip.
        Unable to transfer the data from MAX Chip to PC.

    Unable to transfer the data from MAX Chip to PC :
    ======================================
    When I probe it, MAX chip cts pin is low by default, but max chip does not start transferring the data.
    When I manually toggle the MAX chip CTS pin, MAX chip starts to transfer the data.
    Actually, MAX chip is expecting the CTS pin to toggle for transferring the data but it is supposed to send data when CTS is low.

    I have attached here the Max driver code (max310x.c), Please look at the attachment.

    Please guide us to move forward.

    Thanks,
    Lal


    /*
     *  Maxim (Dallas) MAX3107/8/9, MAX14830 serial driver
     *
     *  Copyright (C) 2012-2014 Alexander Shiyan <shc_work@mail.ru>
     *
     *  Based on max3100.c, by Christian Pellegrin <chripell@evolware.org>
     *  Based on max3110.c, by Feng Tang <feng.tang@intel.com>
     *  Based on max3107.c, by Aavamobile
     *
     *  This program is free software; you can redistribute it and/or modify
     *  it under the terms of the GNU General Public License as published by
     *  the Free Software Foundation; either version 2 of the License, or
     *  (at your option) any later version.
     */
    
    #include <linux/bitops.h>
    #include <linux/clk.h>
    #include <linux/delay.h>
    #include <linux/device.h>
    #include <linux/gpio.h>
    #include <linux/module.h>
    #include <linux/of.h>
    #include <linux/of_device.h>
    #include <linux/regmap.h>
    #include <linux/serial_core.h>
    #include <linux/serial.h>
    #include <linux/tty.h>
    #include <linux/tty_flip.h>
    #include <linux/spi/spi.h>
    #include <linux/uaccess.h>
    
    #define MAX310X_NAME			"max310x"
    #define MAX310X_MAJOR			204
    #define MAX310X_MINOR			209
    
    /* MAX310X register definitions */
    #define MAX310X_RHR_REG			(0x00) /* RX FIFO */
    #define MAX310X_THR_REG			(0x00) /* TX FIFO */
    #define MAX310X_IRQEN_REG		(0x01) /* IRQ enable */
    #define MAX310X_IRQSTS_REG		(0x02) /* IRQ status */
    #define MAX310X_LSR_IRQEN_REG		(0x03) /* LSR IRQ enable */
    #define MAX310X_LSR_IRQSTS_REG		(0x04) /* LSR IRQ status */
    #define MAX310X_REG_05			(0x05)
    #define MAX310X_SPCHR_IRQEN_REG		MAX310X_REG_05 /* Special char IRQ en */
    #define MAX310X_SPCHR_IRQSTS_REG	(0x06) /* Special char IRQ status */
    #define MAX310X_STS_IRQEN_REG		(0x07) /* Status IRQ enable */
    #define MAX310X_STS_IRQSTS_REG		(0x08) /* Status IRQ status */
    #define MAX310X_MODE1_REG		(0x09) /* MODE1 */
    #define MAX310X_MODE2_REG		(0x0a) /* MODE2 */
    #define MAX310X_LCR_REG			(0x0b) /* LCR */
    #define MAX310X_RXTO_REG		(0x0c) /* RX timeout */
    #define MAX310X_HDPIXDELAY_REG		(0x0d) /* Auto transceiver delays */
    #define MAX310X_IRDA_REG		(0x0e) /* IRDA settings */
    #define MAX310X_FLOWLVL_REG		(0x0f) /* Flow control levels */
    #define MAX310X_FIFOTRIGLVL_REG		(0x10) /* FIFO IRQ trigger levels */
    #define MAX310X_TXFIFOLVL_REG		(0x11) /* TX FIFO level */
    #define MAX310X_RXFIFOLVL_REG		(0x12) /* RX FIFO level */
    #define MAX310X_FLOWCTRL_REG		(0x13) /* Flow control */
    #define MAX310X_XON1_REG		(0x14) /* XON1 character */
    #define MAX310X_XON2_REG		(0x15) /* XON2 character */
    #define MAX310X_XOFF1_REG		(0x16) /* XOFF1 character */
    #define MAX310X_XOFF2_REG		(0x17) /* XOFF2 character */
    #define MAX310X_GPIOCFG_REG		(0x18) /* GPIO config */
    #define MAX310X_GPIODATA_REG		(0x19) /* GPIO data */
    #define MAX310X_PLLCFG_REG		(0x1a) /* PLL config */
    #define MAX310X_BRGCFG_REG		(0x1b) /* Baud rate generator conf */
    #define MAX310X_BRGDIVLSB_REG		(0x1c) /* Baud rate divisor LSB */
    #define MAX310X_BRGDIVMSB_REG		(0x1d) /* Baud rate divisor MSB */
    #define MAX310X_CLKSRC_REG		(0x1e) /* Clock source */
    #define MAX310X_REG_1F			(0x1f)
    
    #define MAX310X_REVID_REG		MAX310X_REG_1F /* Revision ID */
    
    #define MAX310X_GLOBALIRQ_REG		MAX310X_REG_1F /* Global IRQ (RO) */
    #define MAX310X_GLOBALCMD_REG		MAX310X_REG_1F /* Global Command (WO) */
    
    /* Extended registers */
    #define MAX310X_REVID_EXTREG		MAX310X_REG_05 /* Revision ID */
    
    /* IRQ register bits */
    #define MAX310X_IRQ_LSR_BIT		(1 << 0) /* LSR interrupt */
    #define MAX310X_IRQ_SPCHR_BIT		(1 << 1) /* Special char interrupt */
    #define MAX310X_IRQ_STS_BIT		(1 << 2) /* Status interrupt */
    #define MAX310X_IRQ_RXFIFO_BIT		(1 << 3) /* RX FIFO interrupt */
    #define MAX310X_IRQ_TXFIFO_BIT		(1 << 4) /* TX FIFO interrupt */
    #define MAX310X_IRQ_TXEMPTY_BIT		(1 << 5) /* TX FIFO empty interrupt */
    #define MAX310X_IRQ_RXEMPTY_BIT		(1 << 6) /* RX FIFO empty interrupt */
    #define MAX310X_IRQ_CTS_BIT		(1 << 7) /* CTS interrupt */
    
    /* LSR register bits */
    #define MAX310X_LSR_RXTO_BIT		(1 << 0) /* RX timeout */
    #define MAX310X_LSR_RXOVR_BIT		(1 << 1) /* RX overrun */
    #define MAX310X_LSR_RXPAR_BIT		(1 << 2) /* RX parity error */
    #define MAX310X_LSR_FRERR_BIT		(1 << 3) /* Frame error */
    #define MAX310X_LSR_RXBRK_BIT		(1 << 4) /* RX break */
    #define MAX310X_LSR_RXNOISE_BIT		(1 << 5) /* RX noise */
    #define MAX310X_LSR_CTS_BIT		(1 << 7) /* CTS pin state */
    
    /* Special character register bits */
    #define MAX310X_SPCHR_XON1_BIT		(1 << 0) /* XON1 character */
    #define MAX310X_SPCHR_XON2_BIT		(1 << 1) /* XON2 character */
    #define MAX310X_SPCHR_XOFF1_BIT		(1 << 2) /* XOFF1 character */
    #define MAX310X_SPCHR_XOFF2_BIT		(1 << 3) /* XOFF2 character */
    #define MAX310X_SPCHR_BREAK_BIT		(1 << 4) /* RX break */
    #define MAX310X_SPCHR_MULTIDROP_BIT	(1 << 5) /* 9-bit multidrop addr char */
    
    /* Status register bits */
    #define MAX310X_STS_GPIO0_BIT		(1 << 0) /* GPIO 0 interrupt */
    #define MAX310X_STS_GPIO1_BIT		(1 << 1) /* GPIO 1 interrupt */
    #define MAX310X_STS_GPIO2_BIT		(1 << 2) /* GPIO 2 interrupt */
    #define MAX310X_STS_GPIO3_BIT		(1 << 3) /* GPIO 3 interrupt */
    #define MAX310X_STS_CLKREADY_BIT	(1 << 5) /* Clock ready */
    #define MAX310X_STS_SLEEP_BIT		(1 << 6) /* Sleep interrupt */
    
    /* MODE1 register bits */
    #define MAX310X_MODE1_RXDIS_BIT		(1 << 0) /* RX disable */
    #define MAX310X_MODE1_TXDIS_BIT		(1 << 1) /* TX disable */
    #define MAX310X_MODE1_TXHIZ_BIT		(1 << 2) /* TX pin three-state */
    #define MAX310X_MODE1_RTSHIZ_BIT	(1 << 3) /* RTS pin three-state */
    #define MAX310X_MODE1_TRNSCVCTRL_BIT	(1 << 4) /* Transceiver ctrl enable */
    #define MAX310X_MODE1_FORCESLEEP_BIT	(1 << 5) /* Force sleep mode */
    #define MAX310X_MODE1_AUTOSLEEP_BIT	(1 << 6) /* Auto sleep enable */
    #define MAX310X_MODE1_IRQSEL_BIT	(1 << 7) /* IRQ pin enable */
    
    /* MODE2 register bits */
    #define MAX310X_MODE2_RST_BIT		(1 << 0) /* Chip reset */
    #define MAX310X_MODE2_FIFORST_BIT	(1 << 1) /* FIFO reset */
    #define MAX310X_MODE2_RXTRIGINV_BIT	(1 << 2) /* RX FIFO INT invert */
    #define MAX310X_MODE2_RXEMPTINV_BIT	(1 << 3) /* RX FIFO empty INT invert */
    #define MAX310X_MODE2_SPCHR_BIT		(1 << 4) /* Special chr detect enable */
    #define MAX310X_MODE2_LOOPBACK_BIT	(1 << 5) /* Internal loopback enable */
    #define MAX310X_MODE2_MULTIDROP_BIT	(1 << 6) /* 9-bit multidrop enable */
    #define MAX310X_MODE2_ECHOSUPR_BIT	(1 << 7) /* ECHO suppression enable */
    
    /* LCR register bits */
    #define MAX310X_LCR_LENGTH0_BIT		(1 << 0) /* Word length bit 0 */
    #define MAX310X_LCR_LENGTH1_BIT		(1 << 1) /* Word length bit 1
    						  *
    						  * Word length bits table:
    						  * 00 -> 5 bit words
    						  * 01 -> 6 bit words
    						  * 10 -> 7 bit words
    						  * 11 -> 8 bit words
    						  */
    #define MAX310X_LCR_STOPLEN_BIT		(1 << 2) /* STOP length bit
    						  *
    						  * STOP length bit table:
    						  * 0 -> 1 stop bit
    						  * 1 -> 1-1.5 stop bits if
    						  *      word length is 5,
    						  *      2 stop bits otherwise
    						  */
    #define MAX310X_LCR_PARITY_BIT		(1 << 3) /* Parity bit enable */
    #define MAX310X_LCR_EVENPARITY_BIT	(1 << 4) /* Even parity bit enable */
    #define MAX310X_LCR_FORCEPARITY_BIT	(1 << 5) /* 9-bit multidrop parity */
    #define MAX310X_LCR_TXBREAK_BIT		(1 << 6) /* TX break enable */
    #define MAX310X_LCR_RTS_BIT		(1 << 7) /* RTS pin control */
    #define MAX310X_LCR_WORD_LEN_5		(0x00)
    #define MAX310X_LCR_WORD_LEN_6		(0x01)
    #define MAX310X_LCR_WORD_LEN_7		(0x02)
    #define MAX310X_LCR_WORD_LEN_8		(0x03)
    
    /* IRDA register bits */
    #define MAX310X_IRDA_IRDAEN_BIT		(1 << 0) /* IRDA mode enable */
    #define MAX310X_IRDA_SIR_BIT		(1 << 1) /* SIR mode enable */
    
    /* Flow control trigger level register masks */
    #define MAX310X_FLOWLVL_HALT_MASK	(0x000f) /* Flow control halt level */
    #define MAX310X_FLOWLVL_RES_MASK	(0x00f0) /* Flow control resume level */
    #define MAX310X_FLOWLVL_HALT(words)	((words / 8) & 0x0f)
    #define MAX310X_FLOWLVL_RES(words)	(((words / 8) & 0x0f) << 4)
    
    /* FIFO interrupt trigger level register masks */
    #define MAX310X_FIFOTRIGLVL_TX_MASK	(0x0f) /* TX FIFO trigger level */
    #define MAX310X_FIFOTRIGLVL_RX_MASK	(0xf0) /* RX FIFO trigger level */
    #define MAX310X_FIFOTRIGLVL_TX(words)	((words / 8) & 0x0f)
    #define MAX310X_FIFOTRIGLVL_RX(words)	(((words / 8) & 0x0f) << 4)
    
    /* Flow control register bits */
    #define MAX310X_FLOWCTRL_AUTORTS_BIT	(1 << 0) /* Auto RTS flow ctrl enable */
    #define MAX310X_FLOWCTRL_AUTOCTS_BIT	(1 << 1) /* Auto CTS flow ctrl enable */
    #define MAX310X_FLOWCTRL_GPIADDR_BIT	(1 << 2) /* Enables that GPIO inputs
    						  * are used in conjunction with
    						  * XOFF2 for definition of
    						  * special character */
    #define MAX310X_FLOWCTRL_SWFLOWEN_BIT	(1 << 3) /* Auto SW flow ctrl enable */
    #define MAX310X_FLOWCTRL_SWFLOW0_BIT	(1 << 4) /* SWFLOW bit 0 */
    #define MAX310X_FLOWCTRL_SWFLOW1_BIT	(1 << 5) /* SWFLOW bit 1
    						  *
    						  * SWFLOW bits 1 & 0 table:
    						  * 00 -> no transmitter flow
    						  *       control
    						  * 01 -> receiver compares
    						  *       XON2 and XOFF2
    						  *       and controls
    						  *       transmitter
    						  * 10 -> receiver compares
    						  *       XON1 and XOFF1
    						  *       and controls
    						  *       transmitter
    						  * 11 -> receiver compares
    						  *       XON1, XON2, XOFF1 and
    						  *       XOFF2 and controls
    						  *       transmitter
    						  */
    #define MAX310X_FLOWCTRL_SWFLOW2_BIT	(1 << 6) /* SWFLOW bit 2 */
    #define MAX310X_FLOWCTRL_SWFLOW3_BIT	(1 << 7) /* SWFLOW bit 3
    						  *
    						  * SWFLOW bits 3 & 2 table:
    						  * 00 -> no received flow
    						  *       control
    						  * 01 -> transmitter generates
    						  *       XON2 and XOFF2
    						  * 10 -> transmitter generates
    						  *       XON1 and XOFF1
    						  * 11 -> transmitter generates
    						  *       XON1, XON2, XOFF1 and
    						  *       XOFF2
    						  */
    
    /* PLL configuration register masks */
    #define MAX310X_PLLCFG_PREDIV_MASK	(0x3f) /* PLL predivision value */
    #define MAX310X_PLLCFG_PLLFACTOR_MASK	(0xc0) /* PLL multiplication factor */
    
    /* Baud rate generator configuration register bits */
    #define MAX310X_BRGCFG_2XMODE_BIT	(1 << 4) /* Double baud rate */
    #define MAX310X_BRGCFG_4XMODE_BIT	(1 << 5) /* Quadruple baud rate */
    
    /* Clock source register bits */
    #define MAX310X_CLKSRC_CRYST_BIT	(1 << 1) /* Crystal osc enable */
    #define MAX310X_CLKSRC_PLL_BIT		(1 << 2) /* PLL enable */
    #define MAX310X_CLKSRC_PLLBYP_BIT	(1 << 3) /* PLL bypass */
    #define MAX310X_CLKSRC_EXTCLK_BIT	(1 << 4) /* External clock enable */
    #define MAX310X_CLKSRC_CLK2RTS_BIT	(1 << 7) /* Baud clk to RTS pin */
    
    /* Global commands */
    #define MAX310X_EXTREG_ENBL		(0xce)
    #define MAX310X_EXTREG_DSBL		(0xcd)
    
    /* Misc definitions */
    #define MAX310X_FIFO_SIZE		(128)
    #define MAX310x_REV_MASK		(0xfc)
    
    /* MAX3107 specific */
    #define MAX3107_REV_ID			(0xa0)
    
    /* MAX3109 specific */
    #define MAX3109_REV_ID			(0xc0)
    
    /* MAX14830 specific */
    #define MAX14830_BRGCFG_CLKDIS_BIT	(1 << 6) /* Clock Disable */
    #define MAX14830_REV_ID			(0xb0)
    
    struct max310x_devtype {
    	char	name[9];
    	int	nr;
    	int	(*detect)(struct device *);
    	void	(*power)(struct uart_port *, int);
    };
    
    struct max310x_one {
    	struct uart_port	port;
    	struct work_struct	tx_work;
    	struct work_struct	md_work;
    };
    
    struct max310x_port {
    	struct uart_driver	uart;
    	struct max310x_devtype	*devtype;
    	struct regmap		*regmap;
    	struct mutex		mutex;
    	struct clk		*clk;
    #ifdef CONFIG_GPIOLIB
    	struct gpio_chip	gpio;
    #endif
    	struct max310x_one	p[0];
    };
    
    static u8 max310x_port_read(struct uart_port *port, u8 reg)
    {
    	struct max310x_port *s = dev_get_drvdata(port->dev);
    	unsigned int val = 0;
    
    	regmap_read(s->regmap, port->iobase + reg, &val);
    
    	return val;
    }
    
    static void max310x_port_write(struct uart_port *port, u8 reg, u8 val)
    {
    	struct max310x_port *s = dev_get_drvdata(port->dev);
    
    	regmap_write(s->regmap, port->iobase + reg, val);
    }
    
    static void max310x_port_update(struct uart_port *port, u8 reg, u8 mask, u8 val)
    {
    	struct max310x_port *s = dev_get_drvdata(port->dev);
    
    	regmap_update_bits(s->regmap, port->iobase + reg, mask, val);
    }
    
    static int max3107_detect(struct device *dev)
    {
    	struct max310x_port *s = dev_get_drvdata(dev);
    	unsigned int val = 0;
    	int ret;
    
    	ret = regmap_read(s->regmap, MAX310X_REVID_REG, &val);
    	if (ret)
    		return ret;
    
    	if (((val & MAX310x_REV_MASK) != MAX3107_REV_ID)) {
    		dev_err(dev,
    			"%s ID 0x%02x does not match\n", s->devtype->name, val);
    		return -ENODEV;
    	}
    
    	return 0;
    }
    
    static int max3108_detect(struct device *dev)
    {
    	struct max310x_port *s = dev_get_drvdata(dev);
    	unsigned int val = 0;
    	int ret;
    
    	/* MAX3108 have not REV ID register, we just check default value
    	 * from clocksource register to make sure everything works.
    	 */
    	ret = regmap_read(s->regmap, MAX310X_CLKSRC_REG, &val);
    	if (ret)
    		return ret;
    
    	if (val != (MAX310X_CLKSRC_EXTCLK_BIT | MAX310X_CLKSRC_PLLBYP_BIT)) {
    		dev_err(dev, "%s not present\n", s->devtype->name);
    		return -ENODEV;
    	}
    
    	return 0;
    }
    
    static int max3109_detect(struct device *dev)
    {
    	struct max310x_port *s = dev_get_drvdata(dev);
    	unsigned int val = 0;
    	int ret;
    
    	ret = regmap_write(s->regmap, MAX310X_GLOBALCMD_REG,
    			   MAX310X_EXTREG_ENBL);
    	if (ret)
    		return ret;
    
    	regmap_read(s->regmap, MAX310X_REVID_EXTREG, &val);
    	regmap_write(s->regmap, MAX310X_GLOBALCMD_REG, MAX310X_EXTREG_DSBL);
    	if (((val & MAX310x_REV_MASK) != MAX3109_REV_ID)) {
    		dev_err(dev,
    			"%s ID 0x%02x does not match\n", s->devtype->name, val);
    		return -ENODEV;
    	}
    
    	return 0;
    }
    
    static void max310x_power(struct uart_port *port, int on)
    {
    	max310x_port_update(port, MAX310X_MODE1_REG,
    			    MAX310X_MODE1_FORCESLEEP_BIT,
    			    on ? 0 : MAX310X_MODE1_FORCESLEEP_BIT);
    	if (on)
    		msleep(50);
    }
    
    static int max14830_detect(struct device *dev)
    {
    	struct max310x_port *s = dev_get_drvdata(dev);
    	unsigned int val = 0;
    	int ret;
    
    	ret = regmap_write(s->regmap, MAX310X_GLOBALCMD_REG,
    			   MAX310X_EXTREG_ENBL);
    	if (ret)
    		return ret;
    	
    	regmap_read(s->regmap, MAX310X_REVID_EXTREG, &val);
    	regmap_write(s->regmap, MAX310X_GLOBALCMD_REG, MAX310X_EXTREG_DSBL);
    	if (((val & MAX310x_REV_MASK) != MAX14830_REV_ID)) {
    		dev_err(dev,
    			"%s ID 0x%02x does not match\n", s->devtype->name, val);
    		return -ENODEV;
    	}
    
    	return 0;
    }
    
    static void max14830_power(struct uart_port *port, int on)
    {
    	max310x_port_update(port, MAX310X_BRGCFG_REG,
    			    MAX14830_BRGCFG_CLKDIS_BIT,
    			    on ? 0 : MAX14830_BRGCFG_CLKDIS_BIT);
    	if (on)
    		msleep(50);
    }
    
    static const struct max310x_devtype max3107_devtype = {
    	.name	= "MAX3107",
    	.nr	= 1,
    	.detect	= max3107_detect,
    	.power	= max310x_power,
    };
    
    static const struct max310x_devtype max3108_devtype = {
    	.name	= "MAX3108",
    	.nr	= 1,
    	.detect	= max3108_detect,
    	.power	= max310x_power,
    };
    
    static const struct max310x_devtype max3109_devtype = {
    	.name	= "MAX3109",
    	.nr	= 2,
    	.detect	= max3109_detect,
    	.power	= max310x_power,
    };
    
    static const struct max310x_devtype max14830_devtype = {
    	.name	= "MAX14830",
    	.nr	= 4,
    	.detect	= max14830_detect,
    	.power	= max14830_power,
    };
    
    static bool max310x_reg_writeable(struct device *dev, unsigned int reg)
    {
    	switch (reg & 0x1f) {
    	case MAX310X_IRQSTS_REG:
    	case MAX310X_LSR_IRQSTS_REG:
    	case MAX310X_SPCHR_IRQSTS_REG:
    	case MAX310X_STS_IRQSTS_REG:
    	case MAX310X_TXFIFOLVL_REG:
    	case MAX310X_RXFIFOLVL_REG:
    		return false;
    	default:
    		break;
    	}
    
    	return true;
    }
    
    static bool max310x_reg_volatile(struct device *dev, unsigned int reg)
    {
    	switch (reg & 0x1f) {
    	case MAX310X_RHR_REG:
    	case MAX310X_IRQSTS_REG:
    	case MAX310X_LSR_IRQSTS_REG:
    	case MAX310X_SPCHR_IRQSTS_REG:
    	case MAX310X_STS_IRQSTS_REG:
    	case MAX310X_TXFIFOLVL_REG:
    	case MAX310X_RXFIFOLVL_REG:
    	case MAX310X_GPIODATA_REG:
    	case MAX310X_BRGDIVLSB_REG:
    	case MAX310X_REG_05:
    	case MAX310X_REG_1F:
    		return true;
    	default:
    		break;
    	}
    
    	return false;
    }
    
    static bool max310x_reg_precious(struct device *dev, unsigned int reg)
    {
    	switch (reg & 0x1f) {
    	case MAX310X_RHR_REG:
    	case MAX310X_IRQSTS_REG:
    	case MAX310X_SPCHR_IRQSTS_REG:
    	case MAX310X_STS_IRQSTS_REG:
    		return true;
    	default:
    		break;
    	}
    
    	return false;
    }
    
    static int max310x_set_baud(struct uart_port *port, int baud)
    {
    	unsigned int mode = 0, clk = port->uartclk, div = clk / baud;
    
    	/* Check for minimal value for divider */
    	if (div < 16)
    		div = 16;
    
    	if (clk % baud && (div / 16) < 0x8000) {
    		/* Mode x2 */
    		mode = MAX310X_BRGCFG_2XMODE_BIT;
    		clk = port->uartclk * 2;
    		div = clk / baud;
    
    		if (clk % baud && (div / 16) < 0x8000) {
    			/* Mode x4 */
    			mode = MAX310X_BRGCFG_4XMODE_BIT;
    			clk = port->uartclk * 4;
    			div = clk / baud;
    		}
    	}
    
    	max310x_port_write(port, MAX310X_BRGDIVMSB_REG, (div / 16) >> 8);
    	max310x_port_write(port, MAX310X_BRGDIVLSB_REG, div / 16);
    	max310x_port_write(port, MAX310X_BRGCFG_REG, (div % 16) | mode);
    
    	return DIV_ROUND_CLOSEST(clk, div);
    }
    
    static int max310x_update_best_err(unsigned long f, long *besterr)
    {
    	/* Use baudrate 115200 for calculate error */
    	long err = f % (115200 * 16);
    
    	if ((*besterr < 0) || (*besterr > err)) {
    		*besterr = err;
    		return 0;
    	}
    
    	return 1;
    }
    
    static int max310x_set_ref_clk(struct max310x_port *s, unsigned long freq,
    			       bool xtal)
    {
    	unsigned int div, clksrc, pllcfg = 0;
    	long besterr = -1;
    	unsigned long fdiv, fmul, bestfreq = freq;
    
    	/* First, update error without PLL */
    	max310x_update_best_err(freq, &besterr);
    
    	/* Try all possible PLL dividers */
    	for (div = 1; (div <= 63) && besterr; div++) {
    		fdiv = DIV_ROUND_CLOSEST(freq, div);
    
    		/* Try multiplier 6 */
    		fmul = fdiv * 6;
    		if ((fdiv >= 500000) && (fdiv <= 800000))
    			if (!max310x_update_best_err(fmul, &besterr)) {
    				pllcfg = (0 << 6) | div;
    				bestfreq = fmul;
    			}
    		/* Try multiplier 48 */
    		fmul = fdiv * 48;
    		if ((fdiv >= 850000) && (fdiv <= 1200000))
    			if (!max310x_update_best_err(fmul, &besterr)) {
    				pllcfg = (1 << 6) | div;
    				bestfreq = fmul;
    			}
    		/* Try multiplier 96 */
    		fmul = fdiv * 96;
    		if ((fdiv >= 425000) && (fdiv <= 1000000))
    			if (!max310x_update_best_err(fmul, &besterr)) {
    				pllcfg = (2 << 6) | div;
    				bestfreq = fmul;
    			}
    		/* Try multiplier 144 */
    		fmul = fdiv * 144;
    		if ((fdiv >= 390000) && (fdiv <= 667000))
    			if (!max310x_update_best_err(fmul, &besterr)) {
    				pllcfg = (3 << 6) | div;
    				bestfreq = fmul;
    			}
    	}
    
    	/* Configure clock source */
    	clksrc = xtal ? MAX310X_CLKSRC_CRYST_BIT : MAX310X_CLKSRC_EXTCLK_BIT;
    
    	/* Configure PLL */
    	if (pllcfg) {
    		clksrc |= MAX310X_CLKSRC_PLL_BIT;
    		regmap_write(s->regmap, MAX310X_PLLCFG_REG, pllcfg);
    	} else
    		clksrc |= MAX310X_CLKSRC_PLLBYP_BIT;
    
    	regmap_write(s->regmap, MAX310X_CLKSRC_REG, clksrc);
    
    	/* Wait for crystal */
    	if (pllcfg && xtal)
    		msleep(10);
    
    	return (int)bestfreq;
    }
    
    static void max310x_handle_rx(struct uart_port *port, unsigned int rxlen)
    {
    	unsigned int sts, ch, flag;
    
    	if (unlikely(rxlen >= port->fifosize)) {
    		dev_warn_ratelimited(port->dev,
    				     "Port %i: Possible RX FIFO overrun\n",
    				     port->line);
    		port->icount.buf_overrun++;
    		/* Ensure sanity of RX level */
    		rxlen = port->fifosize;
    	}
    
    	while (rxlen--) {
    		ch = max310x_port_read(port, MAX310X_RHR_REG);
    		sts = max310x_port_read(port, MAX310X_LSR_IRQSTS_REG);
    
    		sts &= MAX310X_LSR_RXPAR_BIT | MAX310X_LSR_FRERR_BIT |
    		       MAX310X_LSR_RXOVR_BIT | MAX310X_LSR_RXBRK_BIT;
    
    		port->icount.rx++;
    		flag = TTY_NORMAL;
    
    		if (unlikely(sts)) {
    			if (sts & MAX310X_LSR_RXBRK_BIT) {
    				port->icount.brk++;
    				if (uart_handle_break(port))
    					continue;
    			} else if (sts & MAX310X_LSR_RXPAR_BIT)
    				port->icount.parity++;
    			else if (sts & MAX310X_LSR_FRERR_BIT)
    				port->icount.frame++;
    			else if (sts & MAX310X_LSR_RXOVR_BIT)
    				port->icount.overrun++;
    
    			sts &= port->read_status_mask;
    			if (sts & MAX310X_LSR_RXBRK_BIT)
    				flag = TTY_BREAK;
    			else if (sts & MAX310X_LSR_RXPAR_BIT)
    				flag = TTY_PARITY;
    			else if (sts & MAX310X_LSR_FRERR_BIT)
    				flag = TTY_FRAME;
    			else if (sts & MAX310X_LSR_RXOVR_BIT)
    				flag = TTY_OVERRUN;
    		}
    
    		if (uart_handle_sysrq_char(port, ch))
    			continue;
    
    		if (sts & port->ignore_status_mask)
    			continue;
    
    		uart_insert_char(port, sts, MAX310X_LSR_RXOVR_BIT, ch, flag);
    	}
    
    	tty_flip_buffer_push(&port->state->port);
    }
    
    static void max310x_handle_tx(struct uart_port *port)
    {
    	struct circ_buf *xmit = &port->state->xmit;
    	unsigned int txlen, to_send;
    
    	if (unlikely(port->x_char)) {
    		max310x_port_write(port, MAX310X_THR_REG, port->x_char);
    		port->icount.tx++;
    		port->x_char = 0;
    		return;
    	}
    
    	if (uart_circ_empty(xmit) || uart_tx_stopped(port))
    		return;
    
    	/* Get length of data pending in circular buffer */
    	to_send = uart_circ_chars_pending(xmit);
    	if (likely(to_send)) {
    		/* Limit to size of TX FIFO */
    		txlen = max310x_port_read(port, MAX310X_TXFIFOLVL_REG);
    		txlen = port->fifosize - txlen;
    		to_send = (to_send > txlen) ? txlen : to_send;
    
    		/* Add data to send */
    		port->icount.tx += to_send;
    		while (to_send--) {
    			max310x_port_write(port, MAX310X_THR_REG,
    					   xmit->buf[xmit->tail]);
    			xmit->tail = (xmit->tail + 1) & (UART_XMIT_SIZE - 1);
    		}
    	}
    
    	if (uart_circ_chars_pending(xmit) < WAKEUP_CHARS)
    		uart_write_wakeup(port);
    }
    
    static void max310x_port_irq(struct max310x_port *s, int portno)
    {
    	struct uart_port *port = &s->p[portno].port;
    
    	do {
    		unsigned int ists, lsr, rxlen;
    
    		/* Read IRQ status & RX FIFO level */
    		ists = max310x_port_read(port, MAX310X_IRQSTS_REG);
    		rxlen = max310x_port_read(port, MAX310X_RXFIFOLVL_REG);
    		if (!ists && !rxlen)
    			break;
    
    		if (ists & MAX310X_IRQ_CTS_BIT) {
    			lsr = max310x_port_read(port, MAX310X_LSR_IRQSTS_REG);
    			uart_handle_cts_change(port,
    					       !!(lsr & MAX310X_LSR_CTS_BIT));
    		}
    		if (rxlen)
    			max310x_handle_rx(port, rxlen);
    		if (ists & MAX310X_IRQ_TXEMPTY_BIT) {
    			mutex_lock(&s->mutex);
    			max310x_handle_tx(port);
    			mutex_unlock(&s->mutex);
    		}
    	} while (1);
    }
    
    static irqreturn_t max310x_ist(int irq, void *dev_id)
    {
    	struct max310x_port *s = (struct max310x_port *)dev_id;
    
    	if (s->uart.nr > 1) {
    		do {
    			unsigned int val = ~0;
    
    			WARN_ON_ONCE(regmap_read(s->regmap,
    						 MAX310X_GLOBALIRQ_REG, &val));
    			val = ((1 << s->uart.nr) - 1) & ~val;
    			if (!val)
    				break;
    			max310x_port_irq(s, fls(val) - 1);
    		} while (1);
    	} else
    		max310x_port_irq(s, 0);
    
    	return IRQ_HANDLED;
    }
    
    static void max310x_wq_proc(struct work_struct *ws)
    {
    	struct max310x_one *one = container_of(ws, struct max310x_one, tx_work);
    	struct max310x_port *s = dev_get_drvdata(one->port.dev);
    
    	mutex_lock(&s->mutex);
    	max310x_handle_tx(&one->port);
    	mutex_unlock(&s->mutex);
    }
    
    static void max310x_start_tx(struct uart_port *port)
    {
    	struct max310x_one *one = container_of(port, struct max310x_one, port);
    
    	if (!work_pending(&one->tx_work))
    		schedule_work(&one->tx_work);
    }
    
    static unsigned int max310x_tx_empty(struct uart_port *port)
    {
    	unsigned int lvl, sts;
    
    	lvl = max310x_port_read(port, MAX310X_TXFIFOLVL_REG);
    	sts = max310x_port_read(port, MAX310X_IRQSTS_REG);
    
    	return ((sts & MAX310X_IRQ_TXEMPTY_BIT) && !lvl) ? TIOCSER_TEMT : 0;
    }
    
    static unsigned int max310x_get_mctrl(struct uart_port *port)
    {
    	/* DCD and DSR are not wired and CTS/RTS is handled automatically
    	 * so just indicate DSR and CAR asserted
    	 */
    	return TIOCM_DSR | TIOCM_CAR;
    }
    
    static void max310x_md_proc(struct work_struct *ws)
    {
    	struct max310x_one *one = container_of(ws, struct max310x_one, md_work);
    
    	max310x_port_update(&one->port, MAX310X_MODE2_REG,
    			    MAX310X_MODE2_LOOPBACK_BIT,
    			    (one->port.mctrl & TIOCM_LOOP) ?
    			    MAX310X_MODE2_LOOPBACK_BIT : 0);
    }
    
    static void max310x_set_mctrl(struct uart_port *port, unsigned int mctrl)
    {
    	struct max310x_one *one = container_of(port, struct max310x_one, port);
    
    	schedule_work(&one->md_work);
    }
    
    static void max310x_break_ctl(struct uart_port *port, int break_state)
    {
    	max310x_port_update(port, MAX310X_LCR_REG,
    			    MAX310X_LCR_TXBREAK_BIT,
    			    break_state ? MAX310X_LCR_TXBREAK_BIT : 0);
    }
    
    static void max310x_set_termios(struct uart_port *port,
    				struct ktermios *termios,
    				struct ktermios *old)
    {
    	unsigned int lcr, flow = 0;
    	int baud;
    
    	/* Mask termios capabilities we don't support */
    	termios->c_cflag &= ~CMSPAR;
    
    	/* Word size */
    	switch (termios->c_cflag & CSIZE) {
    	case CS5:
    		lcr = MAX310X_LCR_WORD_LEN_5;
    		break;
    	case CS6:
    		lcr = MAX310X_LCR_WORD_LEN_6;
    		break;
    	case CS7:
    		lcr = MAX310X_LCR_WORD_LEN_7;
    		break;
    	case CS8:
    	default:
    		lcr = MAX310X_LCR_WORD_LEN_8;
    		break;
    	}
    
    	/* Parity */
    	if (termios->c_cflag & PARENB) {
    		lcr |= MAX310X_LCR_PARITY_BIT;
    		if (!(termios->c_cflag & PARODD))
    			lcr |= MAX310X_LCR_EVENPARITY_BIT;
    	}
    
    	/* Stop bits */
    	if (termios->c_cflag & CSTOPB)
    		lcr |= MAX310X_LCR_STOPLEN_BIT; /* 2 stops */
    
    	/* Update LCR register */
    	max310x_port_write(port, MAX310X_LCR_REG, lcr);
    
    	/* Set read status mask */
    	port->read_status_mask = MAX310X_LSR_RXOVR_BIT;
    	if (termios->c_iflag & INPCK)
    		port->read_status_mask |= MAX310X_LSR_RXPAR_BIT |
    					  MAX310X_LSR_FRERR_BIT;
    	if (termios->c_iflag & (IGNBRK | BRKINT | PARMRK))
    		port->read_status_mask |= MAX310X_LSR_RXBRK_BIT;
    
    	/* Set status ignore mask */
    	port->ignore_status_mask = 0;
    	if (termios->c_iflag & IGNBRK)
    		port->ignore_status_mask |= MAX310X_LSR_RXBRK_BIT;
    	if (!(termios->c_cflag & CREAD))
    		port->ignore_status_mask |= MAX310X_LSR_RXPAR_BIT |
    					    MAX310X_LSR_RXOVR_BIT |
    					    MAX310X_LSR_FRERR_BIT |
    					    MAX310X_LSR_RXBRK_BIT;
    
    	/* Configure flow control */
    	max310x_port_write(port, MAX310X_XON1_REG, termios->c_cc[VSTART]);
    	max310x_port_write(port, MAX310X_XOFF1_REG, termios->c_cc[VSTOP]);
    	if (termios->c_cflag & CRTSCTS)
    		flow |= MAX310X_FLOWCTRL_AUTOCTS_BIT |
    			MAX310X_FLOWCTRL_AUTORTS_BIT;
    	if (termios->c_iflag & IXON)
    		flow |= MAX310X_FLOWCTRL_SWFLOW3_BIT |
    			MAX310X_FLOWCTRL_SWFLOWEN_BIT;
    	if (termios->c_iflag & IXOFF)
    		flow |= MAX310X_FLOWCTRL_SWFLOW1_BIT |
    			MAX310X_FLOWCTRL_SWFLOWEN_BIT;
    	max310x_port_write(port, MAX310X_FLOWCTRL_REG, flow);
    
    	/* Get baud rate generator configuration */
    	baud = uart_get_baud_rate(port, termios, old,
    				  port->uartclk / 16 / 0xffff,
    				  port->uartclk / 4);
    
    	/* Setup baudrate generator */
    	baud = max310x_set_baud(port, baud);
    
    	/* Update timeout according to new baud rate */
    	uart_update_timeout(port, termios->c_cflag, baud);
    }
    
    static int max310x_rs485_config(struct uart_port *port,
    				struct serial_rs485 *rs485)
    {
    	unsigned int val;
    
    	if (rs485->delay_rts_before_send > 0x0f ||
    		    rs485->delay_rts_after_send > 0x0f)
    		return -ERANGE;
    
    	val = (rs485->delay_rts_before_send << 4) |
    		rs485->delay_rts_after_send;
    	max310x_port_write(port, MAX310X_HDPIXDELAY_REG, val);
    	if (rs485->flags & SER_RS485_ENABLED) {
    		max310x_port_update(port, MAX310X_MODE1_REG,
    				MAX310X_MODE1_TRNSCVCTRL_BIT,
    				MAX310X_MODE1_TRNSCVCTRL_BIT);
    		max310x_port_update(port, MAX310X_MODE2_REG,
    				MAX310X_MODE2_ECHOSUPR_BIT,
    				MAX310X_MODE2_ECHOSUPR_BIT);
    	} else {
    		max310x_port_update(port, MAX310X_MODE1_REG,
    				MAX310X_MODE1_TRNSCVCTRL_BIT, 0);
    		max310x_port_update(port, MAX310X_MODE2_REG,
    				MAX310X_MODE2_ECHOSUPR_BIT, 0);
    	}
    
    	rs485->flags &= SER_RS485_RTS_ON_SEND | SER_RS485_ENABLED;
    	memset(rs485->padding, 0, sizeof(rs485->padding));
    	port->rs485 = *rs485;
    
    	return 0;
    }
    
    static int max310x_startup(struct uart_port *port)
    {
    	struct max310x_port *s = dev_get_drvdata(port->dev);
    	unsigned int val;
    
    	s->devtype->power(port, 1);
    
    	/* Configure MODE1 register */
    	max310x_port_update(port, MAX310X_MODE1_REG,
    			    MAX310X_MODE1_TRNSCVCTRL_BIT, 0);
    
    	/* Configure MODE2 register & Reset FIFOs*/
    	val = MAX310X_MODE2_RXEMPTINV_BIT | MAX310X_MODE2_FIFORST_BIT;
    	max310x_port_write(port, MAX310X_MODE2_REG, val);
    	max310x_port_update(port, MAX310X_MODE2_REG,
    			    MAX310X_MODE2_FIFORST_BIT, 0);
    
    	/* Configure flow control levels */
    	/* Flow control halt level 96, resume level 48 */
    	max310x_port_write(port, MAX310X_FLOWLVL_REG,
    			   MAX310X_FLOWLVL_RES(48) | MAX310X_FLOWLVL_HALT(96));
    
    	/* Clear IRQ status register */
    	max310x_port_read(port, MAX310X_IRQSTS_REG);
    
    	/* Enable RX, TX, CTS change interrupts */
    	val = MAX310X_IRQ_RXEMPTY_BIT | MAX310X_IRQ_TXEMPTY_BIT;
    	max310x_port_write(port, MAX310X_IRQEN_REG, val | MAX310X_IRQ_CTS_BIT);
    
    	return 0;
    }
    
    static void max310x_shutdown(struct uart_port *port)
    {
    	struct max310x_port *s = dev_get_drvdata(port->dev);
    
    	/* Disable all interrupts */
    	max310x_port_write(port, MAX310X_IRQEN_REG, 0);
    
    	s->devtype->power(port, 0);
    }
    
    static const char *max310x_type(struct uart_port *port)
    {
    	struct max310x_port *s = dev_get_drvdata(port->dev);
    
    	return (port->type == PORT_MAX310X) ? s->devtype->name : NULL;
    }
    
    static int max310x_request_port(struct uart_port *port)
    {
    	/* Do nothing */
    	return 0;
    }
    
    static void max310x_config_port(struct uart_port *port, int flags)
    {
    	if (flags & UART_CONFIG_TYPE)
    		port->type = PORT_MAX310X;
    }
    
    static int max310x_verify_port(struct uart_port *port, struct serial_struct *s)
    {
    	if ((s->type != PORT_UNKNOWN) && (s->type != PORT_MAX310X))
    		return -EINVAL;
    	if (s->irq != port->irq)
    		return -EINVAL;
    
    	return 0;
    }
    
    static void max310x_null_void(struct uart_port *port)
    {
    	/* Do nothing */
    }
    
    static const struct uart_ops max310x_ops = {
    	.tx_empty	= max310x_tx_empty,
    	.set_mctrl	= max310x_set_mctrl,
    	.get_mctrl	= max310x_get_mctrl,
    	.stop_tx	= max310x_null_void,
    	.start_tx	= max310x_start_tx,
    	.stop_rx	= max310x_null_void,
    	.break_ctl	= max310x_break_ctl,
    	.startup	= max310x_startup,
    	.shutdown	= max310x_shutdown,
    	.set_termios	= max310x_set_termios,
    	.type		= max310x_type,
    	.request_port	= max310x_request_port,
    	.release_port	= max310x_null_void,
    	.config_port	= max310x_config_port,
    	.verify_port	= max310x_verify_port,
    };
    
    static int __maybe_unused max310x_suspend(struct device *dev)
    {
    	struct max310x_port *s = dev_get_drvdata(dev);
    	int i;
    
    	for (i = 0; i < s->uart.nr; i++) {
    		uart_suspend_port(&s->uart, &s->p[i].port);
    		s->devtype->power(&s->p[i].port, 0);
    	}
    
    	return 0;
    }
    
    static int __maybe_unused max310x_resume(struct device *dev)
    {
    	struct max310x_port *s = dev_get_drvdata(dev);
    	int i;
    
    	for (i = 0; i < s->uart.nr; i++) {
    		s->devtype->power(&s->p[i].port, 1);
    		uart_resume_port(&s->uart, &s->p[i].port);
    	}
    
    	return 0;
    }
    
    static SIMPLE_DEV_PM_OPS(max310x_pm_ops, max310x_suspend, max310x_resume);
    
    #ifdef CONFIG_GPIOLIB
    static int max310x_gpio_get(struct gpio_chip *chip, unsigned offset)
    {
    	unsigned int val;
    	struct max310x_port *s = container_of(chip, struct max310x_port, gpio);
    	struct uart_port *port = &s->p[offset / 4].port;
    
    	val = max310x_port_read(port, MAX310X_GPIODATA_REG);
    
    	return !!((val >> 4) & (1 << (offset % 4)));
    }
    
    static void max310x_gpio_set(struct gpio_chip *chip, unsigned offset, int value)
    {
    	struct max310x_port *s = container_of(chip, struct max310x_port, gpio);
    	struct uart_port *port = &s->p[offset / 4].port;
    
    	max310x_port_update(port, MAX310X_GPIODATA_REG, 1 << (offset % 4),
    			    value ? 1 << (offset % 4) : 0);
    }
    
    static int max310x_gpio_direction_input(struct gpio_chip *chip, unsigned offset)
    {
    	struct max310x_port *s = container_of(chip, struct max310x_port, gpio);
    	struct uart_port *port = &s->p[offset / 4].port;
    
    	max310x_port_update(port, MAX310X_GPIOCFG_REG, 1 << (offset % 4), 0);
    
    	return 0;
    }
    
    static int max310x_gpio_direction_output(struct gpio_chip *chip,
    					 unsigned offset, int value)
    {
    	struct max310x_port *s = container_of(chip, struct max310x_port, gpio);
    	struct uart_port *port = &s->p[offset / 4].port;
    
    	max310x_port_update(port, MAX310X_GPIODATA_REG, 1 << (offset % 4),
    			    value ? 1 << (offset % 4) : 0);
    	max310x_port_update(port, MAX310X_GPIOCFG_REG, 1 << (offset % 4),
    			    1 << (offset % 4));
    
    	return 0;
    }
    #endif
    
    static int max310x_probe(struct device *dev, struct max310x_devtype *devtype,
    			 struct regmap *regmap, int irq, unsigned long flags)
    {
    	int i, ret, fmin, fmax, freq, uartclk;
    	struct clk *clk_osc, *clk_xtal;
    	struct max310x_port *s;
    	bool xtal = false;
    
    	if (IS_ERR(regmap))
    		return PTR_ERR(regmap);
    
    	/* Alloc port structure */
    	s = devm_kzalloc(dev, sizeof(*s) +
    			 sizeof(struct max310x_one) * devtype->nr, GFP_KERNEL);
    	if (!s) {
    		dev_err(dev, "Error allocating port structure\n");
    		return -ENOMEM;
    	}
    
    	clk_osc = devm_clk_get(dev, "osc");
    	clk_xtal = devm_clk_get(dev, "xtal");
    	if (!IS_ERR(clk_osc)) {
    		s->clk = clk_osc;
    		fmin = 500000;
    		fmax = 35000000;
    	} else if (!IS_ERR(clk_xtal)) {
    		s->clk = clk_xtal;
    		fmin = 1000000;
    		fmax = 4000000;
    		xtal = true;
    	} else if (PTR_ERR(clk_osc) == -EPROBE_DEFER ||
    		   PTR_ERR(clk_xtal) == -EPROBE_DEFER) {
    		return -EPROBE_DEFER;
    	} else {
    		dev_err(dev, "Cannot get clock\n");
    		return -EINVAL;
    	}
    
    	ret = clk_prepare_enable(s->clk);
    	if (ret)
    		return ret;
    
    	freq = clk_get_rate(s->clk);
    	/* Check frequency limits */
    	if (freq < fmin || freq > fmax) {
    		ret = -ERANGE;
    		goto out_clk;
    	}
    
    	s->regmap = regmap;
    	s->devtype = devtype;
    	dev_set_drvdata(dev, s);
    
    	/* Check device to ensure we are talking to what we expect */
    	ret = devtype->detect(dev);
    	if (ret)
    		goto out_clk;
    
    	for (i = 0; i < devtype->nr; i++) {
    		unsigned int offs = i << 5;
    
    		/* Reset port */
    		regmap_write(s->regmap, MAX310X_MODE2_REG + offs,
    			     MAX310X_MODE2_RST_BIT);
    		/* Clear port reset */
    		regmap_write(s->regmap, MAX310X_MODE2_REG + offs, 0);
    
    		/* Wait for port startup */
    		do {
    			regmap_read(s->regmap,
    				    MAX310X_BRGDIVLSB_REG + offs, &ret);
    		} while (ret != 0x01);
    
    		regmap_update_bits(s->regmap, MAX310X_MODE1_REG + offs,
    				   MAX310X_MODE1_AUTOSLEEP_BIT,
    				   MAX310X_MODE1_AUTOSLEEP_BIT);
    	}
    
    	uartclk = max310x_set_ref_clk(s, freq, xtal);
    	dev_dbg(dev, "Reference clock set to %i Hz\n", uartclk);
    
    	/* Register UART driver */
    	s->uart.owner		= THIS_MODULE;
    	s->uart.dev_name	= "ttyMAX";
    	s->uart.major		= MAX310X_MAJOR;
    	s->uart.minor		= MAX310X_MINOR;
    	s->uart.nr		= devtype->nr;
    	ret = uart_register_driver(&s->uart);
    	if (ret) {
    		dev_err(dev, "Registering UART driver failed\n");
    		goto out_clk;
    	}
    
    #ifdef CONFIG_GPIOLIB
    	/* Setup GPIO cotroller */
    	s->gpio.owner		= THIS_MODULE;
    	s->gpio.dev		= dev;
    	s->gpio.label		= dev_name(dev);
    	s->gpio.direction_input	= max310x_gpio_direction_input;
    	s->gpio.get		= max310x_gpio_get;
    	s->gpio.direction_output= max310x_gpio_direction_output;
    	s->gpio.set		= max310x_gpio_set;
    	s->gpio.base		= -1;
    	s->gpio.ngpio		= devtype->nr * 4;
    	s->gpio.can_sleep	= 1;
    	ret = gpiochip_add(&s->gpio);
    	if (ret)
    		goto out_uart;
    #endif
    
    	mutex_init(&s->mutex);
    
    	for (i = 0; i < devtype->nr; i++) {
    		/* Initialize port data */
    		s->p[i].port.line	= i;
    		s->p[i].port.dev	= dev;
    		s->p[i].port.irq	= irq;
    		s->p[i].port.type	= PORT_MAX310X;
    		s->p[i].port.fifosize	= MAX310X_FIFO_SIZE;
    		s->p[i].port.flags	= UPF_FIXED_TYPE | UPF_LOW_LATENCY;
    		s->p[i].port.iotype	= UPIO_PORT;
    		s->p[i].port.iobase	= i * 0x20;
    		s->p[i].port.membase	= (void __iomem *)~0;
    		s->p[i].port.uartclk	= uartclk;
    		s->p[i].port.rs485_config = max310x_rs485_config;
    		s->p[i].port.ops	= &max310x_ops;
    		/* Disable all interrupts */
    		max310x_port_write(&s->p[i].port, MAX310X_IRQEN_REG, 0);
    		/* Clear IRQ status register */
    		max310x_port_read(&s->p[i].port, MAX310X_IRQSTS_REG);
    		/* Enable IRQ pin */
    		max310x_port_update(&s->p[i].port, MAX310X_MODE1_REG,
    				    MAX310X_MODE1_IRQSEL_BIT,
    				    MAX310X_MODE1_IRQSEL_BIT);
    		/* Initialize queue for start TX */
    		INIT_WORK(&s->p[i].tx_work, max310x_wq_proc);
    		/* Initialize queue for changing mode */
    		INIT_WORK(&s->p[i].md_work, max310x_md_proc);
    		/* Register port */
    		uart_add_one_port(&s->uart, &s->p[i].port);
    		/* Go to suspend mode */
    		devtype->power(&s->p[i].port, 0);
    	}
    
    	/* Setup interrupt */
    	ret = devm_request_threaded_irq(dev, irq, NULL, max310x_ist,
    					IRQF_ONESHOT | flags, dev_name(dev), s);
    	if (!ret)
    		return 0;
    
    	dev_err(dev, "Unable to reguest IRQ %i\n", irq);
    
    	mutex_destroy(&s->mutex);
    
    #ifdef CONFIG_GPIOLIB
    	gpiochip_remove(&s->gpio);
    
    out_uart:
    #endif
    	uart_unregister_driver(&s->uart);
    
    out_clk:
    	clk_disable_unprepare(s->clk);
    
    	return ret;
    }
    
    static int max310x_remove(struct device *dev)
    {
    	struct max310x_port *s = dev_get_drvdata(dev);
    	int i;
    
    #ifdef CONFIG_GPIOLIB
    	gpiochip_remove(&s->gpio);
    #endif
    
    	for (i = 0; i < s->uart.nr; i++) {
    		cancel_work_sync(&s->p[i].tx_work);
    		cancel_work_sync(&s->p[i].md_work);
    		uart_remove_one_port(&s->uart, &s->p[i].port);
    		s->devtype->power(&s->p[i].port, 0);
    	}
    
    	mutex_destroy(&s->mutex);
    	uart_unregister_driver(&s->uart);
    	clk_disable_unprepare(s->clk);
    
    	return 0;
    }
    
    static const struct of_device_id __maybe_unused max310x_dt_ids[] = {
    	{ .compatible = "maxim,max3107",	.data = &max3107_devtype, },
    	{ .compatible = "maxim,max3108",	.data = &max3108_devtype, },
    	{ .compatible = "maxim,max3109",	.data = &max3109_devtype, },
    	{ .compatible = "maxim,max14830",	.data = &max14830_devtype },
    	{ }
    };
    MODULE_DEVICE_TABLE(of, max310x_dt_ids);
    
    static struct regmap_config regcfg = {
    	.reg_bits = 8,
    	.val_bits = 8,
    	.write_flag_mask = 0x80,
    	.cache_type = REGCACHE_RBTREE,
    	.writeable_reg = max310x_reg_writeable,
    	.volatile_reg = max310x_reg_volatile,
    	.precious_reg = max310x_reg_precious,
    };
    
    #ifdef CONFIG_SPI_MASTER
    static int max310x_spi_probe(struct spi_device *spi)
    {
    	struct max310x_devtype *devtype;
    	unsigned long flags = 0;
    	struct regmap *regmap;
    	int ret;
    
    	/* Setup SPI bus */
    	spi->bits_per_word	= 8;
    	spi->mode		= spi->mode ? : SPI_MODE_0;
    	spi->max_speed_hz	= spi->max_speed_hz ? : 26000000;
    	ret = spi_setup(spi);
    	if (ret)
    		return ret;
    
    	if (spi->dev.of_node) {
    		const struct of_device_id *of_id =
    			of_match_device(max310x_dt_ids, &spi->dev);
    
    		devtype = (struct max310x_devtype *)of_id->data;
    	} else {
    		const struct spi_device_id *id_entry = spi_get_device_id(spi);
    
    		devtype = (struct max310x_devtype *)id_entry->driver_data;
    		flags = IRQF_TRIGGER_FALLING;
    	}
    
    	regcfg.max_register = devtype->nr * 0x20 - 1;
    	regmap = devm_regmap_init_spi(spi, &regcfg);
    
    	return max310x_probe(&spi->dev, devtype, regmap, spi->irq, flags);
    }
    
    static int max310x_spi_remove(struct spi_device *spi)
    {
    	return max310x_remove(&spi->dev);
    }
    
    static const struct spi_device_id max310x_id_table[] = {
    	{ "max3107",	(kernel_ulong_t)&max3107_devtype, },
    	{ "max3108",	(kernel_ulong_t)&max3108_devtype, },
    	{ "max3109",	(kernel_ulong_t)&max3109_devtype, },
    	{ "max14830",	(kernel_ulong_t)&max14830_devtype, },
    	{ }
    };
    MODULE_DEVICE_TABLE(spi, max310x_id_table);
    
    static struct spi_driver max310x_uart_driver = {
    	.driver = {
    		.name		= MAX310X_NAME,
    		.of_match_table	= of_match_ptr(max310x_dt_ids),
    		.pm		= &max310x_pm_ops,
    	},
    	.probe		= max310x_spi_probe,
    	.remove		= max310x_spi_remove,
    	.id_table	= max310x_id_table,
    };
    module_spi_driver(max310x_uart_driver);
    #endif
    
    MODULE_LICENSE("GPL");
    MODULE_AUTHOR("Alexander Shiyan <shc_work@mail.ru>");
    MODULE_DESCRIPTION("MAX310X serial driver");
    

  • https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/968/hci_2D00_testHi Lal,

    It seems like a serial configuration issue.. nothing to do with Bluetopia stack..

    I have a standalong HCI/UART test application to check the BT EN GPIO and HCI/UART connection to the controller, which is completely independent of the Bluetopia stack to check host/controller connectivity. You can try as below:

    $hci-test <dev name> <baudrate> <bt en gpio>

    $hci-test /dev/ttyMAX1 3000000 <gpio>

  • Hi All,

    We are able to fix this issue by doing following changes.

    1. Changes on max driver (driver/tty/serial/max310x.c).
    Max driver is supporting the uart baud rate from 3 to 0.9 Mbps.
    Modified the code to support 3Mbps.

    2. Flow control is not properly configured for max driver on serial core driver (driver/tty/serial/serial_core.c)
    Modified the code to control the flow based on CTS ( uart_handle_cts_change() ).
    CTS high : stop transmission
    CTS low : allow transmission.

    Thanks,
    Lal