Part Number: CC3220
We are using an SMA connector to connect the CC3220 to an external antenna. The enclosure is metal and thus we need an external dipole whip antenna. The issue is the SMA connector shell makes a very low impedance DC ground path which I do not prefer. Can I insert a 10pF between the shell (ground) of the SMA connector and the PCB ground to create isolation or will this just trash the antenna performance?