Tool/software: Code Composer Studio
I have been working over the CC3200 since quite a long time, I achieved what I needed before but now I wanted to make it with low power profile, I tried to implement the idle_profile example code onto my project and it does work good, button and HTTP interruptions both wake up my system but the problem is with the timer interruption it does not work always. First I thought it was a problem with my code but even using the example code it doesn't work always, does any one have experienced this behavior? or there is a pre configuration I'm ignoring
EDIT
I think I've isolated the problem, my code runs (or at least it tries to) like this:
1)Run AP and HTTP server
2)Receive AP parameters and sample time over html
3)Change mode to STA and tries to connect (Red led blinks showing LPDS in/out)
upto this point the codes works just fine, the timer interrupt is generated aswell as the http interrupts and GPIO but when I press a button to restart the process to (1) and send new connections parameters there's where my interrupts stop working when I send the parameters (3) and as I can see it doesn't get to LPDS anymore (Red led is on)