Part Number: CC3120
Other Parts Discussed in Thread: ADS8910B, , MSP432E401Y, CC3100, MSP430F5529
Hi,
In my new project, MSP432E401Y 4 x SPI are occupied by 4 x ADS8910B, so UART is the only communication interface between CC3120 and MSP432E401Y (baud rate up to 3Mbps),
However, from the forum, I found the reply "SPI is used for communication between the host and the CC3120 in the default example code"; is there any other example code for TX/RX data via UART?
Thanks.
Ming