Tool/software: Code Composer Studio
I use provisioning to connect AP, then ping "mqtt server" is success, but cannot broker.
DHCP is ON
IP 192.168.1.158
MASK 255.255.255.0
GW 192.168.1.1
DNS 192.168.1.1
Reply from 192.168.1.170: SUCCESS, Time=111ms, Overall Stat Success (1/1)
[MqttClient_start] Connection to broker fail (-2022)
When I use mqttclient sample code to connect AP, I can to broker.
IP : 192.168.1.158
Mask : 255.255.255.0
Gateway: 192.168.1.1
DNS : 0.0.0.0
[MqttClient_start] Subscription success (0)
refer sample code:
\simplelink_sdk_wifi_plugin_1_60_00_07\examples\rtos\MSP_EXP432E401Y\demos\mqtt_client\tirtos\ccs
\simplelink_sdk_wifi_plugin_1_60_00_07\examples\rtos\MSP_EXP432E401Y\demos\provisioning\tirtos\ccs
I don't know why DNS is different,
how do I setup when I use provisioning to connect?