Tool/software: Linux
So, I have a curious little problem which I'm not sure if it's related to WL1831 or not. It seems that every hour the wifi chip is experiencing beacon losses which disconnects the device from the current network and then reconnects it. We have not been able to relate it to any other device within the network (the minute changes between restarts). Has someone else experienced anything similar or have an idea of what could create such an issue?
See output from syslog below.
BR,
Måns
Jun 21 02:21:15 my-board user.info kernel: [38854.140602] wlcore: Beacon loss detected. roles:0x1
Jun 21 02:21:20 my-board user.info kernel: [38859.022103] wlcore: Connection loss work (role_id: 0).
Jun 21 02:21:20 my-board user.info kernel: [38859.033907] wlan0: Connection to AP c4:ea:1d:e4:9e:97 lost
Jun 21 02:21:20 my-board daemon.info connmand[653]: wlan0 {RX} 27664 packets 4957027 bytes
Jun 21 02:21:20 my-board daemon.info connmand[653]: wlan0 {TX} 3744 packets 654225 bytes
Jun 21 02:21:20 my-board daemon.info connmand[653]: wlan0 {update} flags 36867 <UP>
Jun 21 02:21:20 my-board daemon.info connmand[653]: wlan0 {newlink} index 4 address 88:C2:55:2C:C2:31 mtu 1500
Jun 21 02:21:20 my-board daemon.info connmand[653]: wlan0 {newlink} index 4 operstate 2 <DOWN>
Jun 21 02:21:20 my-board daemon.err connmand[653]: Time request for server 192.168.1.1 failed (101/Network is unreachable)
Jun 21 02:21:20 my-board daemon.err connmand[653]: Time request for server 192.168.1.1 failed (101/Network is unreachable)
Jun 21 02:21:20 my-board user.info kernel: [38859.143024] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
Jun 21 02:21:20 my-board daemon.info connmand[653]: wlan0 {del} address 192.168.1.102/24 label wlan0
Jun 21 02:21:20 my-board daemon.info connmand[653]: wlan0 {del} route 192.168.1.0 gw 0.0.0.0 scope 253 <LINK>
Jun 21 02:21:20 my-board daemon.info connmand[653]: wlan0 {del} route fe80:: gw :: scope 0 <UNIVERSE>
Jun 21 02:21:21 my-board daemon.warn connmand[653]: Skipping disconnect of 4672656a6131_managed_psk, network is connecting.
Jun 21 02:21:21 my-board user.info kernel: [38859.996002] wlan0: authenticate with c4:ea:1d:e4:9e:97
Jun 21 02:21:21 my-board user.info kernel: [38860.028192] wlan0: send auth to c4:ea:1d:e4:9e:97 (try 1/3)
Jun 21 02:21:21 my-board user.info kernel: [38860.051718] wlan0: authenticated
Jun 21 02:21:21 my-board user.info kernel: [38860.072153] wlan0: associate with c4:ea:1d:e4:9e:97 (try 1/3)
Jun 21 02:21:21 my-board user.info kernel: [38860.108663] wlan0: RX AssocResp from c4:ea:1d:e4:9e:97 (capab=0x1411 status=0 aid=2)
Jun 21 02:21:21 my-board user.info kernel: [38860.223725] wlan0: associated
Jun 21 02:21:21 my-board daemon.info connmand[653]: wlan0 {RX} 27665 packets 4957140 bytes
Jun 21 02:21:21 my-board daemon.info connmand[653]: wlan0 {TX} 3744 packets 654225 bytes
Jun 21 02:21:21 my-board daemon.info connmand[653]: wlan0 {update} flags 102403 <UP,LOWER_UP>
Jun 21 02:21:21 my-board daemon.info connmand[653]: wlan0 {newlink} index 4 address 88:C2:55:2C:C2:31 mtu 1500
Jun 21 02:21:21 my-board daemon.info connmand[653]: wlan0 {newlink} index 4 operstate 5 <DORMANT>
Jun 21 02:21:21 my-board daemon.info connmand[653]: wlan0 {add} route fe80:: gw :: scope 0 <UNIVERSE>
Jun 21 02:21:21 my-board user.info kernel: [38860.272287] IPv6: ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready
Jun 21 02:21:21 my-board daemon.info connmand[653]: wlan0 {RX} 27666 packets 4957309 bytes
Jun 21 02:21:21 my-board daemon.info connmand[653]: wlan0 {TX} 3746 packets 654513 bytes
Jun 21 02:21:21 my-board daemon.info connmand[653]: wlan0 {update} flags 102467 <UP,RUNNING,LOWER_UP>
Jun 21 02:21:21 my-board daemon.info connmand[653]: wlan0 {newlink} index 4 address 88:C2:55:2C:C2:31 mtu 1500
Jun 21 02:21:21 my-board daemon.info connmand[653]: wlan0 {newlink} index 4 operstate 6 <UP>
Jun 21 02:21:22 my-board user.info kernel: [38860.444087] wlcore: Association completed.
Jun 21 02:21:22 my-board daemon.info connmand[653]: Setting hostname to my-board
Jun 21 02:21:22 my-board daemon.info connmand[653]: Setting domainname to lan
Jun 21 02:21:22 my-board daemon.info connmand[653]: wlan0 {add} address 192.168.1.102/24 label wlan0 family 2
Jun 21 02:21:22 my-board daemon.info connmand[653]: wlan0 {add} route 192.168.1.0 gw 0.0.0.0 scope 253 <LINK>
Jun 21 02:21:22 my-board daemon.info connmand[653]: wlan0 {add} route 192.168.1.1 gw 0.0.0.0 scope 253 <LINK>
Jun 21 02:21:22 my-board daemon.info connmand[653]: wlan0 {add} route 0.0.0.0 gw 192.168.1.1 scope 0 <UNIVERSE>
Jun 21 02:21:22 my-board daemon.info connmand[653]: ntp: time slew +0.072574 s
Jun 21 02:21:22 my-board daemon.info connmand[653]: wlan0 {add} route 212.227.81.55 gw 192.168.1.1 scope 0 <UNIVERSE>
Jun 21 02:21:22 my-board daemon.info connmand[653]: wlan0 {del} route 212.227.81.55 gw 192.168.1.1 scope 0 <UNIVERSE>
Jun 21 02:21:22 my-board daemon.info connmand[653]: ntp: time slew -0.003862 s