Other Parts Discussed in Thread: WL1837, WL1837MOD, WL1833
Dear TI:
My client has questions about the configuration of the WL183X antenna switch, take the switch control of 5G as an example:
1, When TX: SW_CTRL_TX_3V (D6 of the chip) is 3V and SW_CTRL_RX_3V (E6 of the chip) is 0V
When RX: SW_CTRL_TX_3V (D6 of the chip) is 0V and SW_CTRL_RX_3V (E6 of the chip) is 3V
2, If customer want:
When TX: SW_CTRL_TX_3V (chip's D6 pin) is 3V and SW_CTRL_RX_3V (chip's E6 pin) is 0V,
When RX: SW_CTRL_TX_3V (chip's D6 pin) is 3V and SW_CTRL_RX_3V (chip's D6 pin) is 3V
Can the WL183X support this configuration?
Thanks!