This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3120: CC3120 compatible with TMS570LC4357

Part Number: CC3120
Other Parts Discussed in Thread: LAUNCHXL2-570LC43, TMS570LC4357,

I would like to use the CC3120BOOST with the LAUNCHXL2-570LC43. Are these two launch pad devices compatible? Are there drivers available for the TMS570LC4357? The Simplelink SDK drivers only mention MSP432 compatibility. If these devices are not compatible, is there another simplelink wifi device that is compatible with the TMS570LC4357?