Hi
1.) Question
I need to disable incoming ping responses, so when my device is getting a ping request, it should ignore it
2.) Question
I need to be able to ping a device, so when im connected to a AP, i need to ping a certain IP address to see if it is alive. How can i do this?
3.) Question
In the picture (see link below) you see, that the wifi module sends out a lot of MDNS messages (broadcasts). I need to disable those broadcasts. How can i do this?
4.) Question
I have an issue with the device: When i power up, connect to ap, open a udp socket, transmit data, close socket,.. and then open socket, transmit, close and all over again. no issue. Although, when i power up, connect to ap, open udp socket, transmit, close, DISCONNECT, wait, CONNECT, open socket ... etc.. the device no longer transmitts its data..
Do you have an input what could be the cause of this? It still sends out 3x MDNS packages, but not my message...
Image Link: ibb.co/bGjws9