Hello,
I am connecting my device cc3200 to an enterprise network ( University of Athens ) using EapMethod = SL_ENT_EAP_METHOD_TTLS_MSCHAPv2 succesfully. The University uses eap re-authentication at 30 minute intervals. Does the cc3200 network processor handles this.? My device is loosing connection to the wifi controller exactly after 30 minutes. In the meantime i do not receive any wlan event in the cc3200 such as wifi disconnection or anything else. Also i use an autoconnect policy profile but the processor does not auto connects to the wifi network. The rest ( tasks on free-rtos ) of the processor works ok , does not hung up.