Hello,
I have to design a board in which i use cc3200,so i am asking :
-Can i use to select ANTSEL1 or ANTSEL2 in wifi mode?
-How if i use only one antenna will it impact the connection?
-Does the cc3200 switch automatically from antenna1 to antenna2 automatically?
-If I put the ANTSEL pin high in wifi mode does it force the cc3200 to use only that antenna?
Thank you