Tool/software: Linux
Hi Champs:
Please see the attached.
The Mesh driver dies here:
-->PC is at mesh_get_low_signal_link+0x24/0x6c [mac80211]
Please help to solve.
THanks.
BR Rio
SRV�o�R�b�jg{�c?��n�o��c��g�w�^g�Cg���fG#�K������������������������������������� �������������������������������������������������������������������������������� �������������������������������������������������������������������������������� �������������������������������������������������������������������������������� �����������cGK?�c�K?��foS�cs�[?jRR��?N���{��fw�k'Rnk3f{s�f�S:�K?D�����u%TE? k4DE���D�D5��D%�F �e�E5%?�Ĵ�?E�l��DT??��D�T?D�L��B��LF�� �� ��EE%�ŵĴ�E �DE? ?D��Ĵ??�D��m���M<�@�Mh�D��? OD�]���dd? ��d�ݴ�Ĵd]=�ĥ�D���]����D�D ��5L�T]����T����]B��E�E�E��%D�MM�DMBD�EE?M��EUD?��=?�ť�D��L T�����M? ���I��?�@���DMD�EM��g�D��?Y����K?U?�T����]��]���d�L]d]�D?�QD�L����? t?��?################ mesh start ### ############## netid=0 ========================= OK OK OK OK OK OK Using interface mesh0 with hwaddr 40:bd:32:89:39[ 17.692718] wlcore: down :17 and ssid "" mesh0: interface state UNINITIALIZED->ENABLED AP-ENABLED [ 18.090032] wlcore: PHY firmware version: Rev 8.2.0.0.240 [ 18.269495] wlcore: firmware booted (Rev 8.9.0.0.76) [ 18.283579] IPv6: ADDRCONF(NETDEV_UP): mesh0: link is not ready random: Only 7/20 bytes of strong random data available from /dev/random random: Not enough entropy pool available for secure operations WPA: Not enough entropy in random pool for secure operations - update keys later when t mesh0: joining mesh ATOP_Mesh [ 18.345128] IPv6: ADDRCONF(NETDEV_CHANGE): mesh0: link becomes ready mesh0: CTRL-EVENT-CONNECTED - Connection to 00:00:00:00:00:00 completed [id=0 id_str=] mesh0: MESH-GROUP-STARTED ssid="ATOP_Mesh" id=0 mesh0: mesh plink with 40:bd:32:89:33:6b established mesh0: ===> PLINKS NUMBER: 1 mesh0: MESH-PEER-CONNECTED 40:bd:32:89:33:6b mesh0: mesh plink with 40:bd:32:89:39:41 established mesh0: ===> PLINKS NUMBER: 2 mesh0: MESH-PEER-CONNECTED 40:bd:32:89:39:41 ################# mesh join done ################# adding wlan1 interface Configuration file: /jffs2/hostapd.conf [ 22.811822] IPv6: ADDRCONF(NETDEV_UP): wlan1: link is not ready wlan1: interface state UNINITIALIZED->COUNTRY_UPDATE wlan1: interface state COUNTRY_UPDATE->HT_SCAN Using interface wlan1 with hwaddr 42:bd:32:89:39:16 and ssid "ATOP_AP" random: Cannot read from /dev/random: Resource temporarily unavailable random: Only 0/20 bytes of strong random data available from /dev/random random: Not enough entropy poo[ 24.039375] IPv6: ADDRCONF(NETDEV_CHANGE): wlan1: link l available for secure operations WPA: Not enough entropy in random pool for secure operations - update keys later when t wlan1: interface state HT_SCAN->ENABLED wlan1: AP-ENABLED ################# AP Start ################# ################# wlan0 down ################# [ 27.841350] device mesh0 entered promiscuous mode [ 27.853137] device wlan1 entered promiscuous mode ################# PrimaryAP bridge eth1 mesh0 wlan1 ################# ################# udhcp done ################# [ 32.930674] net eth0: initializing cpsw version 1.12 (0) [ 32.989125] net eth0: phy found : id is : 0x221513 [ 32.994559] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready [ 33.000730] 8021q: adding VLAN 0 to HW filter on device eth0 ################# Set up WAN IP address done ################# ################# NAT done ################# Welcome to ATOP system ATOP login: Welcome to ATOP system ATOP login: wlan1: STA 28:3f:69:25:df:c4 IEEE 802.11: authenticated wlan1: STA 28:3f:69:25:df:c4 IEEE 802.11: associated (aid 1) random: Cannot read from /dev/random: Resource temporarily unavailable random: Only 12/20 bytes of strong random data available from /dev/random random: Not enough entropy pool available for secure operations WPA: Not enough entropy in random pool to proceed - reject first 4-way handshake wlan1: STA 28:3f:69:25:df:c4 IEEE 802.11: authenticated wlan1: STA 28:3f:69:25:df:c4 IEEE 802.11: associated (aid 1) random: Cannot read from /dev/random: Resource temporarily unavailable random: Only 12/20 bytes of strong random data available from /dev/random random: Not enough entropy pool available for secure operations WPA: Not enough entropy in random pool to proceed - reject first 4-way handshake wlan1: STA 28:3f:69:25:df:c4 IEEE 802.11: deauthenticated due to local deauth request Welcome to ATOP system ATOP login: root Password: # ifconfigmesh0: MESH-SAE-AUTH-FAILURE addr=40:bd:32:89:39:3b br0 Link encap:Ethernet HWaddr 40:BD:32:89:39:17 inet addr:10.0.51.100 Bcast:10.0.51.255 Mask:255.255.255.0 inet6 addr: fe80::42bd:32ff:fe89:3917/64 Scope:Link UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:1275 errors:0 dropped:0 overruns:0 frame:0 TX packets:792 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:202021 (197.2 KiB) TX bytes:59046 (57.6 KiB) eth0 Link encap:Ethernet HWaddr 00:60:E9:15:18:13 inet addr:192.168.1.1 Bcast:192.168.1.255 Mask:255.255.255.0 UP BROADCAST PROMISC MULTICAST MTU:1500 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) Interrupt:56 eth1 Link encap:Ethernet HWaddr 00:60:E9:15:18:14 inet6 addr: fe80::260:e9ff:fe15:1814/64 Scope:Link UP BROADCAST RUNNING PROMISC MULTICAST MTU:1500 Metric:1 RX packets:1941 errors:0 dropped:0 overruns:0 frame:0 TX packets:1905 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:319244 (311.7 KiB) TX bytes:202340 (197.5 KiB) lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 inet6 addr: ::1/128 Scope:Host UP LOOPBACK RUNNING MTU:65536 Metric:1 RX packets:2 errors:0 dropped:0 overruns:0 frame:0 TX packets:2 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:0 RX bytes:196 (196.0 B) TX bytes:196 (196.0 B) mesh0 Link encap:Ethernet HWaddr 40:BD:32:89:39:17 inet6 addr: fe80::42bd:32ff:fe89:3917/64 Scope:Link UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:1906 errors:0 dropped:0 overruns:0 frame:0 TX packets:1778 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:224016 (218.7 KiB) TX bytes:341342 (333.3 KiB) wlan1 Link encap:Ethernet HWaddr 42:BD:32:89:39:16 inet6 addr: fe80::40bd:32ff:fe89:3916/64 Scope:Link UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:2 errors:0 dropped:0 overruns:0 frame:0 TX packets:524 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:270 (270.0 B) TX bytes:123358 (120.4 KiB) # [ 82.570574] ------------[ cut here ]------------ [ 82.575630] WARNING: CPU: 0 PID: 726 at /home/jove/project/aw59xx/build-utilites/src /compat_wireless/drivers/net/wireless/ti/wlcore/main.c:5122 wlcore_pending_auth_complet e_work+0x74/0x88 [wlcore]() [ 82.594217] Modules linked in: wlcore_sdio(O) wl18xx(O) wlcore(O) mac80211(O) cfg802 11(O) compat(O) tun GobiNet(O) atop_8250 xr(O) [ 82.606706] CPU: 0 PID: 726 Comm: kworker/u2:2 Tainted: G O 3.14.26-svn180 1 #14 [ 82.615343] Workqueue: phy0 wlcore_pending_auth_complete_work [wlcore] [ 82.622256] [<c0012dac>] (unwind_backtrace) from [<c0011204>] (show_stack+0x10/0x14) [ 82.630415] [<c0011204>] (show_stack) from [<c0033b00>] (warn_slowpath_common+0x6c/0 x8c) [ 82.638929] [<c0033b00>] (warn_slowpath_common) from [<c0033b3c>] (warn_slowpath_nul l+0x1c/0x24) [ 82.648202] [<c0033b3c>] (warn_slowpath_null) from [<bf1b8338>] (wlcore_pending_auth _complete_work+0x74/0x88 [wlcore]) [ 82.659509] [<bf1b8338>] (wlcore_pending_auth_complete_work [wlcore]) from [<c0048ac c>] (process_one_work+0x128/0x3b4) [ 82.670781] [<c0048acc>] (process_one_work) from [<c0048ea0>] (worker_thread+0x114/0 x35c) [ 82.679402] [<c0048ea0>] (worker_thread) from [<c004e3ec>] (kthread+0xbc/0xd8) [ 82.687010] [<c004e3ec>] (kthread) from [<c000e438>] (ret_from_fork+0x14/0x3c) [ 82.694604] ---[ end trace 94e92e9d2857e642 ]--- mesh0: MESH-SAE-AUTH-FAILURE addr=40:bd:32:89:39:3b # # # # iw mesh0 info Interface mesh0 ifindex 10 wdev 0x2 addr 40:bd:32:89:39:17 type mesh point wiphy 0 channel 36 (5180 MHz), width: 40 MHz, center1: 5190 MHz # iw mesh0 station dump Station 40:bd:32:89:39:41 (on mesh0) inactive time: 292 ms rx bytes: 512902 rx packets: 3741 tx bytes: 834652 tx packets: 2763 tx retries: 0 tx failed: 13 signal: 0 dBm signal avg: -71 dBm tx bitrate: 108.0 MBit/s MCS 5 40MHz rx bitrate: 65.0 MBit/s MCS 7 mesh llid: 0 mesh plid: 0 mesh plink: ESTAB mesh local PS mode: ACTIVE mesh peer PS mode: ACTIVE mesh non-peer PS mode: ACTIVE authorized: yes authenticated: yes preamble: long WMM/WME: yes MFP: yes TDLS peer: no Station 40:bd:32:89:33:6b (on mesh0) inactive time: 715 ms rx bytes: 220760 rx packets: 1839 tx bytes: 152432 tx packets: 783 tx retries: 0 tx failed: 0 signal: 0 dBm signal avg: -75 dBm tx bitrate: 108.0 MBit/s MCS 5 40MHz rx bitrate: 58.5 MBit/s MCS 6 mesh llid: 0 mesh plid: 0 mesh plink: ESTAB mesh local PS mode: ACTIVE mesh peer PS mode: ACTIVE mesh non-peer PS mode: ACTIVE authorized: yes authenticated: yes preamble: long WMM/WME: yes MFP: yes TDLS peer: no # # # ping 10.0.51.23 PING 10.0.51.23 (10.0.51.23): 56 data bytes 64 bytes from 10.0.51.23: seq=0 ttl=64 time=8.385 ms 64 bytes from 10.0.51.23: seq=1 ttl=64 time=4.109 ms 64 bytes from 10.0.51.23: seq=2 ttl=64 time=5.530 ms ^C --- 10.0.51.23 ping statistics --- 3 packets transmitted, 3 packets received, 0% packet loss round-trip min/avg/max = 4.109/6.008/8.385 ms # wlan1: STA 28:3f:69:25:df:c4 IEEE 802.11: authenticated wlan1: STA 28:3f:69:25:df:c4 IEEE 802.11: associated (aid 1) wlan1: AP-STA-CONNECTED 28:3f:69:25:df:c4 wlan1: STA 28:3f:69:25:df:c4 WPA: pairwise key handshake completed (RSN) [ 617.658346] Unable to handle kernel NULL pointer dereference at virtual address 0000 005d [ 617.666919] pgd = dcbf4000 [ 617.669936] [0000005d] *pgd=99ca0831, *pte=00000000, *ppte=00000000 [ 617.676575] Internal error: Oops: 17 [#1] ARM [ 617.681152] Modules linked in: wlcore_sdio(O) wl18xx(O) wlcore(O) mac80211(O) cfg802 11(O) compat(O) tun GobiNet(O) atop_8250 xr(O) [ 617.693530] CPU: 0 PID: 1103 Comm: wpa_supplicant Tainted: G W O 3.14.26-svn 1801 #14 [ 617.702392] task: d9d075c0 ti: d7092000 task.ti: d7092000 [ 617.708610] PC is at mesh_get_low_signal_link+0x24/0x6c [mac80211] [ 617.715253] LR is at ieee80211_get_low_signal_mesh+0x10/0x34 [mac80211] [ 617.722202] pc : [<bf133f90>] lr : [<bf0fa220>] psr: 800f0013 [ 617.722202] sp : d7093ca8 ip : dcb44fb0 fp : 00000000 [ 617.734246] r10: dcb44000 r9 : d70a0890 r8 : d71844e8 [ 617.739731] r7 : d7093cf4 r6 : dcb44160 r5 : d7184000 r4 : d7093cc2 [ 617.746578] r3 : d9db9000 r2 : 00000000 r1 : 00000003 r0 : d9db4800 [ 617.753433] Flags: Nzcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user [ 617.760923] Control: 10c5387d Table: 9cbf4019 DAC: 00000015 [ 617.766951] Process wpa_supplicant (pid: 1103, stack limit = 0xd7092238) [ 617.773984] Stack: (0xd7093ca8 to 0xd7094000) [ 617.778562] 3ca0: d9ea8840 d9db9000 bf084724 bf0440cc bf072f40 d70 93cf4 [ 617.787155] 3cc0: 00000001 d9dd2740 d70a0880 bf084724 dcb5b800 bf072f40 d9dd2740 d70 a0880 [ 617.795743] 3ce0: 00000000 c041a724 bf072918 c0417354 00000002 5baafb12 c180044f d70 a0880 [ 617.804333] 3d00: d70a0890 d70a0894 dcb5b800 dcb44000 d7184000 de129800 d70a0880 d9d d2740 [ 617.812928] 3d20: c041a518 d9dd2740 d7093d5c 00000000 00000000 c0419c18 c07b303c d9d d2740 [ 617.821518] 3d40: d9ca1c00 c0419da8 c0419d88 de129800 0000001c c04195e0 0000001c 7ff fffff [ 617.830096] 3d60: d7093e90 d7093f7c d7093e10 d9ca1c00 0000001c 00000000 00000000 c04 19994 [ 617.838675] 3d80: 00000000 c03f5998 d9ca1400 d9dd2740 00000008 d7065dac 00000000 de0 69880 [ 617.847261] 3da0: 00000000 0000044f 00000000 00000000 00000000 c04196ec d9d075c0 d70 93e88 [ 617.855843] 3dc0: 00000000 dda2b6c0 00000000 00000000 d7093e88 c03e8144 00000000 000 00000 [ 617.864428] 3de0: 00000000 d7093e10 d9d075c0 00000000 00000000 00000000 00000000 000 00000 [ 617.873013] 3e00: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 000 0001c [ 617.881601] 3e20: dda2b6c0 d7093ec8 d7093d9c d7093f7c d7093e88 d7093e88 00000008 000 00000 [ 617.890189] 3e40: d7093f7c c03f4998 00000000 bedb71f4 d7093e88 d7093f7c 0000001c c03 e8d54 [ 617.898777] 3e60: d7093e68 d7093e68 00000040 d7093e80 bedb7b24 c03e8a68 c078f890 000 00000 [ 617.907362] 3e80: 001c3928 00003f08 001cda6c 00000000 00000000 00000000 c078da20 c00 74730 [ 617.915944] 3ea0: c35da2b4 d7092000 bedb71a8 bedb71ac ddaf7ac0 bedb71a8 00000004 000 00000 [ 617.924527] 3ec0: 00000004 c03ed7e8 00000010 00000000 00000000 00000000 c36ca2c0 000 0008f [ 617.933118] 3ee0: c07c0a80 c07c0904 00000002 c003dda8 c35d7092 0000008f 00005411 c03 e9278 [ 617.941714] 3f00: 00005452 0000000d 00000000 c00ef91c 7390c1b3 00000003 ffffffff 000 00000 [ 617.950291] 3f20: 00000004 d7093f78 d7092000 bedb7c40 00000001 bedb7c40 00000008 bed b7b24 [ 617.958871] 3f40: 00000000 bedb71f4 00000000 dda2b6c0 bedb71f4 00000000 00000128 c00 0e524 [ 617.967464] 3f60: d7092000 00000000 00000032 c03ea1a4 bedb71a4 00000000 fffffff7 d70 93ec8 [ 617.976048] 3f80: 0000000c d7093e88 00000001 00000000 00000000 00000000 001b2398 001 b2320 [ 617.984633] 3fa0: 001c82b0 c000e3a0 001b2398 001b2320 00000005 bedb71f4 00000000 000 00000 [ 617.993221] 3fc0: 001b2398 001b2320 001c82b0 00000128 bedb71f4 00000033 00000089 000 00032 [ 618.001808] 3fe0: 00000000 bedb71b4 b6d8dd5d b6db69fc 600f0010 00000005 9fef6821 9fe f6c21 [ 618.010756] [<bf133f90>] (mesh_get_low_signal_link [mac80211]) from [<bf0fa220>] (ie ee80211_get_low_signal_mesh+0x10/0x34 [mac80211]) [ 618.023796] [<bf0fa220>] (ieee80211_get_low_signal_mesh [mac80211]) from [<bf0440cc> ] (nl80211_get_low_signal_mesh+0x6c/0x1d0 [cfg80211]) [ 618.036941] [<bf0440cc>] (nl80211_get_low_signal_mesh [cfg80211]) from [<c041a724>] (genl_rcv_msg+0x20c/0x368) [ 618.047444] [<c041a724>] (genl_rcv_msg) from [<c0419c18>] (netlink_rcv_skb+0xac/0xc0 ) [ 618.055670] [<c0419c18>] (netlink_rcv_skb) from [<c0419da8>] (genl_rcv+0x20/0x34) [ 618.063535] [<c0419da8>] (genl_rcv) from [<c04195e0>] (netlink_unicast+0x178/0x1e0) [ 618.071576] [<c04195e0>] (netlink_unicast) from [<c0419994>] (netlink_sendmsg+0x2a8/ 0x388) [ 618.080276] [<c0419994>] (netlink_sendmsg) from [<c03e8144>] (sock_sendmsg+0x84/0xa4 ) [ 618.088508] [<c03e8144>] (sock_sendmsg) from [<c03e8d54>] (___sys_sendmsg.part.25+0x 268/0x278) [ 618.097555] [<c03e8d54>] (___sys_sendmsg.part.25) from [<c03ea1a4>] (__sys_sendmsg+0 x4c/0x78) [ 618.106509] [<c03ea1a4>] (__sys_sendmsg) from [<c000e3a0>] (ret_fast_syscall+0x0/0x3 0) [ 618.114828] Code: e59d3004 e153000c 0a000010 e5932064 (e5d2105d) [ 618.121427] ---[ end trace 94e92e9d2857e643 ]--- wlan1: AP-STA-DISCONNECTED 28:3f:69:25:df:c4
Action frame: SA=40:bd:32:89:33:6b Category=15 [ 413.263269] Internal error: Oops: 17 [#1] ARM
[ 413.271992] Modules linked in: wlcore_sdio(O) wl18xx(O) wlcore(O) mac80211(O) cfg80211(O) compat(O) tun GobiNet(O) atop_8250 xr(O)
[ 413.284358] CPU: 0 PID: 1103 Comm: wpa_supplicant Tainted: G O 3.14.26-svn1801 #14
[ 413.293220] task: d9c0cac0 ti: d709e000 task.ti: d709e000
[ 413.299428] PC is at mesh_get_low_signal_link+0x24/0x6c [mac80211]
[ 413.306067] LR is at ieee80211_get_low_signal_mesh+0x10/0x34 [mac80211]
[ 413.313011] pc : [<bf133f90>] lr : [<bf0fa220>] psr: 200f0013
[ 413.313011] sp : d709fca8 ip : dcb44fb0 fp : 00000000
[ 413.325053] r10: dcb44000 r9 : d71c9050 r8 : d716e4e8
[ 413.330526] r7 : d709fcf4 r6 : dcb44160 r5 : d716e000 r4 : d709fcc2
[ 413.337359] r3 : de0c4800 r2 : 00000000 r1 : 00000003 r0 : dcb57800
[ 413.344194] Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user