We plan to integrate WL1837MOD along-side a cellular modem. In the datasheet, it explicitly states that the module is only certified as a single-modular transmitter. What is required on our end to use this module with the cellular modem? One thing that has come up is that it sounds like we could apply for a class II permissive change so that we can continue to use the same FCC/IC IDs, is this possible with the TI module?