Other Parts Discussed in Thread: CC3200, UNIFLASH
Hello Team !
I am trying to use the get_weather example code with ota But i am getting this error ..
*************************************************
CC3200 TI_CC3200_WITHR00 Application
*************************************************
GET_WEATHER: Test Begin
Host Driver Version: 1.0.1.11
Build Version 2.11.0.1.31.1.5.0.2.1.0.3.37
Device is configured in default state
Started SimpleLink Device: STA Mode
[WLAN EVENT] STA Connected to the AP: TP-LINK_Harish , BSSID: 10:fe:ed:a6:a2:b6
[NETAPP EVENT] IP acquired by the device
Device has connected to TP-LINK_Harish
Device IP Address is 192.168.1.107
Get Host IP succeeded.
Host: api.openweathermap.org IP: 128.199.109.89
EXTLIB_OTA_GET_OPT_IS_PENDING_COMMIT? 0
Starting OTA
OTA run = 2
OTA: NEW IMAGE DOWNLOAD COMPLETE
Rebooting...
*************************************************
CC3200 TI_CC3200_WITHR00 Application
*************************************************
GET_WEATHER: Test Begin
Host Driver Version: 1.0.1.11
Build Version 2.11.0.1.31.1.5.0.2.1.0.3.37
Device is configured in default state
Started SimpleLink Device: STA Mode
[WLAN EVENT] STA Connected to the AP: TP-LINK_Harish , BSSID: 10:fe:ed:a6:a2:b6
[NETAPP EVENT] IP acquired by the device
Device has connected to TP-LINK_Harish
Device IP Address is 192.168.1.107
Get Host IP succeeded.
Host: api.openweathermap.org IP: 128.199.109.89
EXTLIB_OTA_GET_OPT_IS_PENDING_COMMIT? 0
Starting OTA
OTA run = -7
OTA: Error with OTA server
Enter city name, or QUIT to quit: [SOCK ERROR] -close socket (80) operationremote side down from secure to unsecure
Even by the time application is rebooting properly the next reboot is not comming with the dropbox image .It comming with the default image updated through uniflash.
Any pointer would be helpful .
with regards ,
pranav