Other Parts Discussed in Thread: UNIFLASH, , CC3100, CC3200
Tool/software: Linux
Hi. I'm on Ubuntu 18.04. I successfully installed UniFlash 4.4.0.2009. I connected my CC3220SF-LAUNCHXL board and was able to successfully detect it using UniFlash. If I click the "Start" button beneath the serial number of my device, the spinner pops up and nothing happens. Alternately, I tried manually selecting my device in the "New Configuration" section of the UI. I selected "CC3220SF-LAUNCHXL" as my device (also tried with CC31XX/CC32XX with the same outcome). "Serial(UART) Interface" is automatically selected as the connection. Clicking on "Start Image Creator" has the same outcome as just clicking the "Start" button. A spinner comes up and nothing happens.
One thing I notices that is strange is that when I select "CC3220SF-LAUNCHXL" or "CC31XX/CC32XX" as my device, a message pops up that says "Note: CC3100/CC3200 is not supported by Image Creator". I'm not sure why this is coming up, since I'm using a different chip. Also, the CC3220 is on the list of supported devices for this version of UniFlash. Going to "About" and then looking at the components list shows "cc3220_device_support".
Does anyone know what might be going on or how to diagnose this issue?
Thanks in advance,
Eric