Other Parts Discussed in Thread: UNIFLASH, CC3220S, CC3220SF
Hi Ti,
Using uniflash
I am programming binary image in device, on 99% it is giving error
Operation failed: fs_programming error: ret: -10301, ex_err: 2595 - FS_FILE_UNVALID_FILE_SIZE
jumper settings are checked ok, device gets detected, so cable and power are ok. created binary was already programmed earlier and not changed then after. just loading different application binary.
I have two devices, and on both it is showing same error.
please help.