Part Number: CC3220MOD
Other Parts Discussed in Thread: CC3200,
Tool/software: TI-RTOS
Hello All,
I am using CC3200 Launch XL (in Code Composer Studio)and have developed a firmware using mqtt_client example as reference,
Now in designed custom board, its planned to use CC3220MOD or CC3220.
I have gone through the datasheet of both CC3220MOD and CC3220 as per your link mentioned below,
And as per what i have understood is the pin configuration is appearing to be the same but i see that there is an updated SDK for CC3220, So i had few queries,
1. Will the firmware developed using CC3200 LaunchXL be compatible with CC3220MOD or CC3220?
2. If No,What are Changes I need to make to use CC3220MOD or CC3220?
I request you to help me with this issue
Thanks and regards
Utkarash