This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1801MOD: Low output power during TX testing

Part Number: WL1801MOD
Other Parts Discussed in Thread: WL1801, WL1835MOD,

Hi,

I've been trying to get 20 dBm power output from the WL1801 module using the TX testing tool, processors.wiki.ti.com/.../WL18xx_TX_Testing
I'm only getting around 0 dBm output as measured with a spectrum analyzer. I'm getting these power levels consistently no matter what configuration I use.

I've tried the config generated by the configure-device.sh script (answering y/n,1801,n); no config (removing the wl18xx-conf.bin file); wlconf/wl18xx-conf-default.bin; using wlconf to convert official_inis/WL1835MOD_INI.ini into a .bin config.
I even tried hand editing official_inis/WL1835MOD_INI.ini to increase the PwrLimitReference11* and PerChanPwrLimitArr11* parameters to ff (number of 2.4Ghz antennas was set to 1 and 5 Ghz was set to 0).
There is a very small variation (~1-2 dBm) between all the different configs used.

My test sequence is as follows. First, setup the environment with:
ifconfig wlan0 down
calibrator wlan0 plt power_mode on
calibrator wlan0 wl18xx_plt stop_tx
calibrator wlan0 wl18xx_plt tx_tone_stop
calibrator wlan0 wl18xx_plt tune_channel 14 0 0
calibrator wlan0 wl18xx_plt set_tx_power 20000 0 0 14 0 0 0 1 0 0 0 0

Then execute the test itself. Either a continuous TX test or a carrier feedthrough test
(11b continuous test) calibrator wlan0 wl18xx_plt start_tx 500 3 500 0 0 1 0 0 00:11:22:33:44:55 01:02:03:04:05:06 0
(11n continuous test) calibrator wlan0 wl18xx_plt start_tx 400 19 3000 0 0 1 0 0 00:11:22:33:44:55 01:02:03:04:05:06 0
(carrier feed test)   calibrator wlan0 wl18xx_plt tx_tone_start 1 0 0 0

With the carrier feedthrough I get ~5 dBm higher than the 11b continuous test; 11n is even lower than 11b. Using channel 6 instead of 14 results in even lower power by a few (~2-3 dBm).

My Linux distro is based on kernel 4.4. I compiled the drivers as per processors.wiki.ti.com/.../WL18xx_System_Build_Scripts, and grabbed the latest FW .79.
This is the dmesg when drivers are being loaded
[ 4703.996970] Loading modules backported from Linux version R8.7_SP3-0-g8cbba96
[ 4704.004100] Backport generated by backports.git R8.7_SP3-0-gd4777ef
[ 4704.841992] wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
[ 4704.852682] wlcore: loaded
[ 4704.855338] wlcore: driver version: R8.7_SP3
[ 4705.983931] wlcore: PHY firmware version: Rev 8.2.0.0.242
[ 4706.035159] wlcore: firmware booted (Rev 8.9.0.0.79)

Regards,
Emanuel

  • Hi,
    For WL1801MOD, run script with following options and re-run the test:
    Are you using a TI module? [y/n] : y
    What is the chip flavor? [1801/1805/1807/1831/1835/1837 or 0 for unknown] : 1805
    Should certification Class 2 Permissive Change (C2PC) due to higher antenna gain (max 3.2dBm) be applied? [y/n] : y
    How many 2.4GHz antennas are fitted? [1/2] : 1
    Should SISO40 support be applied? [y/n] : <you decide>

    use INI files from : git.ti.com/.../official_inis

    pls keep in mind INI file will limit tx power to meet regulatory compliance. pls consult module datasheet for typical power values

    Thanks
    Saurabh
  • Hi Saurabh,

    Generating the config that way did not solve the problem. In fact, the output powers are pretty much the same with TX carrier testing sitting at ~1 dBm and TX continuous setting at negative values close to 0 dBm. I did another test when I just altered the PwrLimitReference11* values to 'ff' and the output was the same.

    What's more, it seems that the power slowly creeps down as times go on. When I start my test it sits just above 2 dBm but after a few minutes it'll go all the way down to 1.30 or 1.10.

    I have checked that the INIs present in the build output and they are the same as the ones you linked (as they should be  since the build process is from GIT). I've attached both configs that I've used.

    I am aware that WL18xxMOD has a hardware limit in transmit power, in the range ~13 dB to ~17 dB (as per SWRS152M).

    What I am trying to do is to get the device to transmit at the power I specify using the calibrator. I thought that is what the manufacturing tool is for.

    header.magic = 0x10e100ca
    header.version = 0x00070007
    header.checksum = 0x00000000
    core.sg.params = 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x0000000f, 0x0000001b, 0x00000011, 0x000000aa, 0x00000032, 0x00000064, 0x00000320, 0x000000c8, 0x000000c8, 0x00000000, 0x00000000, 0x00000000, 0x00000001, 0x00000000, 0x0000003c, 0x00001388, 0x000004b0, 0x000003e8, 0x00000001, 0x00000003, 0x00000006, 0x0000000a, 0x0000000a, 0x00000002, 0x00000005, 0x0000001e, 0x00000003, 0x0000000a, 0x00000002, 0x00000000, 0x00000019, 0x00000019, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000
    core.sg.state = 0x01
    core.rx.rx_msdu_life_time = 0x0007d000
    core.rx.packet_detection_threshold = 0x00000000
    core.rx.ps_poll_timeout = 0x000f
    core.rx.upsd_timeout = 0x000f
    core.rx.rts_threshold = 0x0931
    core.rx.rx_cca_threshold = 0x0000
    core.rx.irq_blk_threshold = 0xffff
    core.rx.irq_pkt_threshold = 0x0000
    core.rx.irq_timeout = 0x0258
    core.rx.queue_type = 0x00
    core.tx.tx_energy_detection = 0x00
    core.tx.sta_rc_conf.enabled_rates = 0x00000000
    core.tx.sta_rc_conf.short_retry_limit = 0x0a
    core.tx.sta_rc_conf.long_retry_limit = 0x0a
    core.tx.sta_rc_conf.aflags = 0x00
    core.tx.ac_conf_count = 0x04
    core.tx.ac_conf0.ac = 0x00
    core.tx.ac_conf0.cw_min = 0x0f
    core.tx.ac_conf0.cw_max = 0x003f
    core.tx.ac_conf0.aifsn = 0x03
    core.tx.ac_conf0.tx_op_limit = 0x0000
    core.tx.ac_conf1.ac = 0x01
    core.tx.ac_conf1.cw_min = 0x0f
    core.tx.ac_conf1.cw_max = 0x003f
    core.tx.ac_conf1.aifsn = 0x07
    core.tx.ac_conf1.tx_op_limit = 0x0000
    core.tx.ac_conf2.ac = 0x02
    core.tx.ac_conf2.cw_min = 0x0f
    core.tx.ac_conf2.cw_max = 0x003f
    core.tx.ac_conf2.aifsn = 0x01
    core.tx.ac_conf2.tx_op_limit = 0x0bc0
    core.tx.ac_conf3.ac = 0x03
    core.tx.ac_conf3.cw_min = 0x0f
    core.tx.ac_conf3.cw_max = 0x003f
    core.tx.ac_conf3.aifsn = 0x01
    core.tx.ac_conf3.tx_op_limit = 0x05e0
    core.tx.max_tx_retries = 0x64
    core.tx.ap_aging_period = 0x012c
    core.tx.tid_conf_count = 0x04
    core.tx.tid_conf0.queue_id = 0x00
    core.tx.tid_conf0.channel_type = 0x01
    core.tx.tid_conf0.tsid = 0x00
    core.tx.tid_conf0.ps_scheme = 0x00
    core.tx.tid_conf0.ack_policy = 0x00
    core.tx.tid_conf0.apsd_conf = 0x00000000, 0x00000000
    core.tx.tid_conf1.queue_id = 0x01
    core.tx.tid_conf1.channel_type = 0x01
    core.tx.tid_conf1.tsid = 0x01
    core.tx.tid_conf1.ps_scheme = 0x00
    core.tx.tid_conf1.ack_policy = 0x00
    core.tx.tid_conf1.apsd_conf = 0x00000000, 0x00000000
    core.tx.tid_conf2.queue_id = 0x02
    core.tx.tid_conf2.channel_type = 0x01
    core.tx.tid_conf2.tsid = 0x02
    core.tx.tid_conf2.ps_scheme = 0x00
    core.tx.tid_conf2.ack_policy = 0x00
    core.tx.tid_conf2.apsd_conf = 0x00000000, 0x00000000
    core.tx.tid_conf3.queue_id = 0x03
    core.tx.tid_conf3.channel_type = 0x01
    core.tx.tid_conf3.tsid = 0x03
    core.tx.tid_conf3.ps_scheme = 0x00
    core.tx.tid_conf3.ack_policy = 0x00
    core.tx.tid_conf3.apsd_conf = 0x00000000, 0x00000000
    core.tx.tid_conf4.queue_id = 0x00
    core.tx.tid_conf4.channel_type = 0x00
    core.tx.tid_conf4.tsid = 0x00
    core.tx.tid_conf4.ps_scheme = 0x00
    core.tx.tid_conf4.ack_policy = 0x00
    core.tx.tid_conf4.apsd_conf = 0x00000000, 0x00000000
    core.tx.tid_conf5.queue_id = 0x00
    core.tx.tid_conf5.channel_type = 0x00
    core.tx.tid_conf5.tsid = 0x00
    core.tx.tid_conf5.ps_scheme = 0x00
    core.tx.tid_conf5.ack_policy = 0x00
    core.tx.tid_conf5.apsd_conf = 0x00000000, 0x00000000
    core.tx.tid_conf6.queue_id = 0x00
    core.tx.tid_conf6.channel_type = 0x00
    core.tx.tid_conf6.tsid = 0x00
    core.tx.tid_conf6.ps_scheme = 0x00
    core.tx.tid_conf6.ack_policy = 0x00
    core.tx.tid_conf6.apsd_conf = 0x00000000, 0x00000000
    core.tx.tid_conf7.queue_id = 0x00
    core.tx.tid_conf7.channel_type = 0x00
    core.tx.tid_conf7.tsid = 0x00
    core.tx.tid_conf7.ps_scheme = 0x00
    core.tx.tid_conf7.ack_policy = 0x00
    core.tx.tid_conf7.apsd_conf = 0x00000000, 0x00000000
    core.tx.frag_threshold = 0x0930
    core.tx.tx_compl_timeout = 0x015e
    core.tx.tx_compl_threshold = 0x000a
    core.tx.basic_rate = 0x00000001
    core.tx.basic_rate_5 = 0x00000008
    core.tx.tmpl_short_retry_limit = 0x0a
    core.tx.tmpl_long_retry_limit = 0x0a
    core.tx.tx_watchdog_timeout = 0x00001388
    core.tx.slow_link_thold = 0x03
    core.tx.fast_link_thold = 0x1e
    core.conn.wake_up_event = 0x02
    core.conn.listen_interval = 0x01
    core.conn.suspend_wake_up_event = 0x04
    core.conn.suspend_listen_interval = 0x03
    core.conn.bcn_filt_mode = 0x01
    core.conn.bcn_filt_ie_count = 0x03
    core.conn.bcn_filt_ie0.ie = 0x25
    core.conn.bcn_filt_ie0.rule = 0x02
    core.conn.bcn_filt_ie0.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie0.type = 0x00
    core.conn.bcn_filt_ie0.version = 0x00, 0x00
    core.conn.bcn_filt_ie1.ie = 0x3d
    core.conn.bcn_filt_ie1.rule = 0x01
    core.conn.bcn_filt_ie1.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie1.type = 0x00
    core.conn.bcn_filt_ie1.version = 0x00, 0x00
    core.conn.bcn_filt_ie2.ie = 0x2a
    core.conn.bcn_filt_ie2.rule = 0x01
    core.conn.bcn_filt_ie2.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie2.type = 0x00
    core.conn.bcn_filt_ie2.version = 0x00, 0x00
    core.conn.bcn_filt_ie3.ie = 0x00
    core.conn.bcn_filt_ie3.rule = 0x00
    core.conn.bcn_filt_ie3.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie3.type = 0x00
    core.conn.bcn_filt_ie3.version = 0x00, 0x00
    core.conn.bcn_filt_ie4.ie = 0x00
    core.conn.bcn_filt_ie4.rule = 0x00
    core.conn.bcn_filt_ie4.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie4.type = 0x00
    core.conn.bcn_filt_ie4.version = 0x00, 0x00
    core.conn.bcn_filt_ie5.ie = 0x00
    core.conn.bcn_filt_ie5.rule = 0x00
    core.conn.bcn_filt_ie5.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie5.type = 0x00
    core.conn.bcn_filt_ie5.version = 0x00, 0x00
    core.conn.bcn_filt_ie6.ie = 0x00
    core.conn.bcn_filt_ie6.rule = 0x00
    core.conn.bcn_filt_ie6.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie6.type = 0x00
    core.conn.bcn_filt_ie6.version = 0x00, 0x00
    core.conn.bcn_filt_ie7.ie = 0x00
    core.conn.bcn_filt_ie7.rule = 0x00
    core.conn.bcn_filt_ie7.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie7.type = 0x00
    core.conn.bcn_filt_ie7.version = 0x00, 0x00
    core.conn.bcn_filt_ie8.ie = 0x00
    core.conn.bcn_filt_ie8.rule = 0x00
    core.conn.bcn_filt_ie8.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie8.type = 0x00
    core.conn.bcn_filt_ie8.version = 0x00, 0x00
    core.conn.bcn_filt_ie9.ie = 0x00
    core.conn.bcn_filt_ie9.rule = 0x00
    core.conn.bcn_filt_ie9.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie9.type = 0x00
    core.conn.bcn_filt_ie9.version = 0x00, 0x00
    core.conn.bcn_filt_ie10.ie = 0x00
    core.conn.bcn_filt_ie10.rule = 0x00
    core.conn.bcn_filt_ie10.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie10.type = 0x00
    core.conn.bcn_filt_ie10.version = 0x00, 0x00
    core.conn.bcn_filt_ie11.ie = 0x00
    core.conn.bcn_filt_ie11.rule = 0x00
    core.conn.bcn_filt_ie11.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie11.type = 0x00
    core.conn.bcn_filt_ie11.version = 0x00, 0x00
    core.conn.bcn_filt_ie12.ie = 0x00
    core.conn.bcn_filt_ie12.rule = 0x00
    core.conn.bcn_filt_ie12.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie12.type = 0x00
    core.conn.bcn_filt_ie12.version = 0x00, 0x00
    core.conn.bcn_filt_ie13.ie = 0x00
    core.conn.bcn_filt_ie13.rule = 0x00
    core.conn.bcn_filt_ie13.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie13.type = 0x00
    core.conn.bcn_filt_ie13.version = 0x00, 0x00
    core.conn.bcn_filt_ie14.ie = 0x00
    core.conn.bcn_filt_ie14.rule = 0x00
    core.conn.bcn_filt_ie14.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie14.type = 0x00
    core.conn.bcn_filt_ie14.version = 0x00, 0x00
    core.conn.bcn_filt_ie15.ie = 0x00
    core.conn.bcn_filt_ie15.rule = 0x00
    core.conn.bcn_filt_ie15.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie15.type = 0x00
    core.conn.bcn_filt_ie15.version = 0x00, 0x00
    core.conn.bcn_filt_ie16.ie = 0x00
    core.conn.bcn_filt_ie16.rule = 0x00
    core.conn.bcn_filt_ie16.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie16.type = 0x00
    core.conn.bcn_filt_ie16.version = 0x00, 0x00
    core.conn.bcn_filt_ie17.ie = 0x00
    core.conn.bcn_filt_ie17.rule = 0x00
    core.conn.bcn_filt_ie17.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie17.type = 0x00
    core.conn.bcn_filt_ie17.version = 0x00, 0x00
    core.conn.bcn_filt_ie18.ie = 0x00
    core.conn.bcn_filt_ie18.rule = 0x00
    core.conn.bcn_filt_ie18.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie18.type = 0x00
    core.conn.bcn_filt_ie18.version = 0x00, 0x00
    core.conn.bcn_filt_ie19.ie = 0x00
    core.conn.bcn_filt_ie19.rule = 0x00
    core.conn.bcn_filt_ie19.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie19.type = 0x00
    core.conn.bcn_filt_ie19.version = 0x00, 0x00
    core.conn.bcn_filt_ie20.ie = 0x00
    core.conn.bcn_filt_ie20.rule = 0x00
    core.conn.bcn_filt_ie20.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie20.type = 0x00
    core.conn.bcn_filt_ie20.version = 0x00, 0x00
    core.conn.bcn_filt_ie21.ie = 0x00
    core.conn.bcn_filt_ie21.rule = 0x00
    core.conn.bcn_filt_ie21.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie21.type = 0x00
    core.conn.bcn_filt_ie21.version = 0x00, 0x00
    core.conn.bcn_filt_ie22.ie = 0x00
    core.conn.bcn_filt_ie22.rule = 0x00
    core.conn.bcn_filt_ie22.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie22.type = 0x00
    core.conn.bcn_filt_ie22.version = 0x00, 0x00
    core.conn.bcn_filt_ie23.ie = 0x00
    core.conn.bcn_filt_ie23.rule = 0x00
    core.conn.bcn_filt_ie23.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie23.type = 0x00
    core.conn.bcn_filt_ie23.version = 0x00, 0x00
    core.conn.bcn_filt_ie24.ie = 0x00
    core.conn.bcn_filt_ie24.rule = 0x00
    core.conn.bcn_filt_ie24.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie24.type = 0x00
    core.conn.bcn_filt_ie24.version = 0x00, 0x00
    core.conn.bcn_filt_ie25.ie = 0x00
    core.conn.bcn_filt_ie25.rule = 0x00
    core.conn.bcn_filt_ie25.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie25.type = 0x00
    core.conn.bcn_filt_ie25.version = 0x00, 0x00
    core.conn.bcn_filt_ie26.ie = 0x00
    core.conn.bcn_filt_ie26.rule = 0x00
    core.conn.bcn_filt_ie26.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie26.type = 0x00
    core.conn.bcn_filt_ie26.version = 0x00, 0x00
    core.conn.bcn_filt_ie27.ie = 0x00
    core.conn.bcn_filt_ie27.rule = 0x00
    core.conn.bcn_filt_ie27.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie27.type = 0x00
    core.conn.bcn_filt_ie27.version = 0x00, 0x00
    core.conn.bcn_filt_ie28.ie = 0x00
    core.conn.bcn_filt_ie28.rule = 0x00
    core.conn.bcn_filt_ie28.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie28.type = 0x00
    core.conn.bcn_filt_ie28.version = 0x00, 0x00
    core.conn.bcn_filt_ie29.ie = 0x00
    core.conn.bcn_filt_ie29.rule = 0x00
    core.conn.bcn_filt_ie29.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie29.type = 0x00
    core.conn.bcn_filt_ie29.version = 0x00, 0x00
    core.conn.bcn_filt_ie30.ie = 0x00
    core.conn.bcn_filt_ie30.rule = 0x00
    core.conn.bcn_filt_ie30.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie30.type = 0x00
    core.conn.bcn_filt_ie30.version = 0x00, 0x00
    core.conn.bcn_filt_ie31.ie = 0x00
    core.conn.bcn_filt_ie31.rule = 0x00
    core.conn.bcn_filt_ie31.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie31.type = 0x00
    core.conn.bcn_filt_ie31.version = 0x00, 0x00
    core.conn.synch_fail_thold = 0x0000000c
    core.conn.bss_lose_timeout = 0x00000190
    core.conn.beacon_rx_timeout = 0x00002710
    core.conn.broadcast_timeout = 0x00004e20
    core.conn.rx_broadcast_in_ps = 0x01
    core.conn.ps_poll_threshold = 0x0a
    core.conn.sig_weights.rssi_bcn_avg_weight = 0x00
    core.conn.sig_weights.rssi_pkt_avg_weight = 0x00
    core.conn.sig_weights.snr_bcn_avg_weight = 0x00
    core.conn.sig_weights.snr_pkt_avg_weight = 0x00
    core.conn.bet_enable = 0x01
    core.conn.bet_max_consecutive = 0x32
    core.conn.psm_entry_retries = 0x08
    core.conn.psm_exit_retries = 0x10
    core.conn.psm_entry_nullfunc_retries = 0x03
    core.conn.dynamic_ps_timeout = 0x0096
    core.conn.forced_ps = 0x00
    core.conn.keep_alive_interval = 0x0000d6d8
    core.conn.max_listen_interval = 0x14
    core.conn.sta_sleep_auth = 0xff
    core.conn.suspend_rx_ba_activity = 0x00
    core.itrim.enable = 0x00
    core.itrim.timeout = 0x0000c350
    core.pm_config.host_clk_settling_time = 0x00001388
    core.pm_config.host_fast_wakeup_support = 0x01
    core.roam_trigger.trigger_pacing = 0x0001
    core.roam_trigger.avg_weight_rssi_beacon = 0x14
    core.roam_trigger.avg_weight_rssi_data = 0x0a
    core.roam_trigger.avg_weight_snr_beacon = 0x14
    core.roam_trigger.avg_weight_snr_data = 0x0a
    core.scan.min_dwell_time_active = 0x00001d4c
    core.scan.max_dwell_time_active = 0x00007530
    core.scan.min_dwell_time_active_long = 0x000061a8
    core.scan.max_dwell_time_active_long = 0x0000c350
    core.scan.dwell_time_passive = 0x000186a0
    core.scan.dwell_time_dfs = 0x000249f0
    core.scan.num_probe_reqs = 0x0002
    core.scan.split_scan_timeout = 0x0000c350
    core.sched_scan.base_dwell_time = 0x00001d4c
    core.sched_scan.max_dwell_time_delta = 0x000057e4
    core.sched_scan.dwell_time_delta_per_probe = 0x000007d0
    core.sched_scan.dwell_time_delta_per_probe_5 = 0x0000015e
    core.sched_scan.dwell_time_passive = 0x000186a0
    core.sched_scan.dwell_time_dfs = 0x000249f0
    core.sched_scan.num_probe_reqs = 0x02
    core.sched_scan.rssi_threshold = 0xa6
    core.sched_scan.snr_threshold = 0x00
    core.sched_scan.num_short_intervals = 0x0d
    core.sched_scan.long_interval = 0x7530
    core.ht.rx_ba_win_size = 0x20
    core.ht.tx_ba_win_size = 0x40
    core.ht.inactivity_timeout = 0x2710
    core.ht.tx_ba_tid_bitmap = 0x3f
    core.mem.num_stations = 0x01
    core.mem.ssid_profiles = 0x01
    core.mem.rx_block_num = 0x28
    core.mem.tx_min_block_num = 0x28
    core.mem.dynamic_memory = 0x01
    core.mem.min_req_tx_blocks = 0x2d
    core.mem.min_req_rx_blocks = 0x16
    core.mem.tx_min = 0x1b
    core.fm_coex.enable = 0x01
    core.fm_coex.swallow_period = 0x05
    core.fm_coex.n_divider_fref_set_1 = 0xff
    core.fm_coex.n_divider_fref_set_2 = 0x0c
    core.fm_coex.m_divider_fref_set_1 = 0xffff
    core.fm_coex.m_divider_fref_set_2 = 0x0094
    core.fm_coex.coex_pll_stabilization_time = 0xffffffff
    core.fm_coex.ldo_stabilization_time = 0xffff
    core.fm_coex.fm_disturbed_band_margin = 0xff
    core.fm_coex.swallow_clk_diff = 0xff
    core.rx_streaming.duration = 0x00000096
    core.rx_streaming.queues = 0x01
    core.rx_streaming.interval = 0x14
    core.rx_streaming.always = 0x00
    core.fwlog.mode = 0x00
    core.fwlog.mem_blocks = 0x02
    core.fwlog.severity = 0x00
    core.fwlog.timestamp = 0x00
    core.fwlog.output = 0x01
    core.fwlog.threshold = 0x00
    core.rate.rate_retry_score = 0x7d00
    core.rate.per_add = 0x2000
    core.rate.per_th1 = 0x0800
    core.rate.per_th2 = 0x1000
    core.rate.max_per = 0x1fa4
    core.rate.inverse_curiosity_factor = 0x05
    core.rate.tx_fail_low_th = 0x04
    core.rate.tx_fail_high_th = 0x0a
    core.rate.per_alpha_shift = 0x04
    core.rate.per_add_shift = 0x0d
    core.rate.per_beta1_shift = 0x0a
    core.rate.per_beta2_shift = 0x08
    core.rate.rate_check_up = 0x02
    core.rate.rate_check_down = 0x0c
    core.rate.rate_retry_policy = 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
    core.hangover.recover_time = 0x00000000
    core.hangover.hangover_period = 0x14
    core.hangover.dynamic_mode = 0x01
    core.hangover.early_termination_mode = 0x01
    core.hangover.max_period = 0x14
    core.hangover.min_period = 0x01
    core.hangover.increase_delta = 0x01
    core.hangover.decrease_delta = 0x02
    core.hangover.quiet_time = 0x04
    core.hangover.increase_time = 0x01
    core.hangover.window_size = 0x10
    core.recovery.bug_on_recovery = 0x00
    core.recovery.no_recovery = 0x00
    wl18xx.ht.mode = 0x02
    wl18xx.phy.phy_standalone = 0x00
    wl18xx.phy.spare0 = 0x08
    wl18xx.phy.enable_clpc = 0x00
    wl18xx.phy.enable_tx_low_pwr_on_siso_rdl = 0x00
    wl18xx.phy.auto_detect = 0x00
    wl18xx.phy.dedicated_fem = 0x00
    wl18xx.phy.low_band_component = 0x02
    wl18xx.phy.low_band_component_type = 0x05
    wl18xx.phy.high_band_component = 0x01
    wl18xx.phy.high_band_component_type = 0x09
    wl18xx.phy.number_of_assembled_ant2_4 = 0x01
    wl18xx.phy.number_of_assembled_ant5 = 0x00
    wl18xx.phy.pin_muxing_platform_options = 0x00, 0x00
    wl18xx.phy.external_pa_dc2dc = 0x00
    wl18xx.phy.tcxo_ldo_voltage = 0x00
    wl18xx.phy.xtal_itrim_val = 0x04
    wl18xx.phy.srf_state = 0x00
    wl18xx.phy.srf1 = 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
    wl18xx.phy.srf2 = 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
    wl18xx.phy.srf3 = 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
    wl18xx.phy.io_configuration = 0x01
    wl18xx.phy.sdio_configuration = 0x00
    wl18xx.phy.settings = 0x00
    wl18xx.phy.rx_profile = 0x00
    wl18xx.phy.per_chan_pwr_limit_arr_11abg = 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0x2f, 0xff, 0xff, 0xff, 0xff, 0xff, 0xf2, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff
    wl18xx.phy.pwr_limit_reference_11_abg = 0x64
    wl18xx.phy.per_chan_pwr_limit_arr_11p = 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff
    wl18xx.phy.pwr_limit_reference_11p = 0x64
    wl18xx.phy.spare1 = 0x00
    wl18xx.phy.per_chan_bo_mode_11_abg = 0x40, 0x00, 0x04, 0x70, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x18
    wl18xx.phy.per_chan_bo_mode_11_p = 0x00, 0x00, 0x00, 0x00
    wl18xx.phy.primary_clock_setting_time = 0x05
    wl18xx.phy.clock_valid_on_wake_up = 0x00
    wl18xx.phy.secondary_clock_setting_time = 0x05
    wl18xx.phy.board_type = 0x02
    wl18xx.phy.psat = 0x00
    wl18xx.phy.low_power_val = 0xff
    wl18xx.phy.med_power_val = 0xff
    wl18xx.phy.high_power_val = 0xff
    wl18xx.phy.per_sub_band_tx_trace_loss = 0x10, 0x10, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
    wl18xx.phy.per_sub_band_rx_trace_loss = 0x10, 0x10, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
    wl18xx.phy.tx_rf_margin = 0x01
    wl18xx.phy.low_power_val_2nd = 0xff
    wl18xx.phy.med_power_val_2nd = 0xff
    wl18xx.phy.high_power_val_2nd = 0xff
    wl18xx.phy.padding = 0x00
    wl18xx.ap_sleep.idle_duty_cycle = 0x00
    wl18xx.ap_sleep.connected_duty_cycle = 0x00
    wl18xx.ap_sleep.max_stations_thresh = 0x04
    wl18xx.ap_sleep.idle_conn_thresh = 0x08
    

    header.magic = 0x10e100ca
    header.version = 0x00070007
    header.checksum = 0x00000000
    core.sg.params = 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x0000000f, 0x0000001b, 0x00000011, 0x000000aa, 0x00000032, 0x00000064, 0x00000320, 0x000000c8, 0x000000c8, 0x00000000, 0x00000000, 0x00000000, 0x00000001, 0x00000000, 0x0000003c, 0x00001388, 0x000004b0, 0x000003e8, 0x00000001, 0x00000003, 0x00000006, 0x0000000a, 0x0000000a, 0x00000002, 0x00000005, 0x0000001e, 0x00000003, 0x0000000a, 0x00000002, 0x00000000, 0x00000019, 0x00000019, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000
    core.sg.state = 0x01
    core.rx.rx_msdu_life_time = 0x0007d000
    core.rx.packet_detection_threshold = 0x00000000
    core.rx.ps_poll_timeout = 0x000f
    core.rx.upsd_timeout = 0x000f
    core.rx.rts_threshold = 0x0931
    core.rx.rx_cca_threshold = 0x0000
    core.rx.irq_blk_threshold = 0xffff
    core.rx.irq_pkt_threshold = 0x0000
    core.rx.irq_timeout = 0x0258
    core.rx.queue_type = 0x00
    core.tx.tx_energy_detection = 0x00
    core.tx.sta_rc_conf.enabled_rates = 0x00000000
    core.tx.sta_rc_conf.short_retry_limit = 0x0a
    core.tx.sta_rc_conf.long_retry_limit = 0x0a
    core.tx.sta_rc_conf.aflags = 0x00
    core.tx.ac_conf_count = 0x04
    core.tx.ac_conf0.ac = 0x00
    core.tx.ac_conf0.cw_min = 0x0f
    core.tx.ac_conf0.cw_max = 0x003f
    core.tx.ac_conf0.aifsn = 0x03
    core.tx.ac_conf0.tx_op_limit = 0x0000
    core.tx.ac_conf1.ac = 0x01
    core.tx.ac_conf1.cw_min = 0x0f
    core.tx.ac_conf1.cw_max = 0x003f
    core.tx.ac_conf1.aifsn = 0x07
    core.tx.ac_conf1.tx_op_limit = 0x0000
    core.tx.ac_conf2.ac = 0x02
    core.tx.ac_conf2.cw_min = 0x0f
    core.tx.ac_conf2.cw_max = 0x003f
    core.tx.ac_conf2.aifsn = 0x01
    core.tx.ac_conf2.tx_op_limit = 0x0bc0
    core.tx.ac_conf3.ac = 0x03
    core.tx.ac_conf3.cw_min = 0x0f
    core.tx.ac_conf3.cw_max = 0x003f
    core.tx.ac_conf3.aifsn = 0x01
    core.tx.ac_conf3.tx_op_limit = 0x05e0
    core.tx.max_tx_retries = 0x64
    core.tx.ap_aging_period = 0x012c
    core.tx.tid_conf_count = 0x04
    core.tx.tid_conf0.queue_id = 0x00
    core.tx.tid_conf0.channel_type = 0x01
    core.tx.tid_conf0.tsid = 0x00
    core.tx.tid_conf0.ps_scheme = 0x00
    core.tx.tid_conf0.ack_policy = 0x00
    core.tx.tid_conf0.apsd_conf = 0x00000000, 0x00000000
    core.tx.tid_conf1.queue_id = 0x01
    core.tx.tid_conf1.channel_type = 0x01
    core.tx.tid_conf1.tsid = 0x01
    core.tx.tid_conf1.ps_scheme = 0x00
    core.tx.tid_conf1.ack_policy = 0x00
    core.tx.tid_conf1.apsd_conf = 0x00000000, 0x00000000
    core.tx.tid_conf2.queue_id = 0x02
    core.tx.tid_conf2.channel_type = 0x01
    core.tx.tid_conf2.tsid = 0x02
    core.tx.tid_conf2.ps_scheme = 0x00
    core.tx.tid_conf2.ack_policy = 0x00
    core.tx.tid_conf2.apsd_conf = 0x00000000, 0x00000000
    core.tx.tid_conf3.queue_id = 0x03
    core.tx.tid_conf3.channel_type = 0x01
    core.tx.tid_conf3.tsid = 0x03
    core.tx.tid_conf3.ps_scheme = 0x00
    core.tx.tid_conf3.ack_policy = 0x00
    core.tx.tid_conf3.apsd_conf = 0x00000000, 0x00000000
    core.tx.tid_conf4.queue_id = 0x00
    core.tx.tid_conf4.channel_type = 0x00
    core.tx.tid_conf4.tsid = 0x00
    core.tx.tid_conf4.ps_scheme = 0x00
    core.tx.tid_conf4.ack_policy = 0x00
    core.tx.tid_conf4.apsd_conf = 0x00000000, 0x00000000
    core.tx.tid_conf5.queue_id = 0x00
    core.tx.tid_conf5.channel_type = 0x00
    core.tx.tid_conf5.tsid = 0x00
    core.tx.tid_conf5.ps_scheme = 0x00
    core.tx.tid_conf5.ack_policy = 0x00
    core.tx.tid_conf5.apsd_conf = 0x00000000, 0x00000000
    core.tx.tid_conf6.queue_id = 0x00
    core.tx.tid_conf6.channel_type = 0x00
    core.tx.tid_conf6.tsid = 0x00
    core.tx.tid_conf6.ps_scheme = 0x00
    core.tx.tid_conf6.ack_policy = 0x00
    core.tx.tid_conf6.apsd_conf = 0x00000000, 0x00000000
    core.tx.tid_conf7.queue_id = 0x00
    core.tx.tid_conf7.channel_type = 0x00
    core.tx.tid_conf7.tsid = 0x00
    core.tx.tid_conf7.ps_scheme = 0x00
    core.tx.tid_conf7.ack_policy = 0x00
    core.tx.tid_conf7.apsd_conf = 0x00000000, 0x00000000
    core.tx.frag_threshold = 0x0930
    core.tx.tx_compl_timeout = 0x015e
    core.tx.tx_compl_threshold = 0x000a
    core.tx.basic_rate = 0x00000001
    core.tx.basic_rate_5 = 0x00000008
    core.tx.tmpl_short_retry_limit = 0x0a
    core.tx.tmpl_long_retry_limit = 0x0a
    core.tx.tx_watchdog_timeout = 0x00001388
    core.tx.slow_link_thold = 0x03
    core.tx.fast_link_thold = 0x1e
    core.conn.wake_up_event = 0x02
    core.conn.listen_interval = 0x01
    core.conn.suspend_wake_up_event = 0x04
    core.conn.suspend_listen_interval = 0x03
    core.conn.bcn_filt_mode = 0x01
    core.conn.bcn_filt_ie_count = 0x03
    core.conn.bcn_filt_ie0.ie = 0x25
    core.conn.bcn_filt_ie0.rule = 0x02
    core.conn.bcn_filt_ie0.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie0.type = 0x00
    core.conn.bcn_filt_ie0.version = 0x00, 0x00
    core.conn.bcn_filt_ie1.ie = 0x3d
    core.conn.bcn_filt_ie1.rule = 0x01
    core.conn.bcn_filt_ie1.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie1.type = 0x00
    core.conn.bcn_filt_ie1.version = 0x00, 0x00
    core.conn.bcn_filt_ie2.ie = 0x2a
    core.conn.bcn_filt_ie2.rule = 0x01
    core.conn.bcn_filt_ie2.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie2.type = 0x00
    core.conn.bcn_filt_ie2.version = 0x00, 0x00
    core.conn.bcn_filt_ie3.ie = 0x00
    core.conn.bcn_filt_ie3.rule = 0x00
    core.conn.bcn_filt_ie3.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie3.type = 0x00
    core.conn.bcn_filt_ie3.version = 0x00, 0x00
    core.conn.bcn_filt_ie4.ie = 0x00
    core.conn.bcn_filt_ie4.rule = 0x00
    core.conn.bcn_filt_ie4.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie4.type = 0x00
    core.conn.bcn_filt_ie4.version = 0x00, 0x00
    core.conn.bcn_filt_ie5.ie = 0x00
    core.conn.bcn_filt_ie5.rule = 0x00
    core.conn.bcn_filt_ie5.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie5.type = 0x00
    core.conn.bcn_filt_ie5.version = 0x00, 0x00
    core.conn.bcn_filt_ie6.ie = 0x00
    core.conn.bcn_filt_ie6.rule = 0x00
    core.conn.bcn_filt_ie6.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie6.type = 0x00
    core.conn.bcn_filt_ie6.version = 0x00, 0x00
    core.conn.bcn_filt_ie7.ie = 0x00
    core.conn.bcn_filt_ie7.rule = 0x00
    core.conn.bcn_filt_ie7.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie7.type = 0x00
    core.conn.bcn_filt_ie7.version = 0x00, 0x00
    core.conn.bcn_filt_ie8.ie = 0x00
    core.conn.bcn_filt_ie8.rule = 0x00
    core.conn.bcn_filt_ie8.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie8.type = 0x00
    core.conn.bcn_filt_ie8.version = 0x00, 0x00
    core.conn.bcn_filt_ie9.ie = 0x00
    core.conn.bcn_filt_ie9.rule = 0x00
    core.conn.bcn_filt_ie9.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie9.type = 0x00
    core.conn.bcn_filt_ie9.version = 0x00, 0x00
    core.conn.bcn_filt_ie10.ie = 0x00
    core.conn.bcn_filt_ie10.rule = 0x00
    core.conn.bcn_filt_ie10.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie10.type = 0x00
    core.conn.bcn_filt_ie10.version = 0x00, 0x00
    core.conn.bcn_filt_ie11.ie = 0x00
    core.conn.bcn_filt_ie11.rule = 0x00
    core.conn.bcn_filt_ie11.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie11.type = 0x00
    core.conn.bcn_filt_ie11.version = 0x00, 0x00
    core.conn.bcn_filt_ie12.ie = 0x00
    core.conn.bcn_filt_ie12.rule = 0x00
    core.conn.bcn_filt_ie12.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie12.type = 0x00
    core.conn.bcn_filt_ie12.version = 0x00, 0x00
    core.conn.bcn_filt_ie13.ie = 0x00
    core.conn.bcn_filt_ie13.rule = 0x00
    core.conn.bcn_filt_ie13.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie13.type = 0x00
    core.conn.bcn_filt_ie13.version = 0x00, 0x00
    core.conn.bcn_filt_ie14.ie = 0x00
    core.conn.bcn_filt_ie14.rule = 0x00
    core.conn.bcn_filt_ie14.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie14.type = 0x00
    core.conn.bcn_filt_ie14.version = 0x00, 0x00
    core.conn.bcn_filt_ie15.ie = 0x00
    core.conn.bcn_filt_ie15.rule = 0x00
    core.conn.bcn_filt_ie15.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie15.type = 0x00
    core.conn.bcn_filt_ie15.version = 0x00, 0x00
    core.conn.bcn_filt_ie16.ie = 0x00
    core.conn.bcn_filt_ie16.rule = 0x00
    core.conn.bcn_filt_ie16.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie16.type = 0x00
    core.conn.bcn_filt_ie16.version = 0x00, 0x00
    core.conn.bcn_filt_ie17.ie = 0x00
    core.conn.bcn_filt_ie17.rule = 0x00
    core.conn.bcn_filt_ie17.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie17.type = 0x00
    core.conn.bcn_filt_ie17.version = 0x00, 0x00
    core.conn.bcn_filt_ie18.ie = 0x00
    core.conn.bcn_filt_ie18.rule = 0x00
    core.conn.bcn_filt_ie18.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie18.type = 0x00
    core.conn.bcn_filt_ie18.version = 0x00, 0x00
    core.conn.bcn_filt_ie19.ie = 0x00
    core.conn.bcn_filt_ie19.rule = 0x00
    core.conn.bcn_filt_ie19.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie19.type = 0x00
    core.conn.bcn_filt_ie19.version = 0x00, 0x00
    core.conn.bcn_filt_ie20.ie = 0x00
    core.conn.bcn_filt_ie20.rule = 0x00
    core.conn.bcn_filt_ie20.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie20.type = 0x00
    core.conn.bcn_filt_ie20.version = 0x00, 0x00
    core.conn.bcn_filt_ie21.ie = 0x00
    core.conn.bcn_filt_ie21.rule = 0x00
    core.conn.bcn_filt_ie21.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie21.type = 0x00
    core.conn.bcn_filt_ie21.version = 0x00, 0x00
    core.conn.bcn_filt_ie22.ie = 0x00
    core.conn.bcn_filt_ie22.rule = 0x00
    core.conn.bcn_filt_ie22.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie22.type = 0x00
    core.conn.bcn_filt_ie22.version = 0x00, 0x00
    core.conn.bcn_filt_ie23.ie = 0x00
    core.conn.bcn_filt_ie23.rule = 0x00
    core.conn.bcn_filt_ie23.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie23.type = 0x00
    core.conn.bcn_filt_ie23.version = 0x00, 0x00
    core.conn.bcn_filt_ie24.ie = 0x00
    core.conn.bcn_filt_ie24.rule = 0x00
    core.conn.bcn_filt_ie24.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie24.type = 0x00
    core.conn.bcn_filt_ie24.version = 0x00, 0x00
    core.conn.bcn_filt_ie25.ie = 0x00
    core.conn.bcn_filt_ie25.rule = 0x00
    core.conn.bcn_filt_ie25.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie25.type = 0x00
    core.conn.bcn_filt_ie25.version = 0x00, 0x00
    core.conn.bcn_filt_ie26.ie = 0x00
    core.conn.bcn_filt_ie26.rule = 0x00
    core.conn.bcn_filt_ie26.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie26.type = 0x00
    core.conn.bcn_filt_ie26.version = 0x00, 0x00
    core.conn.bcn_filt_ie27.ie = 0x00
    core.conn.bcn_filt_ie27.rule = 0x00
    core.conn.bcn_filt_ie27.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie27.type = 0x00
    core.conn.bcn_filt_ie27.version = 0x00, 0x00
    core.conn.bcn_filt_ie28.ie = 0x00
    core.conn.bcn_filt_ie28.rule = 0x00
    core.conn.bcn_filt_ie28.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie28.type = 0x00
    core.conn.bcn_filt_ie28.version = 0x00, 0x00
    core.conn.bcn_filt_ie29.ie = 0x00
    core.conn.bcn_filt_ie29.rule = 0x00
    core.conn.bcn_filt_ie29.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie29.type = 0x00
    core.conn.bcn_filt_ie29.version = 0x00, 0x00
    core.conn.bcn_filt_ie30.ie = 0x00
    core.conn.bcn_filt_ie30.rule = 0x00
    core.conn.bcn_filt_ie30.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie30.type = 0x00
    core.conn.bcn_filt_ie30.version = 0x00, 0x00
    core.conn.bcn_filt_ie31.ie = 0x00
    core.conn.bcn_filt_ie31.rule = 0x00
    core.conn.bcn_filt_ie31.oui = 0x00, 0x00, 0x00
    core.conn.bcn_filt_ie31.type = 0x00
    core.conn.bcn_filt_ie31.version = 0x00, 0x00
    core.conn.synch_fail_thold = 0x0000000c
    core.conn.bss_lose_timeout = 0x00000190
    core.conn.beacon_rx_timeout = 0x00002710
    core.conn.broadcast_timeout = 0x00004e20
    core.conn.rx_broadcast_in_ps = 0x01
    core.conn.ps_poll_threshold = 0x0a
    core.conn.sig_weights.rssi_bcn_avg_weight = 0x00
    core.conn.sig_weights.rssi_pkt_avg_weight = 0x00
    core.conn.sig_weights.snr_bcn_avg_weight = 0x00
    core.conn.sig_weights.snr_pkt_avg_weight = 0x00
    core.conn.bet_enable = 0x01
    core.conn.bet_max_consecutive = 0x32
    core.conn.psm_entry_retries = 0x08
    core.conn.psm_exit_retries = 0x10
    core.conn.psm_entry_nullfunc_retries = 0x03
    core.conn.dynamic_ps_timeout = 0x0096
    core.conn.forced_ps = 0x00
    core.conn.keep_alive_interval = 0x0000d6d8
    core.conn.max_listen_interval = 0x14
    core.conn.sta_sleep_auth = 0xff
    core.conn.suspend_rx_ba_activity = 0x00
    core.itrim.enable = 0x00
    core.itrim.timeout = 0x0000c350
    core.pm_config.host_clk_settling_time = 0x00001388
    core.pm_config.host_fast_wakeup_support = 0x01
    core.roam_trigger.trigger_pacing = 0x0001
    core.roam_trigger.avg_weight_rssi_beacon = 0x14
    core.roam_trigger.avg_weight_rssi_data = 0x0a
    core.roam_trigger.avg_weight_snr_beacon = 0x14
    core.roam_trigger.avg_weight_snr_data = 0x0a
    core.scan.min_dwell_time_active = 0x00001d4c
    core.scan.max_dwell_time_active = 0x00007530
    core.scan.min_dwell_time_active_long = 0x000061a8
    core.scan.max_dwell_time_active_long = 0x0000c350
    core.scan.dwell_time_passive = 0x000186a0
    core.scan.dwell_time_dfs = 0x000249f0
    core.scan.num_probe_reqs = 0x0002
    core.scan.split_scan_timeout = 0x0000c350
    core.sched_scan.base_dwell_time = 0x00001d4c
    core.sched_scan.max_dwell_time_delta = 0x000057e4
    core.sched_scan.dwell_time_delta_per_probe = 0x000007d0
    core.sched_scan.dwell_time_delta_per_probe_5 = 0x0000015e
    core.sched_scan.dwell_time_passive = 0x000186a0
    core.sched_scan.dwell_time_dfs = 0x000249f0
    core.sched_scan.num_probe_reqs = 0x02
    core.sched_scan.rssi_threshold = 0xa6
    core.sched_scan.snr_threshold = 0x00
    core.sched_scan.num_short_intervals = 0x0d
    core.sched_scan.long_interval = 0x7530
    core.ht.rx_ba_win_size = 0x20
    core.ht.tx_ba_win_size = 0x40
    core.ht.inactivity_timeout = 0x2710
    core.ht.tx_ba_tid_bitmap = 0x3f
    core.mem.num_stations = 0x01
    core.mem.ssid_profiles = 0x01
    core.mem.rx_block_num = 0x28
    core.mem.tx_min_block_num = 0x28
    core.mem.dynamic_memory = 0x01
    core.mem.min_req_tx_blocks = 0x2d
    core.mem.min_req_rx_blocks = 0x16
    core.mem.tx_min = 0x1b
    core.fm_coex.enable = 0x01
    core.fm_coex.swallow_period = 0x05
    core.fm_coex.n_divider_fref_set_1 = 0xff
    core.fm_coex.n_divider_fref_set_2 = 0x0c
    core.fm_coex.m_divider_fref_set_1 = 0xffff
    core.fm_coex.m_divider_fref_set_2 = 0x0094
    core.fm_coex.coex_pll_stabilization_time = 0xffffffff
    core.fm_coex.ldo_stabilization_time = 0xffff
    core.fm_coex.fm_disturbed_band_margin = 0xff
    core.fm_coex.swallow_clk_diff = 0xff
    core.rx_streaming.duration = 0x00000096
    core.rx_streaming.queues = 0x01
    core.rx_streaming.interval = 0x14
    core.rx_streaming.always = 0x00
    core.fwlog.mode = 0x00
    core.fwlog.mem_blocks = 0x02
    core.fwlog.severity = 0x00
    core.fwlog.timestamp = 0x00
    core.fwlog.output = 0x01
    core.fwlog.threshold = 0x00
    core.rate.rate_retry_score = 0x7d00
    core.rate.per_add = 0x2000
    core.rate.per_th1 = 0x0800
    core.rate.per_th2 = 0x1000
    core.rate.max_per = 0x1fa4
    core.rate.inverse_curiosity_factor = 0x05
    core.rate.tx_fail_low_th = 0x04
    core.rate.tx_fail_high_th = 0x0a
    core.rate.per_alpha_shift = 0x04
    core.rate.per_add_shift = 0x0d
    core.rate.per_beta1_shift = 0x0a
    core.rate.per_beta2_shift = 0x08
    core.rate.rate_check_up = 0x02
    core.rate.rate_check_down = 0x0c
    core.rate.rate_retry_policy = 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
    core.hangover.recover_time = 0x00000000
    core.hangover.hangover_period = 0x14
    core.hangover.dynamic_mode = 0x01
    core.hangover.early_termination_mode = 0x01
    core.hangover.max_period = 0x14
    core.hangover.min_period = 0x01
    core.hangover.increase_delta = 0x01
    core.hangover.decrease_delta = 0x02
    core.hangover.quiet_time = 0x04
    core.hangover.increase_time = 0x01
    core.hangover.window_size = 0x10
    core.recovery.bug_on_recovery = 0x00
    core.recovery.no_recovery = 0x00
    wl18xx.ht.mode = 0x02
    wl18xx.phy.phy_standalone = 0x00
    wl18xx.phy.spare0 = 0x08
    wl18xx.phy.enable_clpc = 0x00
    wl18xx.phy.enable_tx_low_pwr_on_siso_rdl = 0x00
    wl18xx.phy.auto_detect = 0x00
    wl18xx.phy.dedicated_fem = 0x00
    wl18xx.phy.low_band_component = 0x02
    wl18xx.phy.low_band_component_type = 0x05
    wl18xx.phy.high_band_component = 0x01
    wl18xx.phy.high_band_component_type = 0x09
    wl18xx.phy.number_of_assembled_ant2_4 = 0x01
    wl18xx.phy.number_of_assembled_ant5 = 0x00
    wl18xx.phy.pin_muxing_platform_options = 0x00, 0x00
    wl18xx.phy.external_pa_dc2dc = 0x00
    wl18xx.phy.tcxo_ldo_voltage = 0x00
    wl18xx.phy.xtal_itrim_val = 0x04
    wl18xx.phy.srf_state = 0x00
    wl18xx.phy.srf1 = 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
    wl18xx.phy.srf2 = 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
    wl18xx.phy.srf3 = 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
    wl18xx.phy.io_configuration = 0x01
    wl18xx.phy.sdio_configuration = 0x00
    wl18xx.phy.settings = 0x00
    wl18xx.phy.rx_profile = 0x00
    wl18xx.phy.per_chan_pwr_limit_arr_11abg = 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x18, 0x78, 0x88, 0x88, 0x78, 0x88, 0x82, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff
    wl18xx.phy.pwr_limit_reference_11_abg = 0x55
    wl18xx.phy.per_chan_pwr_limit_arr_11p = 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff
    wl18xx.phy.pwr_limit_reference_11p = 0x64
    wl18xx.phy.spare1 = 0x00
    wl18xx.phy.per_chan_bo_mode_11_abg = 0x40, 0x00, 0x04, 0x30, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x19
    wl18xx.phy.per_chan_bo_mode_11_p = 0x00, 0x00, 0x00, 0x00
    wl18xx.phy.primary_clock_setting_time = 0x05
    wl18xx.phy.clock_valid_on_wake_up = 0x00
    wl18xx.phy.secondary_clock_setting_time = 0x05
    wl18xx.phy.board_type = 0x02
    wl18xx.phy.psat = 0x00
    wl18xx.phy.low_power_val = 0xff
    wl18xx.phy.med_power_val = 0xff
    wl18xx.phy.high_power_val = 0xff
    wl18xx.phy.per_sub_band_tx_trace_loss = 0x10, 0x10, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
    wl18xx.phy.per_sub_band_rx_trace_loss = 0x10, 0x10, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
    wl18xx.phy.tx_rf_margin = 0x01
    wl18xx.phy.low_power_val_2nd = 0xff
    wl18xx.phy.med_power_val_2nd = 0xff
    wl18xx.phy.high_power_val_2nd = 0xff
    wl18xx.phy.padding = 0x00
    wl18xx.ap_sleep.idle_duty_cycle = 0x00
    wl18xx.ap_sleep.connected_duty_cycle = 0x00
    wl18xx.ap_sleep.max_stations_thresh = 0x04
    wl18xx.ap_sleep.idle_conn_thresh = 0x08
    

  • Hi,
    What hardware platform are you testing this on ? Is it a custom board ?

    Saurabh
  • Yes, it's a custom board. It has a Zynq processor running Petalinux (based on Linux kernel 4.4) and the WL1801 module (among other things).

    All the wireless drivers (loaded in order compat.ko, cfg80211.ko, mac80211.ko, wlcore.ko, wl18xx.ko, wlcore_sdio.ko) are the ones built using the GIT repository.

  • Hi ,
    We don't see this issue at our end. Are you able to perform this on our EVM and use it as reference to troubleshoot your issue ?

    www.ti.com/.../TMDXEVM3358
    www.ti.com/.../WL1837MODCOM8I
    www.ti.com/.../WL18XXCOM82SDMMC

    Thanks
    Saurabh
  • Hi, we haven’t heard back from you, I’m assuming you were able to resolve your issue. If not, just post a reply below (or create a new thread if the thread has locked due to time-out) – thanks