Other Parts Discussed in Thread: CC31XXEMUBOOST
HI
I have a CC3100BOOST plugged onto a CC31XXEMUBOOST board and I have it working on 1 laptop but not on another.
This situation is also happening at our subcontractor on more than one PC.
Both my laptops are running Windows 10 X64 Pro.
I can confirm that the issue is not the USB cable, CC3100BOOST or CC31XXEMUBOOST boards or jumper settings.
On the laptop where it is working the 4 COM ports are correctly registered when I look in the Device Manager and it works just fine.
On the other laptop the 4 COM ports are shown under Other Devices in Device Manager and when I run the same version of Radio Tool (V1.2) I get a Unable to load DLL 'CC3100Lib.dll' message.
Many thanks
BJ