This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC3200: Issue with scanning of 12 and 13 channels in every wifi Access point routers

Part Number: CC3200


Tool/software: Code Composer Studio

Hi this is uday,

         I am working on home automation project, for this we are using CC3200 controller for connecting to internet and we are controlling through UDP/TCP from android/IOS APP. Now my problem is when i am connecting to wifi router it is scanning and connected instead of channel number 12 and 13. when the wifi router is set to 12 and 13 channels at that time even my CC3200 controller is not scanning, why i am don't know it is happening because we have two products one product is scanning every channels but 2nd one is not scanning only 12 and 13 channels, up to bench mark code is same for two products only application level code is different. Can any one please help me for this problem.