Part Number: WL1835MOD
I am designing my own custom board with WL18305MOD module in it. I have gone through many posts on TI forum and through datasheet of module. I would ideally won’t change much in the design to avoid cost of secondary evaluation or additional certificate from FCC. I am also comparing TI’s design with Beagle Bone Black Wireless (BBBW) module. My questions below are related to PCB design and external antenna selections.
Queries:
- TI recommends to have antennas with 2dB gain or less which is different from 3dB gain antenna from BBBW design. Is there any benefit of choosing for less gain antenna as I assume more gain is better for signal strength. I want to understand why TI is recommending 2dB gain antenna and over that asks to have additional 1 dB attenuation on RF trace to reuse the FCC certification while BBW has shorter traces and antenna of 3dB gain
- I also want to understand how antenna selection affects impedance balancing between two antenna traces affects. Why antenna 1 needs to be more away from module compared to antenna 2
- I am planning to have only external antennas in my design. I am planning to use what is recommended by TI but, do I still need to maintain certain distance between antenna or that only applies for on board chip antenna. Are there any specifications for designing external antenna
- If I use only external antenna with SMA connectors then would I still be able to reuse FCC certification
Your reply would be very helpful for me as I am not expert in RF and desperately need your help. I would really appreciate if you can reply me ASAP.
Thanks,