This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220: Power consumption estimation

Part Number: CC3220

Hello,
I plan to use CC3220 as Wi-Fi engine and have to estimate its power consumption and required battery capacity.
Data is collected by another processor that will use CC3220 for communication only.

There are 2 possible scenarios:

  1. "Stand alone". CC3220 is switched off or in deep sleep mode. Sensor collects data (about 1 Kbyte) and  activates CC3220  once per specific period (about 15 minutes). CC3220 establish communication with server, transfers data and returns to deep sleep or shut down.

  2. "Connected".    CC3220 should keep minimal wi-fi connection to be able to receive command from server. If command is received, CC3220 transfers data to server (same amount of data as in "stand alone" mode) and returns to "wait for command" mode.

How can I estimate power consumption (mAh) of these two modes? 

Thanks,

    Yakov