Other Parts Discussed in Thread: CC31XXEMUBOOST, UNIFLASH,
Hi
I have a custom board with a CC3120 device in pre-regulated mode, which I am trying to bring up. All the power rails are OK.
I connected the CC3120 to a CC31xxEMUBOOST according to the CC3120 production line guide and connected that to the PC via J6 on the EMUBOOST.
When I click "Connect" on Uniflash, it doesn't seem to work - the operation times out.
Actually, regardless of if my custom board with the CC3120 is hooked up, the "Connect" operation on Uniflash times out, although I can see the EMUBOOST board in Device Manager.
I have connected the RX, TX, nRESET, and GND on the CC3120 to the EMUBOOST. the nHib line is pulled low. Could this be the issue?
Thanks,
Meenal