Part Number: CC3220
Hello,
I'm trying to work out the scheme whereby we pair our device with a user's alexa account. From what I can tell, this requires us to have our own app, unfortunately. Ok, so the app needs to connect to the CC3220 to provision it to the local wifi SSID. While this functionality is provided by TI, our app will need to read the serial number (or other UID) as well as ask the user to login, so that it can then pair the UID with the user account. OK, the question is, is there an example or app note showing how we can use the simple link mobile app to read the UID?
I see in the SWRU472 app note, section 4.8.5, page 13, that there is this function
public static Boolean setIotUuid(String newName, String baseUrl)
Although it goes the opposite direction, I could make this work if I must -- if I can't read a UUID (or serial number) from the app.
Thoughts?
Chris