Other Parts Discussed in Thread: CC3220S, CC3200
Tool/software: TI-RTOS
wifi_doorlock Project: Mqtt : If Subscription topic increased above 4 , it throws Subscription error.
Hello,
We are using project "wifi_doorlock_CC3220S_LAUNCHXL_tirtos_ccs".
There are 4 subscription topics by default. In our design we need 7 subscription topics.
We are able to connect and subscribe to any (default or customized)4 topic.
But if I add any new topic & increase count to 5. The code give subscription error -4.
How to add more topic?
What is missing ?
FYR, Here are the changes we have made:
*************wifi_doorlock_app.h********************
#define SUBSCRIPTION_TOPIC_COUNT 9
#define SUBSCRIPTION_TOPIC0 "/Broker/To/cc32xx/doorLock"
#define SUBSCRIPTION_TOPIC1 "/cc3220/doorLock/%x%x%x%x%x%x%x%x%x%x%x%x%x%x%x%x/LockControl"
#define SUBSCRIPTION_TOPIC2 "/cc3220/doorLock/%x%x%x%x%x%x%x%x%x%x%x%x%x%x%x%x/LockStatus"
#define SUBSCRIPTION_TOPIC3 "/cc3220/doorLock/%x%x%x%x%x%x%x%x%x%x%x%x%x%x%x%x/LockOTA"
#define SUBSCRIPTION_TOPIC4 "/cc3200/status" // #MQTT_TOPIC
#define SUBSCRIPTION_TOPIC5 "/cc3220/UpReq"
#define SUBSCRIPTION_TOPIC6 "/cc3220/UpResp"
#define SUBSCRIPTION_TOPIC7 "/cc3220/DownReq"
#define SUBSCRIPTION_TOPIC8 "/cc3220/DownResp"
***********mqtt_client_task.c************************
char *topic[SUBSCRIPTION_TOPIC_COUNT] =
{ SUBSCRIPTION_TOPIC0, SUBSCRIPTION_TOPIC1, \
SUBSCRIPTION_TOPIC2, SUBSCRIPTION_TOPIC3, \
SUBSCRIPTION_TOPIC4, SUBSCRIPTION_TOPIC5, SUBSCRIPTION_TOPIC6, SUBSCRIPTION_TOPIC7, SUBSCRIPTION_TOPIC8 };
unsigned char qos[SUBSCRIPTION_TOPIC_COUNT] =
{ MQTT_QOS_0, MQTT_QOS_0, MQTT_QOS_0, MQTT_QOS_0, \
MQTT_QOS_0, MQTT_QOS_0, MQTT_QOS_0, MQTT_QOS_0, MQTT_QOS_0 };