This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/WL1831MOD: kernel thinks the WL1831MOD can use 5 GHz band

Part Number: WL1831MOD

Tool/software: Linux

Hello,

I have a WL1831MOD module on a custom AM335x-based board.  On the latest processor-sdk-linux-rt-4.14.y from ti's git server, the WL1831MOD reports via iw list that it is 5 GHz-capable.  This is causing wifi outages, as our analog front end is not tuned for this frequency, nor do I think the chip is even actually capable of it.

Any help would be appreciated.

From boot:

wlcore: PHY firmware version: Rev 8.2.0.0.242
wlcore: firmware booted (Rev 8.9.0.0.79)

root@XXX:~# iw list
Wiphy phy0
    max # scan SSIDs: 1
    max scan IEs length: 441 bytes
    max # sched scan SSIDs: 16
    max # match sets: 16
    max # scan plans: 1
    max scan plan interval: -1
    max scan plan iterations: 0
    Retry short limit: 7
    Retry long limit: 4
    Coverage class: 0 (up to 0m)
    Device supports AP-side u-APSD.
    Supported Ciphers:
        * WEP40 (00-0f-ac:1)
        * WEP104 (00-0f-ac:5)
        * TKIP (00-0f-ac:2)
        * CCMP-128 (00-0f-ac:4)
        * WPI-SMS4 (00-14-72:1)
    Available Antennas: TX 0 RX 0
    Supported interface modes:
         * managed
         * AP
         * AP/VLAN
         * monitor
         * P2P-client
         * P2P-GO
         * P2P-device
    Band 1:
        Capabilities: 0x107e
            HT20/HT40
            SM Power Save disabled
            RX Greenfield
            RX HT20 SGI
            RX HT40 SGI
            No RX STBC
            Max AMSDU length: 3839 bytes
            DSSS/CCK HT40
        Maximum RX AMPDU length 16383 bytes (exponent: 0x001)
        Minimum RX AMPDU time spacing: 16 usec (0x07)
        HT Max RX data rate: 150 Mbps
        HT TX/RX MCS rate indexes supported: 0-7
        Bitrates (non-HT):
            * 1.0 Mbps
            * 2.0 Mbps (short preamble supported)
            * 5.5 Mbps (short preamble supported)
            * 11.0 Mbps (short preamble supported)
            * 6.0 Mbps
            * 9.0 Mbps
            * 12.0 Mbps
            * 18.0 Mbps
            * 24.0 Mbps
            * 36.0 Mbps
            * 48.0 Mbps
            * 54.0 Mbps
        Frequencies:
            * 2412 MHz [1] (20.0 dBm)
            * 2417 MHz [2] (20.0 dBm)
            * 2422 MHz [3] (20.0 dBm)
            * 2427 MHz [4] (20.0 dBm)
            * 2432 MHz [5] (20.0 dBm)
            * 2437 MHz [6] (20.0 dBm)
            * 2442 MHz [7] (20.0 dBm)
            * 2447 MHz [8] (20.0 dBm)
            * 2452 MHz [9] (20.0 dBm)
            * 2457 MHz [10] (20.0 dBm)
            * 2462 MHz [11] (20.0 dBm)
            * 2467 MHz [12] (20.0 dBm) (no IR)
            * 2472 MHz [13] (20.0 dBm) (no IR)
            * 2484 MHz [14] (20.0 dBm) (no IR)
    Band 2:
        Capabilities: 0x7e
            HT20/HT40
            SM Power Save disabled
            RX Greenfield
            RX HT20 SGI
            RX HT40 SGI
            No RX STBC
            Max AMSDU length: 3839 bytes
            No DSSS/CCK HT40
        Maximum RX AMPDU length 16383 bytes (exponent: 0x001)
        Minimum RX AMPDU time spacing: 16 usec (0x07)
        HT Max RX data rate: 150 Mbps
        HT TX/RX MCS rate indexes supported: 0-7
        Bitrates (non-HT):
            * 6.0 Mbps
            * 9.0 Mbps
            * 12.0 Mbps
            * 18.0 Mbps
            * 24.0 Mbps
            * 36.0 Mbps
            * 48.0 Mbps
            * 54.0 Mbps
        Frequencies:
            * 5040 MHz [8] (disabled)
            * 5060 MHz [12] (disabled)
            * 5080 MHz [16] (disabled)
            * 5170 MHz [34] (disabled)
            * 5180 MHz [36] (20.0 dBm) (no IR)
            * 5190 MHz [38] (20.0 dBm) (no IR)
            * 5200 MHz [40] (20.0 dBm) (no IR)
            * 5210 MHz [42] (20.0 dBm) (no IR)
            * 5220 MHz [44] (20.0 dBm) (no IR)
            * 5230 MHz [46] (20.0 dBm) (no IR)
            * 5240 MHz [48] (20.0 dBm) (no IR)
            * 5260 MHz [52] (20.0 dBm) (no IR, radar detection)
            * 5280 MHz [56] (20.0 dBm) (no IR, radar detection)
            * 5300 MHz [60] (20.0 dBm) (no IR, radar detection)
            * 5320 MHz [64] (20.0 dBm) (no IR, radar detection)
            * 5500 MHz [100] (20.0 dBm) (no IR, radar detection)
            * 5520 MHz [104] (20.0 dBm) (no IR, radar detection)
            * 5540 MHz [108] (20.0 dBm) (no IR, radar detection)
            * 5560 MHz [112] (20.0 dBm) (no IR, radar detection)
            * 5580 MHz [116] (20.0 dBm) (no IR, radar detection)
            * 5600 MHz [120] (20.0 dBm) (no IR, radar detection)
            * 5620 MHz [124] (20.0 dBm) (no IR, radar detection)
            * 5640 MHz [128] (20.0 dBm) (no IR, radar detection)
            * 5660 MHz [132] (20.0 dBm) (no IR, radar detection)
            * 5680 MHz [136] (20.0 dBm) (no IR, radar detection)
            * 5700 MHz [140] (20.0 dBm) (no IR, radar detection)
            * 5745 MHz [149] (20.0 dBm)
            * 5765 MHz [153] (20.0 dBm) (no IR)
            * 5785 MHz [157] (20.0 dBm) (no IR)
            * 5805 MHz [161] (20.0 dBm) (no IR)
            * 5825 MHz [165] (20.0 dBm) (no IR)
    Supported commands:
         * new_interface
         * set_interface
         * new_key
         * start_ap
         * new_station
         * set_bss
         * authenticate
         * associate
         * deauthenticate
         * disassociate
         * join_ibss
         * remain_on_channel
         * set_tx_bitrate_mask
         * frame
         * frame_wait_cancel
         * set_wiphy_netns
         * set_channel
         * set_wds_peer
         * start_sched_scan
         * probe_client
         * set_noack_map
         * register_beacons
         * start_p2p_device
         * set_mcast_rate
         * connect
         * disconnect
         * channel_switch
         * set_qos_map
         * Unknown command (121)
    Supported TX frame types:
         * IBSS: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0
         * managed: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0
         * AP: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0
         * AP/VLAN: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0
         * mesh point: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0
         * P2P-client: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0
         * P2P-GO: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0
         * P2P-device: 0x00 0x10 0x20 0x30 0x40 0x50 0x60 0x70 0x80 0x90 0xa0 0xb0 0xc0 0xd0 0xe0 0xf0
    Supported RX frame types:
         * IBSS: 0x40 0xb0 0xc0 0xd0
         * managed: 0x40 0xd0
         * AP: 0x00 0x20 0x40 0xa0 0xb0 0xc0 0xd0
         * AP/VLAN: 0x00 0x20 0x40 0xa0 0xb0 0xc0 0xd0
         * mesh point: 0xb0 0xc0 0xd0
         * P2P-client: 0x40 0xd0
         * P2P-GO: 0x00 0x20 0x40 0xa0 0xb0 0xc0 0xd0
         * P2P-device: 0x40 0xd0
    WoWLAN support:
         * wake up on anything (device continues operating normally)
         * wake up on pattern match, up to 5 patterns of 1-91 bytes,
           maximum packet offset 0 bytes
    software interface modes (can always be added):
         * AP/VLAN
         * monitor
    valid interface combinations:
         * #{ managed } <= 2, #{ AP, P2P-client, P2P-GO } <= 1, #{ P2P-device } <= 1,
           total <= 3, #channels <= 2
         * #{ AP } <= 2, #{ P2P-device } <= 1,
           total <= 2, #channels <= 1, radar detect widths: { 20 MHz (no HT), 20 MHz, 40 MHz, 80 MHz }

    HT Capability overrides:
         * MCS: ff ff ff ff ff ff ff ff ff ff
         * maximum A-MSDU length
         * supported channel width
         * short GI for 40 MHz
         * max A-MPDU length exponent
         * min MPDU start spacing
    Device supports TX status socket option.
    Device supports HT-IBSS.
    Device supports SAE with AUTHENTICATE command
    Device supports scan flush.
    Device supports AP scan.
    Device supports per-vif TX power setting
    Driver supports full state transitions for AP/GO clients
    Driver supports a userspace MPM
    Device supports configuring vdev MAC-addr on create.