Other Parts Discussed in Thread: WL1837
Hi champs,
The following behavior is seen on a Microprocessor/Linux(4.9) + WL1837 system on wifi side :
- Turn on board and start Linux
- Configure Wifi module and network
- Network is working 300s
- After 300s kernel dump and WiFi module and SDIO communication does not working
Kernel dump stops because WiFi do not respond anymore.
Module is not accessible via SDIO
Still further investigations need to be held but at first sight, is such problem has been already seen in the past? What could be the issue?
Thanks !
Best regards,
Guillaume