Part Number: CC3220
Hi,
I've been having stability problems porting my application from GEN1 (stable with TI-RTOS) to GEN2 with POSIX. (ROV reports no errors but it still occasionally crashes).
I have modified the 'httpget' project (TI-RTOS derivative). In the project I use the TI-RTOS static configurator for task, semaphore and clock function creation.
In the function 'SimplLinkNetAppEventHandler' (in platform.c) once the system has acquired a network address I have replaced the POSIX created httpTask with a Task_SetPri(MyTask,MyPri) call to change MyTask from inactive (-1) to Active (2) and let it run. 'MyTask' is one of the tasks I created using the static configurator.
Now I noticed in the following WIKI that a Task_SetPri() call from a pthread is not allowed:
processors.wiki.ti.com/.../BIOS_POSIX_Thread_(pthread)_Support
"SYS/BIOS supports both pthread and pthread_attrs APIs for POSIX threads.
Since each SYS/BIOS pthread has an underlying Task object, some of the SYS/BIOS Task APIs can be called from a pthread. These include Task_sleep(), Task_yield(), Task_self(), and Task_getPri(). Some Task APIs, such as Task_setPri(), should never be called from a pthread."
Am I still OK however to call Task_SetPri() from the function 'SimpleLinkNetAppEventHandler' ? If not then how would I make my inactive task become active. If I can then my problem must lie elsewhere and I need to dig a bit deeper.
thks & rgds,
Stuart