Part Number: CC3220MODA
Other Parts Discussed in Thread: UNIFLASH, CC3220SF
I am able to connect via Uniflash to a custom board using the CC3220MODASF. I am however unable to program the device and therefore unlock the JTAG. As a result I am also unable to connect via CCS and run the program. I would like tips on how to debug the issue.
This is the information I get from Uniflash:
Device status
Connected: On
Device Type: CC3220SF, Secure
MAC Address: 58:7a:62:41:16:2a
HW Version: 49
Programming Status: On
Current Mode: Production
Storage Capacity: 4096KB
Formatted Capacity: 4096KB
Available for User Files: 2464KB
SFLASH codes: 0xc2,0x28,0x16
Security Alerts: 0 / 15
Is there something I'm missing while using Uniflash?
Thank you!