Part Number: CC3220MODA
I'm working with a customer who is using the pre-certified CC3220MODASF in their handheld application. This is an application where the device is designed to be handheld, but not held against the head. Like a remote control, not like a cell phone. It is our understanding (please confirm) that the additional required SAR testing can be performed by the test house and then the test house can file a class 2 permissive change referencing the original testing performed on the CC3220MODASF.
It is our understanding that the integrated PA is supposed to be kept under a 35% transmit duty cycle during continuous testing to avoid it overheating and drifting out of spec. We also understand that under normal operation CC3220 NWP will automatically [somehow] limit transmit duty cycle to keep the PA under its thermal limit. I'm not sure how the PA limit algorithm works though, and it may have implications in SAR testing.
We are wondering how in the case of SAR testing duty cycle correction should be applied. Do we need to correct up to 100%, or are we okay staying at the 30%-35% levels because this is a normal limit for normal operation?
Please advise.
Thanks,
Stuart