This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200: The customer wants to know the communication speed in the mode.

Part Number: CC3200


Dears:

Customer used CC3200 in their design and the mode is set Station mode.

And the property is follows:

The customer wants to know the communication speed in the mode.

Pls. give some advice about it.

  • Hi Luck,

    Real application throughput at CC3200 depends on application and RF environment. At datasheet are stated values (for the best case):
    UDP: 16 Mbps
    TCP: 13 Mbps

    In real world you can expect slightly lower values than is stated in datasheet.

    Jan