This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3135: Ask UART transparent example

Part Number: CC3135


Do we have UART/Wi-Fi transparent example for CC3135? Thanks.

Besides, it has below error when build power management project.

*** Power management use case Options : ***

    1) for Hibernate

    2) for LPDS

    3) for Transceiver Mode

    4) for Intermittently Connected

    5) for Always Connected

Please enter your Power management use case selection:  3)

number of packets per channel

1

packet size [50-1400 bytes]

50

delay between channels [in miliseconds]

100

packet wifi rate

        1) SL_WLAN_RATE_1M

        2) SL_WLAN_RATE_2M

        3) SL_WLAN_RATE_5_5M

        4) SL_WLAN_RATE_11M

        6) SL_WLAN_RATE_6M

        7) SL_WLAN_RATE_9M

        8) SL_WLAN_RATE_12M

        9) SL_WLAN_RATE_18M

        10) SL_WLAN_RATE_24M

        11) SL_WLAN_RATE_36M

        12) SL_WLAN_RATE_48M

        13) SL_WLAN_RATE_54M

        14) SL_WLAN_RATE_MCS_0

        15) SL_WLAN_RATE_MCS_1

        16) SL_WLAN_RATE_MCS_2

        17) SL_WLAN_RATE_MCS_3

        18) SL_WLAN_RATE_MCS_4

        19) SL_WLAN_RATE_MCS_5

        20) SL_WLAN_RATE_MCS_6

        21) SL_WLAN_RATE_MCS_7

8)

channel mask in HEX [e.g. channels 1,6,11 is 421]

421

power backoff from maximum [0-15 dB]

10

cycle period [in seconds]

2

lowest power level between cycles

        1) for Shutdown (nRESET should be configured in gpioPinConfigs[] under MSP*.c board file)

        2) for Hibernate (nHIB should be configured in gpioPinConfigs[] under MSP*.c board file)

        3) for LPDS 

3)

Error: queueMsg = 0

Error [-1] at line [901] in function [configSimplelinkToUseCase] 

Device Configured to the selected Power Management use case.

unable to start the device