Hi everybody ,
I would like to replace a serial connection via cable with a radio link .
I just need half duplex communication and distance to cover is max 3-5 meters .
the throughput is 1mbit/S ( so 100 bits every 100uS ) , what I need is the 100bit must be received on the other side before a new frame comes in : i must guarantee 100bits every 100uS max . this is mandatory
do you think this is feasible ?
should I use std wifi or I must go for some RAW data ?
will using 5GHz ( a different module ) make life easier ?
any input is welcome
regards
Carlo