Hello.
When CC3220S-LAUNCHXL is plugged in to the computer, device manager recognize not as XDS110 any COM port but unknown device in USB.
When I attempt connect CC3220S-LAUNCHXL to CCS JTAG, there is an error -260 and described that xds firmware update is needed.
So I would like to update the firmware of XDS110.
I am referring following document.
C:\ti\ccs901\ccs\ccs_base\common\uscif\xds110\XDS110SupportReadMe.pdf
After doing "Recovering a Bricked XDS110 without JTAG", only D7 LED seems to be on.
Then, I execute following command referring "Updating the Firmware Using xdsdfu", but command prompt say "The request device was not found on the bus".
C:\ti\ccs901\ccs\ccs_base\common\uscif\xds110>xdsdfu.exe -m
Could you tell me how to recover XDS110 in CC3220S-LAUNCHXL?
Regards,
U-SK